OPAMP_Init_TypeDef Struct ReferenceEMLIB > OPAMP
OPAMP init structure.
       Definition at line
       
        442
       
       of file
       
        em_opamp.h
       
       .
      
      
       #include <
       
     
        em_opamp.h
       
       >
      
         Data Fields | 
       |
| uint32_t | bias | 
| bool | defaultOffset | 
| bool | halfBias | 
| bool | hcmDisable | 
| bool | lpfNegPadDisable | 
| bool | lpfPosPadDisable | 
| OPAMP_NegSel_TypeDef | negSel | 
| bool | nextOut | 
| bool | npEn | 
| uint32_t | offset | 
| OPAMP_OutMode_TypeDef | outMode | 
| uint32_t | outPen | 
| OPAMP_PosSel_TypeDef | posSel | 
| bool | ppEn | 
| OPAMP_ResInMux_TypeDef | resInMux | 
| OPAMP_ResSel_TypeDef | resSel | 
| bool | shortInputs | 
Field Documentation
| uint32_t OPAMP_Init_TypeDef::bias | 
| bool OPAMP_Init_TypeDef::defaultOffset | 
Use factory calibrated opamp offset value.
        Definition at line
        
         502
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::halfBias | 
Divide OPAMP bias current by 2.
        Definition at line
        
         494
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::hcmDisable | 
Disable input rail-to-rail capability.
        Definition at line
        
         501
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::lpfNegPadDisable | 
Disable low pass filter on negative pad.
        Definition at line
        
         496
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::lpfPosPadDisable | 
Disable low pass filter on positive pad.
        Definition at line
        
         495
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_NegSel_TypeDef OPAMP_Init_TypeDef::negSel | 
Select input source for negative terminal.
        Definition at line
        
         443
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::nextOut | 
Enable NEXTOUT signal source.
        Definition at line
        
         497
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::npEn | 
| uint32_t OPAMP_Init_TypeDef::offset | 
Opamp offset value when defaultOffset is false.
        Definition at line
        
         503
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_OutMode_TypeDef OPAMP_Init_TypeDef::outMode | 
Output terminal connection.
        Definition at line
        
         445
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| uint32_t OPAMP_Init_TypeDef::outPen | 
        Alternate output enable bit mask. This value should consist one or more of the DAC_OPA[opa#]MUX_OUTPEN_OUT[output#] flags (defined in <part_name>_dac.h) OR'ed together.
        
        
        For OPA0:
       
- DAC_OPA0MUX_OUTPEN_OUT0
 - DAC_OPA0MUX_OUTPEN_OUT1
 - DAC_OPA0MUX_OUTPEN_OUT2
 - DAC_OPA0MUX_OUTPEN_OUT3
 - DAC_OPA0MUX_OUTPEN_OUT4
 
For OPA1:
- DAC_OPA1MUX_OUTPEN_OUT0
 - DAC_OPA1MUX_OUTPEN_OUT1
 - DAC_OPA1MUX_OUTPEN_OUT2
 - DAC_OPA1MUX_OUTPEN_OUT3
 - DAC_OPA1MUX_OUTPEN_OUT4
 
For OPA2:
- DAC_OPA2MUX_OUTPEN_OUT0
 - DAC_OPA2MUX_OUTPEN_OUT1
 
        E.g:
        
        init.outPen = DAC_OPA0MUX_OUTPEN_OUT0 | DAC_OPA0MUX_OUTPEN_OUT2 | DAC_OPA0MUX_OUTPEN_OUT4;
       
        Definition at line
        
         448
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_PosSel_TypeDef OPAMP_Init_TypeDef::posSel | 
Select input source for positive terminal.
        Definition at line
        
         444
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::ppEn | 
| OPAMP_ResInMux_TypeDef OPAMP_Init_TypeDef::resInMux | 
Select input source for resistor ladder.
        Definition at line
        
         447
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| OPAMP_ResSel_TypeDef OPAMP_Init_TypeDef::resSel | 
Select R2/R1 resistor ratio.
        Definition at line
        
         446
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::shortInputs | 
Short OPAMP input terminals.
        Definition at line
        
         500
        
        of file
        
         em_opamp.h
        
        .
       
Referenced by OPAMP_Enable() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_opamp.h