SPIDRV_Init Struct ReferenceEMDRV > SPIDRV
An SPI driver instance initialization structure. Contains a number of SPIDRV configuration options. This structure is passed to SPIDRV_Init() when initializing a SPIDRV instance. Some common initialization data sets are predefined in SPIDRV_MASTER_USART0 and friends.
       Definition at line
       
        118
       
       of file
       
        spidrv.h
       
       .
      
      
       #include <
       
     
        spidrv.h
       
       >
      
         Data Fields | 
       |
| SPIDRV_BitOrder_t | bitOrder | 
| 
         A bit order on the SPI bus, MSB or LSB first.
          | 
       |
| uint32_t | bitRate | 
| 
         An SPI bitrate.
          | 
       |
| SPIDRV_ClockMode_t | clockMode | 
| 
         SPI mode, CLKPOL/CLKPHASE setting.
          | 
       |
| SPIDRV_CsControl_t | csControl | 
| 
         A select master mode chip select (CS) control scheme.
          | 
       |
| uint32_t | dummyTxValue | 
| 
         The value to transmit when using SPI receive API functions.
          | 
       |
| uint32_t | frameLength | 
| 
         An SPI framelength, valid numbers are 4..16.
          | 
       |
| USART_TypeDef * | port | 
| 
         The USART used for SPI.
          | 
       |
| uint8_t | portLocation | 
| 
         A location number for SPI pins.
          | 
       |
| SPIDRV_SlaveStart_t | slaveStartMode | 
| 
         A slave mode transfer start scheme.
          | 
       |
| SPIDRV_Type_t | type | 
| 
         An SPI type, master or slave.
          | 
       |
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emdrv/spidrv/inc/
       
spidrv.h