USB_EndpointDescriptor_TypeDef Struct ReferencePlatform Middleware > USB > USB_COMMON
USB Endpoint Descriptor.
       Definition at line
       
        490
       
       of file
       
        em_usb.h
       
       .
      
      
       #include <
       
     
        em_usb.h
       
       >
      
         Data Fields | 
       |
| uint8_t | bDescriptorType | 
| uint8_t | bEndpointAddress | 
| uint8_t | bInterval | 
| uint8_t | bLength | 
| uint8_t | bmAttributes | 
| uint16_t | wMaxPacketSize | 
Field Documentation
| uint8_t USB_EndpointDescriptor_TypeDef::bDescriptorType | 
Constant ENDPOINT Descriptor Type
        Definition at line
        
         492
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintEndpointDescriptor() .
| uint8_t USB_EndpointDescriptor_TypeDef::bEndpointAddress | 
The address of the endpoint
        Definition at line
        
         493
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBD_Init() , USBH_AssignHostChannel() , and USBH_PrintEndpointDescriptor() .
| uint8_t USB_EndpointDescriptor_TypeDef::bInterval | 
Interval for polling EP for data transfers
        Definition at line
        
         496
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintEndpointDescriptor() , USBH_Read() , and USBH_Write() .
| uint8_t USB_EndpointDescriptor_TypeDef::bLength | 
Size of this descriptor in bytes
        Definition at line
        
         491
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintEndpointDescriptor() .
| uint8_t USB_EndpointDescriptor_TypeDef::bmAttributes | 
This field describes the endpoint attributes
        Definition at line
        
         494
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBD_Init() , USBH_AssignHostChannel() , and USBH_PrintEndpointDescriptor() .
| uint16_t USB_EndpointDescriptor_TypeDef::wMaxPacketSize | 
Maximum packet size for the endpoint
        Definition at line
        
         495
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBD_Init() , USBH_AssignHostChannel() , and USBH_PrintEndpointDescriptor() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
       
em_usb.h