USBH_Device_TypeDef Struct ReferencePlatform Middleware > USB > USB_HOST
USB HOST device definition.
A host application should not manipulate the contents of this struct.
       Definition at line
       
        865
       
       of file
       
        em_usb.h
       
       .
      
      
       #include <
       
     
        em_usb.h
       
       >
      
         Data Fields | 
       |
| uint8_t | addr | 
| USB_ConfigurationDescriptor_TypeDef | confDesc | 
| USB_DeviceDescriptor_TypeDef | devDesc | 
| USBH_Ep_TypeDef * | ep | 
| USBH_Ep_TypeDef | ep0 | 
| USB_InterfaceDescriptor_TypeDef | itfDesc | 
| int | numEp | 
| uint8_t | speed | 
Field Documentation
| uint8_t USBH_Device_TypeDef::addr | 
The device address.
        Definition at line
        
         872
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_InitDeviceData() , and USBH_SetAddressB() .
| USB_ConfigurationDescriptor_TypeDef USBH_Device_TypeDef::confDesc | 
The device configuration descriptor.
        Definition at line
        
         867
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_InitDeviceData() , and USBH_QueryDeviceB() .
| USB_DeviceDescriptor_TypeDef USBH_Device_TypeDef::devDesc | 
The device device descriptor.
        Definition at line
        
         866
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_InitDeviceData() , USBH_QueryDeviceB() , and USBH_WaitForDeviceConnectionB() .
| USBH_Ep_TypeDef * USBH_Device_TypeDef::ep | 
Array of endpoint status data.
        Definition at line
        
         870
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_InitDeviceData() , USBH_QueryDeviceB() , USBH_SetAltInterfaceB() , and USBH_SetConfigurationB() .
| USBH_Ep_TypeDef USBH_Device_TypeDef::ep0 | 
Endpoint 0 status data.
        Definition at line
        
         869
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_GetConfigurationDescriptorB() , USBH_GetDeviceDescriptorB() , USBH_GetStringB() , USBH_InitDeviceData() , USBH_QueryDeviceB() , USBH_SetAddressB() , USBH_SetAltInterfaceB() , USBH_SetConfigurationB() , USBH_StallEpB() , and USBH_UnStallEpB() .
| USB_InterfaceDescriptor_TypeDef USBH_Device_TypeDef::itfDesc | 
The device interface descriptor.
        Definition at line
        
         868
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_InitDeviceData() .
| int USBH_Device_TypeDef::numEp | 
Number of endpoints.
        Definition at line
        
         871
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_InitDeviceData() , USBH_SetAltInterfaceB() , and USBH_SetConfigurationB() .
| uint8_t USBH_Device_TypeDef::speed | 
The device speed (low or full speed).
        Definition at line
        
         873
        
        of file
        
         em_usb.h
        
        .
       
Referenced by MSDBOT_Init() , USBH_InitDeviceData() , and USBH_QueryDeviceB() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
       
em_usb.h