CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
       Definition at line
       
        1447
       
       of file
       
        em_cmu.h
       
       .
      
      
       #include <
       
     
        em_cmu.h
       
       >
      
         Data Fields | 
       |
| uint8_t | boost | 
| bool | glitchDetector | 
| CMU_OscMode_TypeDef | mode | 
| uint8_t | timeout | 
Field Documentation
| uint8_t CMU_HFXOInit_TypeDef::boost | 
HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%
        Definition at line
        
         1472
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::glitchDetector | 
Enable/disable glitch detector
        Definition at line
        
         1474
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode | 
| uint8_t CMU_HFXOInit_TypeDef::timeout | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       
em_cmu.h