DAC_TypeDef Struct ReferenceDevices > EZR32LG_DAC
       Definition at line
       
        48
       
       of file
       
        ezr32lg_dac.h
       
       .
      
         Data Fields | 
       |
| __IOM uint32_t | BIASPROG | 
| __IOM uint32_t | CAL | 
| __IOM uint32_t | CH0CTRL | 
| __IOM uint32_t | CH0DATA | 
| __IOM uint32_t | CH1CTRL | 
| __IOM uint32_t | CH1DATA | 
| __IOM uint32_t | COMBDATA | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | OPA0MUX | 
| __IOM uint32_t | OPA1MUX | 
| __IOM uint32_t | OPA2MUX | 
| __IOM uint32_t | OPACTRL | 
| __IOM uint32_t | OPAOFFSET | 
| uint32_t | RESERVED0 [8] | 
| __IM uint32_t | STATUS | 
Field Documentation
| __IOM uint32_t DAC_TypeDef::BIASPROG | 
| __IOM uint32_t DAC_TypeDef::CAL | 
Calibration Register
        Definition at line
        
         60
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_Init() , and DAC_Reset() .
| __IOM uint32_t DAC_TypeDef::CH0CTRL | 
Channel 0 Control Register
        Definition at line
        
         51
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_Enable() , DAC_Init() , DAC_InitChannel() , and DAC_Reset() .
| __IOM uint32_t DAC_TypeDef::CH0DATA | 
Channel 0 Data Register
        Definition at line
        
         57
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_Channel0OutputSet() .
| __IOM uint32_t DAC_TypeDef::CH1CTRL | 
Channel 1 Control Register
        Definition at line
        
         52
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_Enable() , DAC_Init() , DAC_InitChannel() , and DAC_Reset() .
| __IOM uint32_t DAC_TypeDef::CH1DATA | 
Channel 1 Data Register
        Definition at line
        
         58
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_Channel1OutputSet() .
| __IOM uint32_t DAC_TypeDef::COMBDATA | 
Combined Data Register
        Definition at line
        
         59
        
        of file
        
         ezr32lg_dac.h
        
        .
       
| __IOM uint32_t DAC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         49
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_Init() , and DAC_Reset() .
| __IOM uint32_t DAC_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         53
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_IntDisable() , DAC_IntEnable() , DAC_IntGetEnabled() , and DAC_Reset() .
| __IM uint32_t DAC_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         54
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_IntGet() , and DAC_IntGetEnabled() .
| __IOM uint32_t DAC_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         56
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_IntClear() , and DAC_Reset() .
| __IOM uint32_t DAC_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         55
        
        of file
        
         ezr32lg_dac.h
        
        .
       
Referenced by DAC_IntSet() .
| __IOM uint32_t DAC_TypeDef::OPA0MUX | 
Operational Amplifier Mux Configuration Register
        Definition at line
        
         65
        
        of file
        
         ezr32lg_dac.h
        
        .
       
| __IOM uint32_t DAC_TypeDef::OPA1MUX | 
Operational Amplifier Mux Configuration Register
        Definition at line
        
         66
        
        of file
        
         ezr32lg_dac.h
        
        .
       
| __IOM uint32_t DAC_TypeDef::OPA2MUX | 
Operational Amplifier Mux Configuration Register
        Definition at line
        
         67
        
        of file
        
         ezr32lg_dac.h
        
        .
       
| __IOM uint32_t DAC_TypeDef::OPACTRL | 
Operational Amplifier Control Register
        Definition at line
        
         63
        
        of file
        
         ezr32lg_dac.h
        
        .
       
| __IOM uint32_t DAC_TypeDef::OPAOFFSET | 
Operational Amplifier Offset Register
        Definition at line
        
         64
        
        of file
        
         ezr32lg_dac.h
        
        .
       
| uint32_t DAC_TypeDef::RESERVED0[8] | 
Reserved for future use
        Definition at line
        
         62
        
        of file
        
         ezr32lg_dac.h
        
        .
       
| __IM uint32_t DAC_TypeDef::STATUS | 
Status Register
        Definition at line
        
         50
        
        of file
        
         ezr32lg_dac.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
       
ezr32lg_dac.h