hidkbd.h File Reference
USB Human Interface Devices (HID) class keyboard driver.
- Version
 - 5.5.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        hidkbd.h
       
       .
      
       #include <stdint.h>
      
      
       #include "
       
        em_usb.h
       
       "
      
      
         Data Structures | 
       |
| struct | HIDKBD_Init_t | 
| struct | HIDKBD_KeyReport_t | 
         Typedefs | 
       |
| typedef void(* | HIDKBD_SetReportFunc_t ) (uint8_t report) | 
| 
         Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.
          | 
       |
         Functions | 
       |
| void | HIDKBD_Init ( HIDKBD_Init_t *init) | 
| 
         Initialize HID Keyboard driver.
          | 
       |
| void | HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t *report) | 
| 
         Report a keyboard press/release event.
          | 
       |
| int | HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup) | 
| 
         Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
          | 
       |
| void | HIDKBD_StateChangeEvent ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| 
         Handle USB state change events, this function must be called each time the USB device state is changed.
          | 
       |
         Variables | 
       |
| const char | HIDKBD_ReportDescriptor [69] |