retargetserial.c File Reference
Provide stdio retargeting to USART/UART or LEUART.
- Version
 - 5.5.0
 
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        retargetserial.c
       
       .
      
       #include <stdio.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_cmu.h
       
       "
      
      
       #include "
       
        em_core.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        retargetserial.h
       
       "
      
      
       #include "retargetserialconfig.h"
      
      
         Macros | 
       |
| #define | _GENERIC_UART_STATUS_IDLE LEUART_STATUS_TXC | 
| #define | RXBUFSIZE 8 | 
         Functions | 
       |
| static void | disableRxInterrupt () | 
| 
         Disable RX interrupt.
          | 
       |
| static void | enableRxInterrupt () | 
| 
         Enable RX interrupt.
          | 
       |
| void | RETARGET_IRQ_NAME (void) | 
| 
         UART/LEUART IRQ Handler.
          | 
       |
| int | RETARGET_ReadChar (void) | 
| 
         Receive a byte from USART/LEUART and put into global buffer.
          | 
       |
| void | RETARGET_SerialCrLf (int on) | 
| 
         UART/LEUART toggle LF to CRLF conversion.
          | 
       |
| bool | RETARGET_SerialEnableFlowControl (void) | 
| 
         Enable hardware flow control. (RTS + CTS)
          | 
       |
| void | RETARGET_SerialFlush (void) | 
| 
         Flush UART/LEUART.
          | 
       |
| void | RETARGET_SerialInit (void) | 
| 
         Intializes UART/LEUART.
          | 
       |
| int | RETARGET_WriteChar (char c) | 
| 
         Transmit single byte to USART/LEUART.
          | 
       |
         Variables | 
       |
| static bool | initialized = false | 
| static uint8_t | LFtoCRLF = 0 | 
| static volatile uint8_t | rxBuffer [ RXBUFSIZE ] | 
| static volatile int | rxCount = 0 | 
| static volatile int | rxReadIndex = 0 | 
| static volatile int | rxWriteIndex = 0 |