CANEMLIB
Detailed Description
Controller Area Network API.
The Controller Area Network Interface Bus (CAN) implements a multi-master serial bus for connecting microcontrollers and devices, also known as nodes, to communicate with each other in applications without a host computer. CAN is a message-based protocol, designed originally for automotive applications, but also used in many other scenarios. The complexity of a node can range from a simple I/O device up to an embedded computer with a CAN interface and sophisticated software. The node may also be a gateway allowing a standard computer to communicate over a USB or Ethernet port to the devices on a CAN network. Devices are connected to the bus through a host processor, a CAN controller, and a CAN transceiver.
em_can.h
"
em_cmu.h
"
em_gpio.h
"
Data Structures |
|
struct | CAN_Init_TypeDef |
struct | CAN_MessageObject_TypeDef |
Macros |
|
#define | CAN_INIT_DEFAULT |
Enumerations |
|
enum |
CAN_ErrorCode_TypeDef
{
canErrorNoError = CAN_STATUS_LEC_NONE, canErrorStuff = CAN_STATUS_LEC_STUFF, canErrorForm = CAN_STATUS_LEC_FORM, canErrorAck = CAN_STATUS_LEC_ACK, canErrorBit1 = CAN_STATUS_LEC_BIT1, canErrorBit0 = CAN_STATUS_LEC_BIT0, canErrorCrc = CAN_STATUS_LEC_CRC, canErrorUnused = CAN_STATUS_LEC_UNUSED } |
enum |
CAN_Mode_TypeDef
{
canModeNormal , canModeBasic , canModeLoopBack , canModeSilentLoopBack , canModeSilent } |
Functions |
|
void | CAN_AbortSendMessage ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
Abort sending a message.
|
|
void | CAN_ConfigureMessageObject ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool valid, bool tx, bool remoteTransfer, bool endOfBuffer, bool wait) |
Configure valid, TX/RX, remoteTransfer for a specific Message Object.
|
|
__STATIC_INLINE void | CAN_Enable ( CAN_TypeDef *can, bool enable) |
Enable the Host Controller to send messages.
|
|
uint32_t | CAN_GetClockFrequency ( CAN_TypeDef *can) |
Get the CAN module frequency.
|
|
__STATIC_INLINE uint32_t | CAN_GetErrorCount ( CAN_TypeDef *can) |
Get the error count.
|
|
__STATIC_INLINE CAN_ErrorCode_TypeDef | CAN_GetLastErrorCode ( CAN_TypeDef *can) |
Get the last error code and clear its register.
|
|
__STATIC_INLINE uint32_t | CAN_HasNewdata ( CAN_TypeDef *can) |
Indicates which message objects have received new data.
|
|
void | CAN_Init ( CAN_TypeDef *can, const CAN_Init_TypeDef *init) |
Initialize CAN.
|
|
__STATIC_INLINE bool | CAN_IsEnabled ( CAN_TypeDef *can) |
Give the communication capabilities state.
|
|
__STATIC_INLINE void | CAN_MessageIntClear ( CAN_TypeDef *can, uint32_t flags) |
Clear one or more pending CAN message interrupts.
|
|
__STATIC_INLINE void | CAN_MessageIntDisable ( CAN_TypeDef *can, uint32_t flags) |
Disable CAN message interrupts.
|
|
__STATIC_INLINE void | CAN_MessageIntEnable ( CAN_TypeDef *can, uint32_t flags) |
Enable CAN message interrupts.
|
|
__STATIC_INLINE uint32_t | CAN_MessageIntGet ( CAN_TypeDef *can) |
Get pending CAN message interrupt flags.
|
|
__STATIC_INLINE uint32_t | CAN_MessageIntGetEnabled ( CAN_TypeDef *can) |
Get CAN message interrupt flags that are pending and enabled.
|
|
__STATIC_INLINE void | CAN_MessageIntSet ( CAN_TypeDef *can, uint32_t flags) |
Set one or more CAN message interrupts.
|
|
bool | CAN_MessageLost ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum) |
Read a Message Object to find if a message was lost ; reset the 'Message Lost' flag.
|
|
void | CAN_ReadMessage ( CAN_TypeDef *can, uint8_t interface, CAN_MessageObject_TypeDef *message) |
Read data from a Message Object in RAM and store it in a message.
|
|
__STATIC_INLINE void | CAN_ReadyWait ( CAN_TypeDef *can, uint8_t interface) |
Waiting function.
|
|
void | CAN_Reset ( CAN_TypeDef *can) |
Set all CAN registers to RESETVALUE. Leave the CAN device disabled.
|
|
void | CAN_ResetMessages ( CAN_TypeDef *can, uint8_t interface) |
Reset all Message Objects and set their data to 0.
|
|
void | CAN_SendMessage ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message, bool wait) |
Send data from the Message Object message.
|
|
void | CAN_SendRequest ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
Send a request for writing or reading RAM of the Message Object msgNum.
|
|
void | CAN_SetBitTiming ( CAN_TypeDef *can, uint32_t bitrate, uint16_t propagationTimeSegment, uint16_t phaseBufferSegment1, uint16_t phaseBufferSegment2, uint16_t synchronisationJumpWidth) |
Set the bitrate and its parameters.
|
|
void | CAN_SetIdAndFilter ( CAN_TypeDef *can, uint8_t interface, bool useMask, const CAN_MessageObject_TypeDef *message, bool wait) |
Set the ID and the filter for a specific Message Object.
|
|
void | CAN_SetMode ( CAN_TypeDef *can, CAN_Mode_TypeDef mode) |
Set the CAN operation mode.
|
|
void | CAN_SetRoute ( CAN_TypeDef *can, bool active, uint16_t pinRxLoc, uint16_t pinTxLoc) |
Set the ROUTE registers.
|
|
__STATIC_INLINE void | CAN_StatusClear ( CAN_TypeDef *can, uint32_t flags) |
Clear CAN status.
|
|
__STATIC_INLINE uint32_t | CAN_StatusGet ( CAN_TypeDef *can) |
Get CAN status.
|
|
__STATIC_INLINE void | CAN_StatusIntClear ( CAN_TypeDef *can, uint32_t flags) |
Clear one or more pending CAN status interrupts.
|
|
__STATIC_INLINE void | CAN_StatusIntDisable ( CAN_TypeDef *can, uint32_t flags) |
Disable CAN status interrupts.
|
|
__STATIC_INLINE void | CAN_StatusIntEnable ( CAN_TypeDef *can, uint32_t flags) |
Enable CAN status interrupts.
|
|
__STATIC_INLINE uint32_t | CAN_StatusIntGet ( CAN_TypeDef *can) |
Get pending CAN status interrupt flags.
|
|
__STATIC_INLINE uint32_t | CAN_StatusIntGetEnabled ( CAN_TypeDef *can) |
Get pending and enabled CAN status interrupt flags.
|
|
__STATIC_INLINE void | CAN_StatusIntSet ( CAN_TypeDef *can, uint32_t flags) |
Set one or more CAN status interrupts.
|
|
void | CAN_WriteData ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message) |
Write data from a message to the MIRx registers.
|
|
Macro Definition Documentation
#define CAN_INIT_DEFAULT |
Default initialization of CAN_Init_TypeDef . The total duration of a bit with these default parameters is 10 tq (time quantum : tq = brp/fsys, brp being the baudrate prescaler and being set according to the wanted bitrate, fsys beeing the CAN device frequency).
Definition at line
184
of file
em_can.h
.
Enumeration Type Documentation
CAN Status codes.
Definition at line
64
of file
em_can.h
.
enum CAN_Mode_TypeDef |
CAN peripheral mode.
Definition at line
94
of file
em_can.h
.
Function Documentation
void CAN_AbortSendMessage | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
uint8_t |
msgNum,
|
||
bool |
wait
|
||
) |
Abort sending a message.
Set the TXRQST of the CTRL register to 0. Doesn't touch data or the other parameters. The user can call CAN_SendMessage() to send the object after using CAN_AbortSendMessage() .
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] msgNum
A message number of this Message Object, [1 - 32]. [in] wait
If true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately. The transfer can still be in progress.
Definition at line
732
of file
em_can.c
.
References _CAN_MIR_CTRL_TXRQST_MASK , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_WRRD , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , and CAN_TypeDef::MIR .
void CAN_ConfigureMessageObject | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
uint8_t |
msgNum,
|
||
bool |
valid,
|
||
bool |
tx,
|
||
bool |
remoteTransfer,
|
||
bool |
endOfBuffer,
|
||
bool |
wait
|
||
) |
Configure valid, TX/RX, remoteTransfer for a specific Message Object.
The initialization bit has to be 0 to use this function.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] msgNum
A message number of this Message Object, [1 - 32]. [in] valid
True if the Message Object is valid, false otherwise. [in] tx
True if the Message Object is used for transmission, false if used for reception. [in] remoteTransfer
True if the Message Object is used for remote transmission, false otherwise. [in] endOfBuffer
True if it is for a single Message Object or the end of a FIFO buffer, false if the Message Object is part of a FIFO buffer and not the last. [in] wait
If true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
504
of file
em_can.c
.
References _CAN_MIR_ARB_DIR_MASK , _CAN_MIR_ARB_DIR_SHIFT , _CAN_MIR_ARB_MSGVAL_MASK , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_CTRL_EOB_SHIFT , _CAN_MIR_CTRL_RMTEN_SHIFT , _CAN_MIR_CTRL_RXIE_MASK , _CAN_MIR_CTRL_TXIE_MASK , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , and CAN_TypeDef::MIR .
__STATIC_INLINE void CAN_Enable | ( | CAN_TypeDef * |
can,
|
bool |
enable
|
||
) |
Enable the Host Controller to send messages.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] enable
True to enable CAN device, false to disable it. If the CAN device is enabled, it goes to normal mode (the default working mode).
Definition at line
272
of file
em_can.h
.
References _CAN_CTRL_INIT_SHIFT , BUS_RegBitWrite() , and CAN_TypeDef::CTRL .
Referenced by CAN_Init() , and CAN_Reset() .
uint32_t CAN_GetClockFrequency | ( | CAN_TypeDef * |
can
|
) |
Get the CAN module frequency.
An internal prescaler of 2 is inside the CAN module.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- A clock value.
Definition at line
132
of file
em_can.c
.
References CAN0 , CAN1 , CMU_ClockFreqGet() , cmuClock_CAN0 , and cmuClock_CAN1 .
Referenced by CAN_SetBitTiming() .
__STATIC_INLINE uint32_t CAN_GetErrorCount | ( | CAN_TypeDef * |
can
|
) |
Get the error count.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- Error count.
Definition at line
483
of file
em_can.h
.
References CAN_TypeDef::ERRCNT .
__STATIC_INLINE CAN_ErrorCode_TypeDef CAN_GetLastErrorCode | ( | CAN_TypeDef * |
can
|
) |
Get the last error code and clear its register.
- Parameters
-
[in] can
Pointer to CAN peripheral register block.
- Returns
- return Last error code.
Definition at line
320
of file
em_can.h
.
References _CAN_STATUS_LEC_MASK , and CAN_TypeDef::STATUS .
__STATIC_INLINE uint32_t CAN_HasNewdata | ( | CAN_TypeDef * |
can
|
) |
Indicates which message objects have received new data.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- State of MESSAGEDATA register indicating which message objects have received new data.
Definition at line
339
of file
em_can.h
.
References CAN_TypeDef::MESSAGEDATA .
void CAN_Init | ( | CAN_TypeDef * |
can,
|
const CAN_Init_TypeDef * |
init
|
||
) |
Initialize CAN.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] init
A pointer to the CAN initialization structure.
Definition at line
99
of file
em_can.c
.
References _CAN_CTRL_TEST_MASK , _CAN_TEST_RESETVALUE , CAN_Init_TypeDef::bitrate , CAN_CTRL_INIT , CAN_Enable() , CAN_ResetMessages() , CAN_SetBitTiming() , CAN_TypeDef::CTRL , CAN_Init_TypeDef::enable , CAN_Init_TypeDef::phaseBufferSegment1 , CAN_Init_TypeDef::phaseBufferSegment2 , CAN_Init_TypeDef::propagationTimeSegment , CAN_Init_TypeDef::resetMessages , CAN_Init_TypeDef::synchronisationJumpWidth , and CAN_TypeDef::TEST .
__STATIC_INLINE bool CAN_IsEnabled | ( | CAN_TypeDef * |
can
|
) |
Give the communication capabilities state.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- True if the Host Controller can send messages, false otherwise.
Definition at line
287
of file
em_can.h
.
References _CAN_CTRL_INIT_MASK , and CAN_TypeDef::CTRL .
Referenced by CAN_SetBitTiming() .
__STATIC_INLINE void CAN_MessageIntClear | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Clear one or more pending CAN message interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
Pending CAN message interrupt source(s) to clear.
Definition at line
498
of file
em_can.h
.
References CAN_TypeDef::IF0IFC .
__STATIC_INLINE void CAN_MessageIntDisable | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Disable CAN message interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
CAN message interrupt source(s) to disable.
Definition at line
513
of file
em_can.h
.
References CAN_TypeDef::IF0IEN .
__STATIC_INLINE void CAN_MessageIntEnable | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Enable CAN message interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
CAN message interrupt source(s) to enable.
Definition at line
528
of file
em_can.h
.
References CAN_TypeDef::IF0IEN .
__STATIC_INLINE uint32_t CAN_MessageIntGet | ( | CAN_TypeDef * |
can
|
) |
Get pending CAN message interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- CAN message interrupt source(s) pending.
Definition at line
546
of file
em_can.h
.
References CAN_TypeDef::IF0IF .
__STATIC_INLINE uint32_t CAN_MessageIntGetEnabled | ( | CAN_TypeDef * |
can
|
) |
Get CAN message interrupt flags that are pending and enabled.
- Note
- This function does not clear event bits.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- CAN message interrupt source(s) pending and enabled.
Definition at line
564
of file
em_can.h
.
References CAN_TypeDef::IF0IEN , and CAN_TypeDef::IF0IF .
__STATIC_INLINE void CAN_MessageIntSet | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Set one or more CAN message interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
CAN message interrupt source(s) to set as pending.
Definition at line
582
of file
em_can.h
.
References CAN_TypeDef::IF0IFS .
bool CAN_MessageLost | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
uint8_t |
msgNum
|
||
) |
Read a Message Object to find if a message was lost ; reset the 'Message Lost' flag.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] msgNum
A message number of the Message Object, [1 - 32].
- Returns
- True if a message was lost, false otherwise.
Definition at line
166
of file
em_can.c
.
References _CAN_MIR_CTRL_MESSAGEOF_MASK , CAN_MIR_CMDMASK_CLRINTPND , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , and CAN_TypeDef::MIR .
void CAN_ReadMessage | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
CAN_MessageObject_TypeDef * |
message
|
||
) |
Read data from a Message Object in RAM and store it in a message.
Read the information from RAM on this Message Object : data but also the configuration of the other registers.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] message
A Message Object.
Definition at line
662
of file
em_can.c
.
References _CAN_MIR_CTRL_DLC_MASK , _CAN_MIR_CTRL_DLC_SHIFT , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CLRINTPND , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_TXRQSTNEWDAT , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::data , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MessageObject_TypeDef::dlc , CAN_TypeDef::MIR , CAN_MessageObject_TypeDef::msgNum , and SL_MIN .
__STATIC_INLINE void CAN_ReadyWait | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface
|
||
) |
Waiting function.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use.
Definition at line
303
of file
em_can.h
.
References _CAN_MIR_CMDREQ_BUSY_MASK , CAN_MIR_TypeDef::CMDREQ , and CAN_TypeDef::MIR .
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_Reset() , CAN_ResetMessages() , CAN_SendMessage() , CAN_SendRequest() , CAN_SetIdAndFilter() , and CAN_WriteData() .
void CAN_Reset | ( | CAN_TypeDef * |
can
|
) |
Set all CAN registers to RESETVALUE. Leave the CAN device disabled.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
Definition at line
796
of file
em_can.c
.
References _CAN_BITTIMING_RESETVALUE , _CAN_BRPE_RESETVALUE , _CAN_CONFIG_RESETVALUE , _CAN_CTRL_CCE_MASK , _CAN_CTRL_TEST_MASK , _CAN_IF0IEN_RESETVALUE , _CAN_IF0IFC_RESETVALUE , _CAN_IF0IFS_RESETVALUE , _CAN_IF1IEN_RESETVALUE , _CAN_IF1IF_RESETVALUE , _CAN_IF1IFC_RESETVALUE , _CAN_MIR_ARB_RESETVALUE , _CAN_MIR_CMDMASK_RESETVALUE , _CAN_MIR_CMDREQ_RESETVALUE , _CAN_MIR_CTRL_RESETVALUE , _CAN_MIR_DATAH_RESETVALUE , _CAN_MIR_DATAL_RESETVALUE , _CAN_MIR_MASK_RESETVALUE , _CAN_ROUTE_RESETVALUE , _CAN_STATUS_RESETVALUE , _CAN_TEST_RESETVALUE , CAN_MIR_TypeDef::ARB , CAN_TypeDef::BITTIMING , CAN_TypeDef::BRPE , CAN_Enable() , CAN_ReadyWait() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CMDREQ , CAN_TypeDef::CONFIG , CAN_TypeDef::CTRL , CAN_MIR_TypeDef::CTRL , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_TypeDef::IF0IEN , CAN_TypeDef::IF0IFC , CAN_TypeDef::IF0IFS , CAN_TypeDef::IF1IEN , CAN_TypeDef::IF1IFC , CAN_TypeDef::IF1IFS , CAN_MIR_TypeDef::MASK , CAN_TypeDef::MIR , CAN_TypeDef::ROUTE , CAN_TypeDef::STATUS , and CAN_TypeDef::TEST .
void CAN_ResetMessages | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface
|
||
) |
Reset all Message Objects and set their data to 0.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use.
Definition at line
764
of file
em_can.c
.
References _CAN_MIR_ARB_RESETVALUE , _CAN_MIR_CTRL_RESETVALUE , _CAN_MIR_MASK_RESETVALUE , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_WRRD , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MIR_TypeDef::MASK , and CAN_TypeDef::MIR .
Referenced by CAN_Init() .
void CAN_SendMessage | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
const CAN_MessageObject_TypeDef * |
message,
|
||
bool |
wait
|
||
) |
Send data from the Message Object message.
If the message is configured as TX and remoteTransfer = 0, calling this function will send the data of this Message Object if its parameters are correct. If the message is TX and remoteTransfer = 1, this function will set the data of message to RAM and exit. Data will be automatically sent after reception of a remote frame. If the message is RX and remoteTransfer = 1, this function will send a remote frame to the corresponding ID. If the message is RX and remoteTransfer = 0, the user shouldn't call this function. It will also send a remote frame.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] message
A Message Object. [in] wait
If true, wait for the end of the transfer between the MIRx registers and RAM to exit. If false, exit immediately. The transfer can still be in progress.
Definition at line
575
of file
em_can.c
.
References _CAN_MIR_ARB_DIR_MASK , _CAN_MIR_ARB_DIR_RX , _CAN_MIR_ARB_ID_MASK , _CAN_MIR_ARB_ID_SHIFT , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_ARB_XTD_MASK , _CAN_MIR_CTRL_DLC_MASK , _CAN_MIR_CTRL_RMTEN_MASK , _CAN_STATUS_LEC_MASK , CAN_MIR_TypeDef::ARB , BUS_RegMaskedWrite() , CAN_MIR_ARB_XTD_EXT , CAN_MIR_ARB_XTD_STD , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_MIR_CTRL_DATAVALID , CAN_MIR_CTRL_TXRQST , CAN_ReadyWait() , CAN_SendRequest() , CAN_WriteData() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::dlc , CAN_MessageObject_TypeDef::extended , CAN_MessageObject_TypeDef::id , CAN_TypeDef::MIR , CAN_MessageObject_TypeDef::msgNum , and CAN_TypeDef::STATUS .
void CAN_SendRequest | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
uint8_t |
msgNum,
|
||
bool |
wait
|
||
) |
Send a request for writing or reading RAM of the Message Object msgNum.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] msgNum
A message number of the Message Object, [1 - 32]. [in] wait
If true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately. The transfer can still be in progress.
Definition at line
892
of file
em_can.c
.
References _CAN_MIR_CMDREQ_MSGNUM_SHIFT , CAN_ReadyWait() , CAN_MIR_TypeDef::CMDREQ , and CAN_TypeDef::MIR .
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_ResetMessages() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
void CAN_SetBitTiming | ( | CAN_TypeDef * |
can,
|
uint32_t |
bitrate,
|
||
uint16_t |
propagationTimeSegment,
|
||
uint16_t |
phaseBufferSegment1,
|
||
uint16_t |
phaseBufferSegment2,
|
||
uint16_t |
synchronisationJumpWidth
|
||
) |
Set the bitrate and its parameters.
Multiple parameters need to be properly configured. See the reference manual for a detailed description. Careful : the BRP (Baud Rate Prescaler) is calculated by: 'brp = freq / (period * bitrate);'. freq is the frequency of the CAN device, period the time of transmission of a bit. The result is an uint32_t. Hence it's truncated, causing an approximation error. This error is non negligible when the period is high, the bitrate is high, and frequency is low.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] bitrate
A wanted bitrate on the CAN bus. [in] propagationTimeSegment
A value for the Propagation Time Segment. [in] phaseBufferSegment1
A value for the Phase Buffer Segment 1. [in] phaseBufferSegment2
A value for the Phase Buffer Segment 2. [in] synchronisationJumpWidth
A value for the Synchronization Jump Width.
Definition at line
263
of file
em_can.c
.
References _CAN_BITTIMING_BRP_SHIFT , _CAN_BITTIMING_SJW_SHIFT , _CAN_BITTIMING_TSEG1_SHIFT , _CAN_BITTIMING_TSEG2_SHIFT , _CAN_CTRL_CCE_MASK , _CAN_CTRL_INIT_MASK , CAN_TypeDef::BITTIMING , CAN_TypeDef::BRPE , CAN_CTRL_CCE , CAN_CTRL_INIT , CAN_GetClockFrequency() , CAN_IsEnabled() , and CAN_TypeDef::CTRL .
Referenced by CAN_Init() .
void CAN_SetIdAndFilter | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
bool |
useMask,
|
||
const CAN_MessageObject_TypeDef * |
message,
|
||
bool |
wait
|
||
) |
Set the ID and the filter for a specific Message Object.
The initialization bit has to be 0 to use this function.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] useMask
A boolean to choose whether or not to use the masks. [in] message
A Message Object. [in] wait
If true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
409
of file
em_can.c
.
References _CAN_MIR_ARB_ID_MASK , _CAN_MIR_ARB_ID_SHIFT , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_CTRL_UMASK_SHIFT , _CAN_MIR_MASK_MASK_SHIFT , _CAN_MIR_MASK_MDIR_SHIFT , _CAN_MIR_MASK_MXTD_SHIFT , CAN_MIR_TypeDef::ARB , BUS_RegBitWrite() , CAN_MIR_ARB_XTD_EXT , CAN_MIR_ARB_XTD_STD , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::directionMask , CAN_MessageObject_TypeDef::extended , CAN_MessageObject_TypeDef::extendedMask , CAN_MessageObject_TypeDef::id , CAN_MIR_TypeDef::MASK , CAN_MessageObject_TypeDef::mask , CAN_TypeDef::MIR , and CAN_MessageObject_TypeDef::msgNum .
void CAN_SetMode | ( | CAN_TypeDef * |
can,
|
CAN_Mode_TypeDef |
mode
|
||
) |
Set the CAN operation mode.
In initialization mode, the CAN module is deactivated. Reset the messages in all other modes to be sure that there is no leftover data that needs to be configured before use.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] mode
Mode of operation : Init, Normal, Loopback, SilentLoopback, Silent, Basic.
Definition at line
335
of file
em_can.c
.
References _CAN_CTRL_EIE_MASK , _CAN_CTRL_IE_MASK , _CAN_CTRL_SIE_MASK , _CAN_CTRL_TEST_MASK , _CAN_TEST_RESETVALUE , CAN_CTRL_TEST , CAN_TEST_BASIC , CAN_TEST_LBACK , CAN_TEST_SILENT , canModeBasic , canModeLoopBack , canModeNormal , canModeSilent , canModeSilentLoopBack , CAN_TypeDef::CTRL , and CAN_TypeDef::TEST .
void CAN_SetRoute | ( | CAN_TypeDef * |
can,
|
bool |
active,
|
||
uint16_t |
pinRxLoc,
|
||
uint16_t |
pinTxLoc
|
||
) |
Set the ROUTE registers.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] active
A boolean indicating whether or not to activate the ROUTE registers. [in] pinRxLoc
A location of the RX pin. [in] pinTxLoc
A location of the TX pin.
Definition at line
216
of file
em_can.c
.
References _CAN_ROUTE_RXLOC_SHIFT , _CAN_ROUTE_TXLOC_SHIFT , CAN_ROUTE_TXPEN , and CAN_TypeDef::ROUTE .
__STATIC_INLINE void CAN_StatusClear | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Clear CAN status.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
CAN status bits to clear.
Definition at line
468
of file
em_can.h
.
References CAN_TypeDef::STATUS .
__STATIC_INLINE uint32_t CAN_StatusGet | ( | CAN_TypeDef * |
can
|
) |
Get CAN status.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- A value of CAN register STATUS.
Definition at line
453
of file
em_can.h
.
References _CAN_STATUS_LEC_MASK , and CAN_TypeDef::STATUS .
__STATIC_INLINE void CAN_StatusIntClear | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Clear one or more pending CAN status interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
Pending CAN status interrupt source(s) to clear.
Definition at line
354
of file
em_can.h
.
References CAN_TypeDef::IF1IFC .
__STATIC_INLINE void CAN_StatusIntDisable | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Disable CAN status interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
CAN status interrupt source(s) to disable.
Definition at line
369
of file
em_can.h
.
References CAN_TypeDef::IF1IEN .
__STATIC_INLINE void CAN_StatusIntEnable | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Enable CAN status interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
CAN status interrupt source(s) to enable.
Definition at line
384
of file
em_can.h
.
References CAN_TypeDef::IF1IEN .
__STATIC_INLINE uint32_t CAN_StatusIntGet | ( | CAN_TypeDef * |
can
|
) |
Get pending CAN status interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- CAN interrupt source(s) pending.
Definition at line
402
of file
em_can.h
.
References CAN_TypeDef::IF1IF .
__STATIC_INLINE uint32_t CAN_StatusIntGetEnabled | ( | CAN_TypeDef * |
can
|
) |
Get pending and enabled CAN status interrupt flags.
- Note
- This function does not clear event bits.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block.
- Returns
- CAN interrupt source(s) pending and enabled.
Definition at line
420
of file
em_can.h
.
References CAN_TypeDef::IF1IEN , and CAN_TypeDef::IF1IF .
__STATIC_INLINE void CAN_StatusIntSet | ( | CAN_TypeDef * |
can,
|
uint32_t |
flags
|
||
) |
Set one or more CAN status interrupts.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] flags
CAN status interrupt source(s) to set to pending.
Definition at line
438
of file
em_can.h
.
References CAN_TypeDef::IF1IFS .
void CAN_WriteData | ( | CAN_TypeDef * |
can,
|
uint8_t |
interface,
|
||
const CAN_MessageObject_TypeDef * |
message
|
||
) |
Write data from a message to the MIRx registers.
- Parameters
-
[in] can
A pointer to the CAN peripheral register block. [in] interface
Indicate which Message Interface Register to use. [in] message
A Message Object.
Definition at line
846
of file
em_can.c
.
References CAN_ReadyWait() , CAN_MessageObject_TypeDef::data , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MessageObject_TypeDef::dlc , CAN_TypeDef::MIR , and SL_MIN .
Referenced by CAN_SendMessage() .