CHIPEMLIB
Detailed Description
Chip errata workarounds initialization API.
API to initialize chip for errata workarounds.
Functions | |
__STATIC_INLINE void | CHIP_Init (void) |
Chip initialization routine for revision errata workarounds. | |
Function Documentation
__STATIC_INLINE void CHIP_Init | ( | void |
| ) |
Chip initialization routine for revision errata workarounds.
- Note
- This function must be called immediately in main().
This initialization function configures the device to a state as similar to later revisions as possible to improve software compatibility with newer parts. See the device-specific errata for details.
Definition at line 68
of file em_chip.h
.
References _CMU_HFXOSTARTUPCTRL_IBTRIMXOCORE_MASK, _CMU_HFXOSTARTUPCTRL_IBTRIMXOCORE_SHIFT, _CMU_LFRCOCTRL_VREFUPDATE_MASK, _EMU_DCDCCLIMCTRL_BYPLIMEN_SHIFT, _GPIO_P_CTRL_RESETVALUE, _GPIO_P_CTRL_SLEWRATE_MASK, _GPIO_P_CTRL_SLEWRATE_SHIFT, _GPIO_P_CTRL_SLEWRATEALT_MASK, _GPIO_P_CTRL_SLEWRATEALT_SHIFT, BUS_RegBitWrite(), CMU, CMU_HFBUSCLKEN0_GPIO, CMU_HFBUSCLKEN0_LE, CMU_LFACLKEN0_LCD, CMU_LFRCOCTRL_ENVREF, CMU_LFRCOCTRL_VREFUPDATE_64CYCLES, EMU, EMU_BASE, GPIO, LCD_BASE, SYSTEM_ChipRevision_TypeDef::major, SYSTEM_ChipRevision_TypeDef::minor, MSC, MSC_CACHECMD_INVCACHE, SYSTEM_ChipRevisionGet(), and SYSTEM_GetProdRev().
Referenced by BSP_initDevice().