ACMP_VBConfig_TypeDef Struct ReferenceEMLIB > ACMP
VB Configuration structure. This structure is used to configure the VB voltage input source and its dividers.
Definition at line 907
of file em_acmp.h
.
#include <
em_acmp.h
>
Data Fields | |
uint32_t | div0 |
uint32_t | div1 |
ACMP_VBInput_TypeDef | input |
Field Documentation
uint32_t ACMP_VBConfig_TypeDef::div0 |
A divider for VB voltage input source when ACMP output is 0. This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div0 + 1) / 64
Definition at line 917
of file em_acmp.h
.
Referenced by ACMP_VBSetup().
uint32_t ACMP_VBConfig_TypeDef::div1 |
A divider for VB voltage input source when ACMP output is 1. This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div1 + 1) / 64
Definition at line 926
of file em_acmp.h
.
Referenced by ACMP_VBSetup().
ACMP_VBInput_TypeDef ACMP_VBConfig_TypeDef::input |
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_acmp.h