FPUEH_TypeDef Struct ReferenceDevices > FPUEH
FPUEH Register Declaration
Definition at line
48
of file
efm32gg12b_fpueh.h
.
#include <
efm32gg12b_fpueh.h
>
Data Fields |
|
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
Field Documentation
| __IOM uint32_t FPUEH_TypeDef::IEN |
Interrupt Enable Register
Definition at line
52
of file
efm32gg12b_fpueh.h
.
| __IM uint32_t FPUEH_TypeDef::IF |
Interrupt Flag Register
Definition at line
49
of file
efm32gg12b_fpueh.h
.
| __IOM uint32_t FPUEH_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
51
of file
efm32gg12b_fpueh.h
.
| __IOM uint32_t FPUEH_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
50
of file
efm32gg12b_fpueh.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32GG12B/Include/
efm32gg12b_fpueh.h