EMU_TypeDef Struct ReferenceDevices > EMU
EMU Register Declaration
Definition at line
48
of file
efm32gg12b_emu.h
.
#include <
efm32gg12b_emu.h
>
Data Fields |
|
| __IOM uint32_t | BUCTRL |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | DCDCCLIMCTRL |
| __IOM uint32_t | DCDCCTRL |
| __IOM uint32_t | DCDCLNCOMPCTRL |
| __IOM uint32_t | DCDCLNFREQCTRL |
| __IOM uint32_t | DCDCLNVCTRL |
| __IOM uint32_t | DCDCLPCTRL |
| __IOM uint32_t | DCDCLPEM01CFG |
| __IOM uint32_t | DCDCLPVCTRL |
| __IOM uint32_t | DCDCMISCCTRL |
| __IM uint32_t | DCDCSYNC |
| __IOM uint32_t | DCDCZDETCTRL |
| __IOM uint32_t | EM23PERNORETAINCMD |
| __IOM uint32_t | EM23PERNORETAINCTRL |
| __IM uint32_t | EM23PERNORETAINSTATUS |
| __IOM uint32_t | EM4CTRL |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | LOCK |
| __IOM uint32_t | PWRCTRL |
| __IOM uint32_t | PWRLOCK |
| __IOM uint32_t | R5VADCCTRL |
| __IOM uint32_t | R5VCTRL |
| __IOM uint32_t | R5VDETCTRL |
| __IOM uint32_t | R5VOUTLEVEL |
| __IM uint32_t | R5VSTATUS |
| __IM uint32_t | R5VSYNC |
| __IOM uint32_t | RAM0CTRL |
| __IOM uint32_t | RAM1CTRL |
| __IOM uint32_t | RAM2CTRL |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [1U] |
| uint32_t | RESERVED10 [3U] |
| uint32_t | RESERVED11 [1U] |
| uint32_t | RESERVED12 [1U] |
| uint32_t | RESERVED2 [2U] |
| uint32_t | RESERVED3 [1U] |
| uint32_t | RESERVED4 [1U] |
| uint32_t | RESERVED5 [1U] |
| uint32_t | RESERVED6 [5U] |
| uint32_t | RESERVED7 [3U] |
| uint32_t | RESERVED8 [2U] |
| uint32_t | RESERVED9 [2U] |
| __IM uint32_t | STATUS |
| __IM uint32_t | TEMP |
| __IOM uint32_t | TEMPLIMITS |
| __IOM uint32_t | VMONALTAVDDCTRL |
| __IOM uint32_t | VMONAVDDCTRL |
| __IOM uint32_t | VMONBUVDDCTRL |
| __IOM uint32_t | VMONDVDDCTRL |
| __IOM uint32_t | VMONIO0CTRL |
| __IOM uint32_t | VMONIO1CTRL |
Field Documentation
| __IOM uint32_t EMU_TypeDef::BUCTRL |
Backup Power Configuration Register
Definition at line
97
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::CMD |
Command Register
Definition at line
53
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::CTRL |
Control Register
Definition at line
49
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCCLIMCTRL |
DCDC Power Train PFET Current Limiter Control Register
Definition at line
72
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCCTRL |
DCDC Control
Definition at line
67
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCLNCOMPCTRL |
DCDC Low Noise Compensator Control Register
Definition at line
73
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCLNFREQCTRL |
DCDC Low Noise Controller Frequency Control
Definition at line
81
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCLNVCTRL |
DCDC Low Noise Voltage Register
Definition at line
74
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCLPCTRL |
DCDC Low Power Control Register
Definition at line
80
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCLPEM01CFG |
Configuration Bits for Low Power Mode to Be Applied During EM01, This Field is Only Relevant If LP Mode is Used in EM01
Definition at line
107
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCLPVCTRL |
DCDC Low Power Voltage Register
Definition at line
77
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCMISCCTRL |
DCDC Miscellaneous Control Register
Definition at line
70
of file
efm32gg12b_emu.h
.
| __IM uint32_t EMU_TypeDef::DCDCSYNC |
DCDC Read Status Register
Definition at line
84
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::DCDCZDETCTRL |
DCDC Power Train NFET Zero Current Detector Control Register
Definition at line
71
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::EM23PERNORETAINCMD |
Clears Corresponding Bits in EM23PERNORETAINSTATUS Unlocking Access to Peripheral
Definition at line
114
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::EM23PERNORETAINCTRL |
When Set Corresponding Peripherals May Get Powered Down in EM23
Definition at line
116
of file
efm32gg12b_emu.h
.
| __IM uint32_t EMU_TypeDef::EM23PERNORETAINSTATUS |
Status Indicating If Peripherals Were Powered Down in EM23, Subsequently Locking Access to It
Definition at line
115
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::EM4CTRL |
EM4 Control Register
Definition at line
56
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line
62
of file
efm32gg12b_emu.h
.
| __IM uint32_t EMU_TypeDef::IF |
Interrupt Flag Register
Definition at line
59
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
61
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
60
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line
51
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::PWRCTRL |
Power Control Register
Definition at line
66
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::PWRLOCK |
Regulator and Supply Lock Register
Definition at line
63
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::R5VADCCTRL |
5V Regulator Control
Definition at line
100
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::R5VCTRL |
5V Regulator Control
Definition at line
99
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::R5VDETCTRL |
5V Detector Enables
Definition at line
104
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::R5VOUTLEVEL |
5V Regulator Voltage Select
Definition at line
101
of file
efm32gg12b_emu.h
.
| __IM uint32_t EMU_TypeDef::R5VSTATUS |
5V Detector Status Register
Definition at line
108
of file
efm32gg12b_emu.h
.
| __IM uint32_t EMU_TypeDef::R5VSYNC |
5V Read Status Register
Definition at line
111
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::RAM0CTRL |
Memory Control Register
Definition at line
52
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::RAM1CTRL |
Memory Control Register
Definition at line
95
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::RAM2CTRL |
Memory Control Register
Definition at line
96
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
55
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
65
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED10[3U] |
Reserved for future use
Definition at line
106
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED11[1U] |
Reserved for future use
Definition at line
110
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED12[1U] |
Reserved for future use
Definition at line
113
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED2[2U] |
Reserved for future use
Definition at line
69
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED3[1U] |
Reserved for future use
Definition at line
76
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED4[1U] |
Reserved for future use
Definition at line
79
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED5[1U] |
Reserved for future use
Definition at line
83
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED6[5U] |
Reserved for future use
Definition at line
86
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED7[3U] |
Reserved for future use
Definition at line
94
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED8[2U] |
Reserved for future use
Definition at line
98
of file
efm32gg12b_emu.h
.
| uint32_t EMU_TypeDef::RESERVED9[2U] |
Reserved for future use
Definition at line
103
of file
efm32gg12b_emu.h
.
| __IM uint32_t EMU_TypeDef::STATUS |
Status Register
Definition at line
50
of file
efm32gg12b_emu.h
.
| __IM uint32_t EMU_TypeDef::TEMP |
Value of Last Temperature Measurement
Definition at line
58
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::TEMPLIMITS |
Temperature Limits for Interrupt Generation
Definition at line
57
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::VMONALTAVDDCTRL |
Alternate VMON AVDD Channel Control
Definition at line
88
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::VMONAVDDCTRL |
VMON AVDD Channel Control
Definition at line
87
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::VMONBUVDDCTRL |
VMON BUVDD Channel Control
Definition at line
92
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::VMONDVDDCTRL |
VMON DVDD Channel Control
Definition at line
89
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::VMONIO0CTRL |
VMON IOVDD0 Channel Control
Definition at line
90
of file
efm32gg12b_emu.h
.
| __IOM uint32_t EMU_TypeDef::VMONIO1CTRL |
VMON IOVDD1 Channel Control
Definition at line
91
of file
efm32gg12b_emu.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFM32GG12B/Include/
efm32gg12b_emu.h