This module includes functions for Channel Manager.
Functions |
|
| void | otChannelManagerRequestChannelChange ( otInstance *aInstance, uint8_t aChannel) |
|
This function requests a Thread network channel change.
|
|
| uint8_t | otChannelManagerGetRequestedChannel ( otInstance *aInstance) |
This function gets the channel from the last successful call to
otChannelManagerRequestChannelChange()
|
|
| uint16_t | otChannelManagerGetDelay ( otInstance *aInstance) |
|
This function gets the delay (in seconds) used by Channel Manager for a channel change.
|
|
| otError | otChannelManagerSetDelay ( otInstance *aInstance, uint16_t aDelay) |
|
This function sets the delay (in seconds) used for a channel change.
|
|
| otError | otChannelManagerRequestChannelSelect ( otInstance *aInstance, bool aSkipQualityCheck) |
This function requests that
ChannelManager
checks and selects a new channel and starts a channel change.
|
|
| void | otChannelManagerSetAutoChannelSelectionEnabled ( otInstance *aInstance, bool aEnabled) |
|
This function enables/disables the auto-channel-selection functionality.
|
|
| bool | otChannelManagerGetAutoChannelSelectionEnabled ( otInstance *aInstance) |
|
This function indicates whether the auto-channel-selection functionality is enabled or not.
|
|
| otError | otChannelManagerSetAutoChannelSelectionInterval ( otInstance *aInstance, uint32_t aInterval) |
|
This function sets the period interval (in seconds) used by auto-channel-selection functionality.
|
|
| uint32_t | otChannelManagerGetAutoChannelSelectionInterval ( otInstance *aInstance) |
|
This function gets the period interval (in seconds) used by auto-channel-selection functionality.
|
|
| uint32_t | otChannelManagerGetSupportedChannels ( otInstance *aInstance) |
|
This function gets the supported channel mask.
|
|
| void | otChannelManagerSetSupportedChannels ( otInstance *aInstance, uint32_t aChannelMask) |
|
This function sets the supported channel mask.
|
|
| uint32_t | otChannelManagerGetFavoredChannels ( otInstance *aInstance) |
|
This function gets the favored channel mask.
|
|
| void | otChannelManagerSetFavoredChannels ( otInstance *aInstance, uint32_t aChannelMask) |
|
This function sets the favored channel mask.
|
|
| uint16_t | otChannelManagerGetCcaFailureRateThreshold ( otInstance *aInstance) |
|
This function gets the CCA failure rate threshold.
|
|
| void | otChannelManagerSetCcaFailureRateThreshold ( otInstance *aInstance, uint16_t aThreshold) |
|
This function sets the CCA failure rate threshold.
|
|
Detailed Description
This module includes functions for Channel Manager.
The functions in this module are available when Channel Manager feature (
OPENTHREAD_CONFIG_CHANNEL_MANAGER_ENABLE
) is enabled. Channel Manager is available only on an FTD build.
Function Documentation
◆ otChannelManagerGetAutoChannelSelectionEnabled()
| bool otChannelManagerGetAutoChannelSelectionEnabled | ( | otInstance * |
aInstance
|
) |
This function indicates whether the auto-channel-selection functionality is enabled or not.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- TRUE if enabled, FALSE if disabled.
◆ otChannelManagerGetAutoChannelSelectionInterval()
| uint32_t otChannelManagerGetAutoChannelSelectionInterval | ( | otInstance * |
aInstance
|
) |
This function gets the period interval (in seconds) used by auto-channel-selection functionality.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The interval in seconds.
◆ otChannelManagerGetCcaFailureRateThreshold()
| uint16_t otChannelManagerGetCcaFailureRateThreshold | ( | otInstance * |
aInstance
|
) |
This function gets the CCA failure rate threshold.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The CCA failure rate threshold. Value 0 maps to 0% and 0xffff maps to 100%.
◆ otChannelManagerGetDelay()
| uint16_t otChannelManagerGetDelay | ( | otInstance * |
aInstance
|
) |
This function gets the delay (in seconds) used by Channel Manager for a channel change.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The delay (in seconds) for channel change.
◆ otChannelManagerGetFavoredChannels()
| uint32_t otChannelManagerGetFavoredChannels | ( | otInstance * |
aInstance
|
) |
This function gets the favored channel mask.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The favored channels as a bit-mask.
◆ otChannelManagerGetRequestedChannel()
| uint8_t otChannelManagerGetRequestedChannel | ( | otInstance * |
aInstance
|
) |
This function gets the channel from the last successful call to
otChannelManagerRequestChannelChange()
- Returns
- The last requested channel or zero if there has been no channel change request yet.
◆ otChannelManagerGetSupportedChannels()
| uint32_t otChannelManagerGetSupportedChannels | ( | otInstance * |
aInstance
|
) |
This function gets the supported channel mask.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The supported channels as a bit-mask.
◆ otChannelManagerRequestChannelChange()
| void otChannelManagerRequestChannelChange | ( | otInstance * |
aInstance,
|
| uint8_t |
aChannel
|
||
| ) |
This function requests a Thread network channel change.
The network switches to the given channel after a specified delay (see otChannelManagerSetDelay() ). The channel change is performed by updating the Pending Operational Dataset.
A subsequent call to this function will cancel an ongoing previously requested channel change.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aChannelThe new channel for the Thread network.
◆ otChannelManagerRequestChannelSelect()
| otError otChannelManagerRequestChannelSelect | ( | otInstance * |
aInstance,
|
| bool |
aSkipQualityCheck
|
||
| ) |
This function requests that
ChannelManager
checks and selects a new channel and starts a channel change.
Unlike the
otChannelManagerRequestChannelChange()
where the channel must be given as a parameter, this function asks the
ChannelManager
to select a channel by itself (based of collected channel quality info).
Once called, the Channel Manager will perform the following 3 steps:
1)
ChannelManager
decides if the channel change would be helpful. This check can be skipped if
aSkipQualityCheck
is set to true (forcing a channel selection to happen and skipping the quality check). This step uses the collected link quality metrics on the device (such as CCA failure rate, frame and message error rates per neighbor, etc.) to determine if the current channel quality is at the level that justifies a channel change.
2) If the first step passes, then
ChannelManager
selects a potentially better channel. It uses the collected channel quality data by
ChannelMonitor
module. The supported and favored channels are used at this step. (see
otChannelManagerSetSupportedChannels()
and
otChannelManagerSetFavoredChannels()
).
3) If the newly selected channel is different from the current channel,
ChannelManager
requests/starts the channel change process (internally invoking a
RequestChannelChange()
).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aSkipQualityCheckIndicates whether the quality check (step 1) should be skipped.
- Return values
-
OT_ERROR_NONEChannel selection finished successfully. OT_ERROR_NOT_FOUNDSupported channel mask is empty, therefore could not select a channel.
◆ otChannelManagerSetAutoChannelSelectionEnabled()
| void otChannelManagerSetAutoChannelSelectionEnabled | ( | otInstance * |
aInstance,
|
| bool |
aEnabled
|
||
| ) |
This function enables/disables the auto-channel-selection functionality.
When enabled,
ChannelManager
will periodically invoke a
RequestChannelSelect(false)
. The period interval can be set by
SetAutoChannelSelectionInterval()
.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aEnabledIndicates whether to enable or disable this functionality.
◆ otChannelManagerSetAutoChannelSelectionInterval()
| otError otChannelManagerSetAutoChannelSelectionInterval | ( | otInstance * |
aInstance,
|
| uint32_t |
aInterval
|
||
| ) |
This function sets the period interval (in seconds) used by auto-channel-selection functionality.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aIntervalThe interval in seconds.
- Return values
-
OT_ERROR_NONEThe interval was set successfully. OT_ERROR_INVALID_ARGSThe aIntervalis not valid (zero).
◆ otChannelManagerSetCcaFailureRateThreshold()
| void otChannelManagerSetCcaFailureRateThreshold | ( | otInstance * |
aInstance,
|
| uint16_t |
aThreshold
|
||
| ) |
This function sets the CCA failure rate threshold.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aThresholdA CCA failure rate threshold. Value 0 maps to 0% and 0xffff maps to 100%.
◆ otChannelManagerSetDelay()
| otError otChannelManagerSetDelay | ( | otInstance * |
aInstance,
|
| uint16_t |
aDelay
|
||
| ) |
This function sets the delay (in seconds) used for a channel change.
The delay should preferably be longer than maximum data poll interval used by all sleepy-end-devices within the Thread network.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aDelayDelay in seconds.
- Return values
-
OT_ERROR_NONEDelay was updated successfully. OT_ERROR_INVALID_ARGSThe given delay aDelayis too short.
◆ otChannelManagerSetFavoredChannels()
| void otChannelManagerSetFavoredChannels | ( | otInstance * |
aInstance,
|
| uint32_t |
aChannelMask
|
||
| ) |
This function sets the favored channel mask.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aChannelMaskA channel mask.
◆ otChannelManagerSetSupportedChannels()
| void otChannelManagerSetSupportedChannels | ( | otInstance * |
aInstance,
|
| uint32_t |
aChannelMask
|
||
| ) |
This function sets the supported channel mask.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aChannelMaskA channel mask.