This structure holds diagnostic information for a neighboring Thread node.
#include <
include/openthread/thread.h
>
Public Attributes |
|
| otExtAddress | mExtAddress |
|
IEEE 802.15.4 Extended Address.
|
|
| uint32_t | mAge |
|
Time last heard.
|
|
| uint16_t | mRloc16 |
|
RLOC16.
|
|
| uint32_t | mLinkFrameCounter |
|
Link Frame Counter.
|
|
| uint32_t | mMleFrameCounter |
|
MLE Frame Counter.
|
|
| uint8_t | mLinkQualityIn |
|
Link Quality In.
|
|
| int8_t | mAverageRssi |
|
Average RSSI.
|
|
| int8_t | mLastRssi |
|
Last observed RSSI.
|
|
| uint16_t | mFrameErrorRate |
|
Frame error rate (0xffff->100%). Requires error tracking feature.
|
|
| uint16_t | mMessageErrorRate |
|
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature.
|
|
| bool | mRxOnWhenIdle : 1 |
|
rx-on-when-idle
|
|
| bool | mFullThreadDevice : 1 |
|
Full Thread Device.
|
|
| bool | mFullNetworkData : 1 |
|
Full Network Data.
|
|
| bool | mIsChild : 1 |
|
Is the neighbor a child.
|
|
This structure holds diagnostic information for a neighboring Thread node.
The documentation for this struct was generated from the following file:
-
include/openthread/
thread.h