otDnsTxtEntry Struct Reference
This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3).
#include <
include/openthread/dns.h
>
Public Attributes |
|
| const char * | mKey |
|
The TXT record key string.
|
|
| const uint8_t * | mValue |
The TXT record value or already encoded TXT-DATA (depending on
mKey
).
|
|
| uint16_t | mValueLength |
Number of bytes in
mValue
buffer.
|
|
This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3).
The string buffers pointed to by
mKey
and
mValue
MUST persist and remain unchanged after an instance of such structure is passed to OpenThread (as part of
otSrpClientService
instance).
An array of
otDnsTxtEntry
entries are used in
otSrpClientService
to specify the full TXT record (a list of entries).
Member Data Documentation
◆ mKey
| const char* otDnsTxtEntry::mKey |
The TXT record key string.
If
mKey
is not NULL, then it MUST be a null-terminated C string. The entry is treated as key/value pair with
mValue
buffer providing the value.
-
The entry is encoded as follows:
- A single string length byte followed by "key=value" format (without the quotation marks).
- In this case, the overall encoded length must be 255 bytes or less.
-
If
mValueis NULL, then key is treated as a boolean attribute and encoded as "key" (with no=). -
If
mValueis not NULL butmValueLengthis zero, then it is treated as empty value and encoded as "key=".
If
mKey
is NULL, then
mValue
buffer is treated as an already encoded TXT-DATA and is appended as is in the DNS message.
The documentation for this struct was generated from the following file:
-
include/openthread/
dns.h