This module includes functions for child supervision feature.
Functions |
|
| uint16_t | otChildSupervisionGetInterval ( otInstance *aInstance) |
|
Get the child supervision interval (in seconds).
|
|
| void | otChildSupervisionSetInterval ( otInstance *aInstance, uint16_t aInterval) |
|
Set the child supervision interval (in seconds).
|
|
| uint16_t | otChildSupervisionGetCheckTimeout ( otInstance *aInstance) |
|
Get the supervision check timeout interval (in seconds).
|
|
| void | otChildSupervisionSetCheckTimeout ( otInstance *aInstance, uint16_t aTimeout) |
|
Set the supervision check timeout interval (in seconds).
|
|
Detailed Description
This module includes functions for child supervision feature.
The functions in this module are available when child supervision feature (
OPENTHREAD_CONFIG_CHILD_SUPERVISION_ENABLE
) is enabled.
Function Documentation
◆ otChildSupervisionGetCheckTimeout()
| uint16_t otChildSupervisionGetCheckTimeout | ( | otInstance * |
aInstance
|
) |
Get the supervision check timeout interval (in seconds).
If the device is a sleepy child and it does not hear from its parent within the specified check timeout, it initiates the re-attach process (MLE Child Update Request/Response exchange with its parent).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The supervision check timeout. Zero indicates that supervision check on the child is disabled.
◆ otChildSupervisionGetInterval()
| uint16_t otChildSupervisionGetInterval | ( | otInstance * |
aInstance
|
) |
Get the child supervision interval (in seconds).
Child supervision feature provides a mechanism for parent to ensure that a message is sent to each sleepy child within the supervision interval. If there is no transmission to the child within the supervision interval, OpenThread enqueues and sends a supervision message (a data message with empty payload) to the child.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The child supervision interval. Zero indicates that child supervision is disabled.
◆ otChildSupervisionSetCheckTimeout()
| void otChildSupervisionSetCheckTimeout | ( | otInstance * |
aInstance,
|
| uint16_t |
aTimeout
|
||
| ) |
Set the supervision check timeout interval (in seconds).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aTimeoutThe check timeout (in seconds). Zero to disable supervision check on the child.
◆ otChildSupervisionSetInterval()
| void otChildSupervisionSetInterval | ( | otInstance * |
aInstance,
|
| uint16_t |
aInterval
|
||
| ) |
Set the child supervision interval (in seconds).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aIntervalThe supervision interval (in seconds). Zero to disable supervision on parent.