This structure represents a received IEEE 802.15.4 Beacon.
#include <
include/openthread/link.h
>
Public Attributes |
|
| otExtAddress | mExtAddress |
|
IEEE 802.15.4 Extended Address.
|
|
| otNetworkName | mNetworkName |
|
Thread Network Name.
|
|
| otExtendedPanId | mExtendedPanId |
|
Thread Extended PAN ID.
|
|
| otSteeringData | mSteeringData |
|
Steering Data.
|
|
| uint16_t | mPanId |
|
IEEE 802.15.4 PAN ID.
|
|
| uint16_t | mJoinerUdpPort |
|
Joiner UDP Port.
|
|
| uint8_t | mChannel |
|
IEEE 802.15.4 Channel.
|
|
| int8_t | mRssi |
|
RSSI (dBm)
|
|
| uint8_t | mLqi |
|
LQI.
|
|
| unsigned int | mVersion : 4 |
|
Version.
|
|
| bool | mIsNative : 1 |
|
Native Commissioner flag.
|
|
| bool | mDiscover : 1 |
|
Result from MLE Discovery.
|
|
| bool | mIsJoinable : 1 |
|
Joining Permitted flag.
|
|
This structure represents a received IEEE 802.15.4 Beacon.
The documentation for this struct was generated from the following file:
-
include/openthread/
link.h