Crypto - Platform
This module includes the platform abstraction for Crypto.
Classes | |
struct | otCryptoKey |
This structure represents the Key Material required for Crypto operations. | |
struct | otCryptoContext |
This structure stores the context object for platform APIs. |
Typedefs | |
typedef uint32_t | otCryptoKeyRef |
This datatype represents the key reference. | |
typedef struct otCryptoKey | otCryptoKey |
typedef struct otCryptoContext | otCryptoContext |
Enumerations | |
enum | otCryptoKeyType { OT_CRYPTO_KEY_TYPE_RAW, OT_CRYPTO_KEY_TYPE_AES, OT_CRYPTO_KEY_TYPE_HMAC } |
This enumeration defines the key types. | |
enum | otCryptoKeyAlgorithm { OT_CRYPTO_KEY_ALG_VENDOR, OT_CRYPTO_KEY_ALG_AES_ECB, OT_CRYPTO_KEY_ALG_HMAC_SHA_256 } |
This enumeration defines the key algorithms. | |
enum | { OT_CRYPTO_KEY_USAGE_NONE = 0, OT_CRYPTO_KEY_USAGE_EXPORT = 1 << 0, OT_CRYPTO_KEY_USAGE_ENCRYPT = 1 << 1, OT_CRYPTO_KEY_USAGE_DECRYPT = 1 << 2, OT_CRYPTO_KEY_USAGE_SIGN_HASH = 1 << 3 } |
This enumeration defines the key usage flags. | |
enum | otCryptoKeyStorage { OT_CRYPTO_KEY_STORAGE_VOLATILE, OT_CRYPTO_KEY_STORAGE_PERSISTENT } |
This enumeration defines the key storage types. |
Functions | |
void | otPlatCryptoInit (void) |
Initialize the Crypto module. | |
otError | otPlatCryptoImportKey (otCryptoKeyRef *aKeyRef, otCryptoKeyType aKeyType, otCryptoKeyAlgorithm aKeyAlgorithm, int aKeyUsage, otCryptoKeyStorage aKeyPersistence, const uint8_t *aKey, size_t aKeyLen) |
Import a key into PSA ITS. | |
otError | otPlatCryptoExportKey (otCryptoKeyRef aKeyRef, uint8_t *aBuffer, size_t aBufferLen, size_t *aKeyLen) |
Export a key stored in PSA ITS. | |
otError | otPlatCryptoDestroyKey (otCryptoKeyRef aKeyRef) |
Destroy a key stored in PSA ITS. | |
bool | otPlatCryptoHasKey (otCryptoKeyRef aKeyRef) |
Check if the key ref passed has an associated key in PSA ITS. | |
otError | otPlatCryptoHmacSha256Init (otCryptoContext *aContext) |
Initialize the HMAC operation. | |
otError | otPlatCryptoHmacSha256Deinit (otCryptoContext *aContext) |
Uninitialize the HMAC operation. | |
otError | otPlatCryptoHmacSha256Start (otCryptoContext *aContext, const otCryptoKey *aKey) |
Start HMAC operation. | |
otError | otPlatCryptoHmacSha256Update (otCryptoContext *aContext, const void *aBuf, uint16_t aBufLength) |
Update the HMAC operation with new input. | |
otError | otPlatCryptoHmacSha256Finish (otCryptoContext *aContext, uint8_t *aBuf, size_t aBufLength) |
Complete the HMAC operation. | |
otError | otPlatCryptoAesInit (otCryptoContext *aContext) |
Initialise the AES operation. | |
otError | otPlatCryptoAesSetKey (otCryptoContext *aContext, const otCryptoKey *aKey) |
Set the key for AES operation. | |
otError | otPlatCryptoAesEncrypt (otCryptoContext *aContext, const uint8_t *aInput, uint8_t *aOutput) |
Encrypt the given data. | |
otError | otPlatCryptoAesFree (otCryptoContext *aContext) |
Free the AES context. | |
otError | otPlatCryptoHkdfInit (otCryptoContext *aContext) |
Initialise the HKDF context. | |
otError | otPlatCryptoHkdfExpand (otCryptoContext *aContext, const uint8_t *aInfo, uint16_t aInfoLength, uint8_t *aOutputKey, uint16_t aOutputKeyLength) |
Perform HKDF Expand step. | |
otError | otPlatCryptoHkdfExtract (otCryptoContext *aContext, const uint8_t *aSalt, uint16_t aSaltLength, const otCryptoKey *aInputKey) |
Perform HKDF Extract step. | |
otError | otPlatCryptoHkdfDeinit (otCryptoContext *aContext) |
Uninitialize the HKDF context. | |
otError | otPlatCryptoSha256Init (otCryptoContext *aContext) |
Initialise the SHA-256 operation. | |
otError | otPlatCryptoSha256Deinit (otCryptoContext *aContext) |
Uninitialize the SHA-256 operation. | |
otError | otPlatCryptoSha256Start (otCryptoContext *aContext) |
Start SHA-256 operation. | |
otError | otPlatCryptoSha256Update (otCryptoContext *aContext, const void *aBuf, uint16_t aBufLength) |
Update SHA-256 operation with new input. | |
otError | otPlatCryptoSha256Finish (otCryptoContext *aContext, uint8_t *aHash, uint16_t aHashSize) |
Finish SHA-256 operation. | |
void | otPlatCryptoRandomInit (void) |
Initialize cryptographically-secure pseudorandom number generator (CSPRNG). | |
void | otPlatCryptoRandomDeinit (void) |
Deinitialize cryptographically-secure pseudorandom number generator (CSPRNG). | |
otError | otPlatCryptoRandomGet (uint8_t *aBuffer, uint16_t aSize) |
Fills a given buffer with cryptographically secure random bytes. |
Detailed Description
This module includes the platform abstraction for Crypto.
Enumeration Type Documentation
◆ anonymous enum
anonymous enum |
This enumeration defines the key usage flags.
◆ otCryptoKeyAlgorithm
enum otCryptoKeyAlgorithm |
◆ otCryptoKeyStorage
enum otCryptoKeyStorage |
◆ otCryptoKeyType
enum otCryptoKeyType |
Function Documentation
◆ otPlatCryptoAesEncrypt()
otError otPlatCryptoAesEncrypt | ( | otCryptoContext * | aContext, |
const uint8_t * | aInput, |
||
uint8_t * | aOutput |
||
) |
Encrypt the given data.
- Parameters
-
[in] aContext
Context for AES operation. [in] aInput
Pointer to the input buffer. [in] aOutput
Pointer to the output buffer.
- Return values
-
OT_ERROR_NONE
Successfully encrypted aInput
.OT_ERROR_FAILED
Failed to encrypt aInput
.OT_ERROR_INVALID_ARGS
aContext
oraKey
oraOutput
were NULL
◆ otPlatCryptoAesFree()
otError otPlatCryptoAesFree | ( | otCryptoContext * | aContext | ) |
Free the AES context.
- Parameters
-
[in] aContext
Context for AES operation.
- Return values
-
OT_ERROR_NONE
Successfully freed AES context. OT_ERROR_FAILED
Failed to free AES context. OT_ERROR_INVALID_ARGS
aContext
was NULL
◆ otPlatCryptoAesInit()
otError otPlatCryptoAesInit | ( | otCryptoContext * | aContext | ) |
Initialise the AES operation.
- Parameters
-
[in] aContext
Context for AES operation.
- Return values
-
OT_ERROR_NONE
Successfully Initialised AES operation. OT_ERROR_FAILED
Failed to Initialise AES operation. OT_ERROR_INVALID_ARGS
aContext
was NULLOT_ERROR_NO_BUFS
Cannot allocate the context.
- Note
- The platform driver shall point the context to the correct object such as psa_key_id or mbedtls_aes_context_t.
◆ otPlatCryptoAesSetKey()
otError otPlatCryptoAesSetKey | ( | otCryptoContext * | aContext, |
const otCryptoKey * | aKey |
||
) |
Set the key for AES operation.
- Parameters
-
[in] aContext
Context for AES operation. [out] aKey
Key to use for AES operation.
- Return values
-
OT_ERROR_NONE
Successfully set the key for AES operation. OT_ERROR_FAILED
Failed to set the key for AES operation. OT_ERROR_INVALID_ARGS
aContext
oraKey
was NULL
◆ otPlatCryptoDestroyKey()
otError otPlatCryptoDestroyKey | ( | otCryptoKeyRef | aKeyRef | ) |
Destroy a key stored in PSA ITS.
- Parameters
-
[in] aKeyRef
The key ref to be destroyed
- Return values
-
OT_ERROR_NONE
Successfully destroyed the key. OT_ERROR_FAILED
Failed to destroy the key.
- Note
- This API is only used by OT core when
OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE
is enabled.
◆ otPlatCryptoExportKey()
otError otPlatCryptoExportKey | ( | otCryptoKeyRef | aKeyRef, |
uint8_t * | aBuffer, |
||
size_t | aBufferLen, |
||
size_t * | aKeyLen |
||
) |
Export a key stored in PSA ITS.
- Parameters
-
[in] aKeyRef
The key ref to be used for crypto operations. [out] aBuffer
Pointer to the buffer where key needs to be exported. [in] aBufferLen
Length of the buffer passed to store the exported key. [out] aKeyLen
Pointer to return the length of the exported key.
- Return values
-
OT_ERROR_NONE
Successfully exported aKeyRef
.OT_ERROR_FAILED
Failed to export aKeyRef
.OT_ERROR_INVALID_ARGS
aBuffer
was NULL
- Note
- This API is only used by OT core when
OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE
is enabled.
◆ otPlatCryptoHasKey()
bool otPlatCryptoHasKey | ( | otCryptoKeyRef | aKeyRef | ) |
Check if the key ref passed has an associated key in PSA ITS.
- Parameters
-
[in] aKeyRef
The Key Ref to check.
- Return values
-
TRUE
There is an associated key with aKeyRef
.FALSE
There is no associated key with aKeyRef
.
- Note
- This API is only used by OT core when
OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE
is enabled.
◆ otPlatCryptoHkdfDeinit()
otError otPlatCryptoHkdfDeinit | ( | otCryptoContext * | aContext | ) |
Uninitialize the HKDF context.
- Parameters
-
[in] aContext
Context for HKDF operation.
- Return values
-
OT_ERROR_NONE
Successfully un-initialised HKDF operation. OT_ERROR_FAILED
Failed to un-initialised HKDF operation. OT_ERROR_INVALID_ARGS
aContext
was NULL
◆ otPlatCryptoHkdfExpand()
otError otPlatCryptoHkdfExpand | ( | otCryptoContext * | aContext, |
const uint8_t * | aInfo, |
||
uint16_t | aInfoLength, |
||
uint8_t * | aOutputKey, |
||
uint16_t | aOutputKeyLength |
||
) |
Perform HKDF Expand step.
- Parameters
-
[in] aContext
Operation context for HKDF operation. [in] aInfo
Pointer to the Info sequence. [in] aInfoLength
Length of the Info sequence. [out] aOutputKey
Pointer to the output Key. [in] aOutputKeyLength
Size of the output key buffer.
- Return values
-
OT_ERROR_NONE
HKDF Expand was successful. OT_ERROR_FAILED
HKDF Expand failed. OT_ERROR_INVALID_ARGS
aContext
was NULL
◆ otPlatCryptoHkdfExtract()
otError otPlatCryptoHkdfExtract | ( | otCryptoContext * | aContext, |
const uint8_t * | aSalt, |
||
uint16_t | aSaltLength, |
||
const otCryptoKey * | aInputKey |
||
) |
Perform HKDF Extract step.
- Parameters
-
[in] aContext
Operation context for HKDF operation. [in] aSalt
Pointer to the Salt for HKDF. [in] aSaltLength
Length of Salt. [in] aInputKey
Pointer to the input key.
- Return values
-
OT_ERROR_NONE
HKDF Extract was successful. OT_ERROR_FAILED
HKDF Extract failed.
◆ otPlatCryptoHkdfInit()
otError otPlatCryptoHkdfInit | ( | otCryptoContext * | aContext | ) |
Initialise the HKDF context.
- Parameters
-
[in] aContext
Context for HKDF operation.
- Return values
-
OT_ERROR_NONE
Successfully Initialised AES operation. OT_ERROR_FAILED
Failed to Initialise AES operation. OT_ERROR_INVALID_ARGS
aContext
was NULL
- Note
- The platform driver shall point the context to the correct object such as psa_key_derivation_operation_t or HmacSha256::Hash
◆ otPlatCryptoHmacSha256Deinit()
otError otPlatCryptoHmacSha256Deinit | ( | otCryptoContext * | aContext | ) |
Uninitialize the HMAC operation.
- Parameters
-
[in] aContext
Context for HMAC operation.
- Return values
-
OT_ERROR_NONE
Successfully uninitialized HMAC operation. OT_ERROR_FAILED
Failed to uninitialized HMAC operation. OT_ERROR_INVALID_ARGS
aContext
was NULL
◆ otPlatCryptoHmacSha256Finish()
otError otPlatCryptoHmacSha256Finish | ( | otCryptoContext * | aContext, |
uint8_t * | aBuf, |
||
size_t | aBufLength |
||
) |
Complete the HMAC operation.
- Parameters
-
[in] aContext
Context for HMAC operation. [out] aBuf
A pointer to the output buffer. [in] aBufLength
The length of aBuf
in bytes.
- Return values
-
OT_ERROR_NONE
Successfully completed HMAC operation. OT_ERROR_FAILED
Failed to complete HMAC operation. OT_ERROR_INVALID_ARGS
aContext
oraBuf
was NULL
◆ otPlatCryptoHmacSha256Init()
otError otPlatCryptoHmacSha256Init | ( | otCryptoContext * | aContext | ) |
Initialize the HMAC operation.
- Parameters
-
[in] aContext
Context for HMAC operation.
- Return values
-
OT_ERROR_NONE
Successfully initialized HMAC operation. OT_ERROR_FAILED
Failed to initialize HMAC operation. OT_ERROR_INVALID_ARGS
aContext
was NULL
- Note
- The platform driver shall point the context to the correct object such as psa_mac_operation_t or mbedtls_md_context_t.
◆ otPlatCryptoHmacSha256Start()
otError otPlatCryptoHmacSha256Start | ( | otCryptoContext * | aContext, |
const otCryptoKey * | aKey |
||
) |
Start HMAC operation.
- Parameters
-
[in] aContext
Context for HMAC operation. [in] aKey
Key material to be used for for HMAC operation.
- Return values
-
OT_ERROR_NONE
Successfully started HMAC operation. OT_ERROR_FAILED
Failed to start HMAC operation. OT_ERROR_INVALID_ARGS
aContext
oraKey
was NULL
◆ otPlatCryptoHmacSha256Update()
otError otPlatCryptoHmacSha256Update | ( | otCryptoContext * | aContext, |
const void * | aBuf, |
||
uint16_t | aBufLength |
||
) |
Update the HMAC operation with new input.
- Parameters
-
[in] aContext
Context for HMAC operation. [in] aBuf
A pointer to the input buffer. [in] aBufLength
The length of aBuf
in bytes.
- Return values
-
OT_ERROR_NONE
Successfully updated HMAC with new input operation. OT_ERROR_FAILED
Failed to update HMAC operation. OT_ERROR_INVALID_ARGS
aContext
oraBuf
was NULL
◆ otPlatCryptoImportKey()
otError otPlatCryptoImportKey | ( | otCryptoKeyRef * | aKeyRef, |
otCryptoKeyType | aKeyType, |
||
otCryptoKeyAlgorithm | aKeyAlgorithm, |
||
int | aKeyUsage, |
||
otCryptoKeyStorage | aKeyPersistence, |
||
const uint8_t * | aKey, |
||
size_t | aKeyLen |
||
) |
Import a key into PSA ITS.
- Parameters
-
[in,out] aKeyRef
Pointer to the key ref to be used for crypto operations. [in] aKeyType
Key Type encoding for the key. [in] aKeyAlgorithm
Key algorithm encoding for the key. [in] aKeyUsage
Key Usage encoding for the key (combinations of OT_CRYPTO_KEY_USAGE_*
).[in] aKeyPersistence
Key Persistence for this key [in] aKey
Actual key to be imported. [in] aKeyLen
Length of the key to be imported.
- Return values
-
OT_ERROR_NONE
Successfully imported the key. OT_ERROR_FAILED
Failed to import the key. OT_ERROR_INVALID_ARGS
aKey
was set to NULL.
- Note
- If OT_CRYPTO_KEY_STORAGE_PERSISTENT is passed for aKeyPersistence then
aKeyRef
is input and platform should use the given aKeyRef and MUST not change it.
If OT_CRYPTO_KEY_STORAGE_VOLATILE is passed for aKeyPersistence then aKeyRef
is output, the initial value does not matter and platform API MUST update it to return the new key ref.
This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE
is enabled.
◆ otPlatCryptoRandomGet()
otError otPlatCryptoRandomGet | ( | uint8_t * | aBuffer, |
uint16_t | aSize |
||
) |
Fills a given buffer with cryptographically secure random bytes.
- Parameters
-
[out] aBuffer
A pointer to a buffer to fill with the random bytes. [in] aSize
Size of buffer (number of bytes to fill).
- Return values
-
OT_ERROR_NONE
Successfully filled buffer with random values. OT_ERROR_FAILED
Operation failed.
◆ otPlatCryptoSha256Deinit()
otError otPlatCryptoSha256Deinit | ( | otCryptoContext * | aContext | ) |
Uninitialize the SHA-256 operation.
- Parameters
-
[in] aContext
Context for SHA-256 operation.
- Return values
-
OT_ERROR_NONE
Successfully un-initialised SHA-256 operation. OT_ERROR_FAILED
Failed to un-initialised SHA-256 operation. OT_ERROR_INVALID_ARGS
aContext
was NULL
◆ otPlatCryptoSha256Finish()
otError otPlatCryptoSha256Finish | ( | otCryptoContext * | aContext, |
uint8_t * | aHash, |
||
uint16_t | aHashSize |
||
) |
Finish SHA-256 operation.
- Parameters
-
[in] aContext
Context for SHA-256 operation. [in] aHash
A pointer to the output buffer, where hash needs to be stored. [in] aHashSize
The length of aHash
in bytes.
- Return values
-
OT_ERROR_NONE
Successfully completed the SHA-256 operation. OT_ERROR_FAILED
Failed to complete SHA-256 operation. OT_ERROR_INVALID_ARGS
aContext
oraHash
was NULL
◆ otPlatCryptoSha256Init()
otError otPlatCryptoSha256Init | ( | otCryptoContext * | aContext | ) |
Initialise the SHA-256 operation.
- Parameters
-
[in] aContext
Context for SHA-256 operation.
- Return values
-
OT_ERROR_NONE
Successfully initialised SHA-256 operation. OT_ERROR_FAILED
Failed to initialise SHA-256 operation. OT_ERROR_INVALID_ARGS
aContext
was NULL
- Note
- The platform driver shall point the context to the correct object such as psa_hash_operation_t or mbedtls_sha256_context.
◆ otPlatCryptoSha256Start()
otError otPlatCryptoSha256Start | ( | otCryptoContext * | aContext | ) |
Start SHA-256 operation.
- Parameters
-
[in] aContext
Context for SHA-256 operation.
- Return values
-
OT_ERROR_NONE
Successfully started SHA-256 operation. OT_ERROR_FAILED
Failed to start SHA-256 operation. OT_ERROR_INVALID_ARGS
aContext
was NULL
◆ otPlatCryptoSha256Update()
otError otPlatCryptoSha256Update | ( | otCryptoContext * | aContext, |
const void * | aBuf, |
||
uint16_t | aBufLength |
||
) |
Update SHA-256 operation with new input.
- Parameters
-
[in] aContext
Context for SHA-256 operation. [in] aBuf
A pointer to the input buffer. [in] aBufLength
The length of aBuf
in bytes.
- Return values
-
OT_ERROR_NONE
Successfully updated SHA-256 with new input operation. OT_ERROR_FAILED
Failed to update SHA-256 operation. OT_ERROR_INVALID_ARGS
aContext
oraBuf
was NULL