Factory Diagnostics - Platform
This module includes the platform abstraction for diagnostics features.
Functions |
|
| otError | otPlatDiagProcess ( otInstance *aInstance, uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen) |
|
This function processes a factory diagnostics command line.
|
|
| void | otPlatDiagModeSet (bool aMode) |
|
This function enables/disables the factory diagnostics mode.
|
|
| bool | otPlatDiagModeGet (void) |
|
This function indicates whether or not factory diagnostics mode is enabled.
|
|
| void | otPlatDiagChannelSet (uint8_t aChannel) |
|
This function sets the channel to use for factory diagnostics.
|
|
| void | otPlatDiagTxPowerSet (int8_t aTxPower) |
|
This function sets the transmit power to use for factory diagnostics.
|
|
| void | otPlatDiagRadioReceived ( otInstance *aInstance, otRadioFrame *aFrame, otError aError) |
|
This function processes the received radio frame.
|
|
| void | otPlatDiagAlarmCallback ( otInstance *aInstance) |
|
This function processes the alarm event.
|
|
Detailed Description
This module includes the platform abstraction for diagnostics features.
Function Documentation
◆ otPlatDiagAlarmCallback()
| void otPlatDiagAlarmCallback | ( | otInstance * |
aInstance
|
) |
This function processes the alarm event.
- Parameters
-
[in] aInstanceThe OpenThread instance for current request.
◆ otPlatDiagChannelSet()
| void otPlatDiagChannelSet | ( | uint8_t |
aChannel
|
) |
This function sets the channel to use for factory diagnostics.
- Parameters
-
[in] aChannelThe channel value.
◆ otPlatDiagModeGet()
| bool otPlatDiagModeGet | ( | void |
|
) |
This function indicates whether or not factory diagnostics mode is enabled.
- Returns
- TRUE if factory diagnostics mode is enabled, FALSE otherwise.
◆ otPlatDiagModeSet()
| void otPlatDiagModeSet | ( | bool |
aMode
|
) |
This function enables/disables the factory diagnostics mode.
- Parameters
-
[in] aModeTRUE to enable diagnostics mode, FALSE otherwise.
◆ otPlatDiagProcess()
| otError otPlatDiagProcess | ( | otInstance * |
aInstance,
|
| uint8_t |
aArgsLength,
|
||
| char * |
aArgs[],
|
||
| char * |
aOutput,
|
||
| size_t |
aOutputMaxLen
|
||
| ) |
This function processes a factory diagnostics command line.
The output of this function (the content written to
aOutput
) MUST terminate with
\0
and the
\0
is within the output buffer.
- Parameters
-
[in] aInstanceThe OpenThread instance for current request. [in] aArgsLengthThe number of arguments in aArgs.[in] aArgsThe arguments of diagnostics command line. [out] aOutputThe diagnostics execution result. [in] aOutputMaxLenThe output buffer size.
- Return values
-
OT_ERROR_INVALID_ARGSThe command is supported but invalid arguments provided. OT_ERROR_NONEThe command is successfully process. OT_ERROR_INVALID_COMMANDThe command is not valid or not supported.
◆ otPlatDiagRadioReceived()
| void otPlatDiagRadioReceived | ( | otInstance * |
aInstance,
|
| otRadioFrame * |
aFrame,
|
||
| otError |
aError
|
||
| ) |
This function processes the received radio frame.
- Parameters
-
[in] aInstanceThe OpenThread instance for current request. [in] aFrameThe received radio frame. [in] aErrorThe received radio frame status.
◆ otPlatDiagTxPowerSet()
| void otPlatDiagTxPowerSet | ( | int8_t |
aTxPower
|
) |
This function sets the transmit power to use for factory diagnostics.
- Parameters
-
[in] aTxPowerThe transmit power value.