otHistoryTrackerNeighborInfo Struct Reference
This structure represents a neighbor info.
#include <
include/openthread/history_tracker.h
>
Public Attributes |
|
| otExtAddress | mExtAddress |
|
Neighbor's Extended Address.
|
|
| uint16_t | mRloc16 |
|
Neighbor's RLOC16.
|
|
| int8_t | mAverageRssi |
|
Average RSSI of rx frames from neighbor at the time of recording entry.
|
|
| uint8_t | mEvent : 2 |
Indicates the event (
OT_HISTORY_TRACKER_NEIGHBOR_EVENT_*
enumeration).
|
|
| bool | mRxOnWhenIdle : 1 |
|
Rx-on-when-idle.
|
|
| bool | mFullThreadDevice : 1 |
|
Full Thread Device.
|
|
| bool | mFullNetworkData : 1 |
|
Full Network Data.
|
|
| bool | mIsChild : 1 |
|
Indicates whether or not the neighbor is a child.
|
|
This structure represents a neighbor info.
The documentation for this struct was generated from the following file:
-
include/openthread/
history_tracker.h