This structure represents the MLE Parent Response data.
#include <
include/openthread/thread.h
>
Public Attributes |
|
| otExtAddress | mExtAddr |
|
IEEE 802.15.4 Extended Address of the Parent.
|
|
| uint16_t | mRloc16 |
|
Short address of the Parent.
|
|
| int8_t | mRssi |
|
Rssi of the Parent.
|
|
| int8_t | mPriority |
|
Parent priority.
|
|
| uint8_t | mLinkQuality3 |
|
Parent Link Quality 3.
|
|
| uint8_t | mLinkQuality2 |
|
Parent Link Quality 2.
|
|
| uint8_t | mLinkQuality1 |
|
Parent Link Quality 1.
|
|
| bool | mIsAttached |
|
Is the node receiving parent response attached.
|
|
This structure represents the MLE Parent Response data.
The documentation for this struct was generated from the following file:
-
include/openthread/
thread.h