Records the history of different events, for example RX and TX messages or network info changes.
Classes |
|
| struct | otHistoryTrackerIterator |
|
This type represents an iterator to iterate through a history list.
|
|
| struct | otHistoryTrackerNetworkInfo |
|
This structure represents Thread network info.
|
|
| struct | otHistoryTrackerUnicastAddressInfo |
|
This structure represent a unicast IPv6 address info.
|
|
| struct | otHistoryTrackerMulticastAddressInfo |
|
This structure represent an IPv6 multicast address info.
|
|
| struct | otHistoryTrackerMessageInfo |
|
This structure represents a RX/TX IPv6 message info.
|
|
| struct | otHistoryTrackerNeighborInfo |
|
This structure represents a neighbor info.
|
|
| struct | otHistoryTrackerOnMeshPrefixInfo |
|
This structure represent a Network Data on mesh prefix info.
|
|
| struct | otHistoryTrackerExternalRouteInfo |
|
This structure represent a Network Data extern route info.
|
|
Macros |
|
| #define | OT_HISTORY_TRACKER_MAX_AGE (49 * 24 * 60 * 60 * 1000u) |
|
This constant specifies the maximum age of entries which is 49 days (in msec).
|
|
| #define | OT_HISTORY_TRACKER_ENTRY_AGE_STRING_SIZE 21 |
|
Recommended size for string representation of an entry age.
|
|
Typedefs |
|
| typedef struct otHistoryTrackerIterator | otHistoryTrackerIterator |
|
This type represents an iterator to iterate through a history list.
|
|
| typedef struct otHistoryTrackerNetworkInfo | otHistoryTrackerNetworkInfo |
|
This structure represents Thread network info.
|
|
| typedef struct otHistoryTrackerUnicastAddressInfo | otHistoryTrackerUnicastAddressInfo |
|
This structure represent a unicast IPv6 address info.
|
|
| typedef struct otHistoryTrackerMulticastAddressInfo | otHistoryTrackerMulticastAddressInfo |
|
This structure represent an IPv6 multicast address info.
|
|
| typedef struct otHistoryTrackerMessageInfo | otHistoryTrackerMessageInfo |
|
This structure represents a RX/TX IPv6 message info.
|
|
| typedef struct otHistoryTrackerNeighborInfo | otHistoryTrackerNeighborInfo |
|
This structure represents a neighbor info.
|
|
| typedef struct otHistoryTrackerOnMeshPrefixInfo | otHistoryTrackerOnMeshPrefixInfo |
|
This structure represent a Network Data on mesh prefix info.
|
|
| typedef struct otHistoryTrackerExternalRouteInfo | otHistoryTrackerExternalRouteInfo |
|
This structure represent a Network Data extern route info.
|
|
Functions |
|
| void | otHistoryTrackerInitIterator ( otHistoryTrackerIterator *aIterator) |
This function initializes an
otHistoryTrackerIterator
.
|
|
| const otHistoryTrackerNetworkInfo * | otHistoryTrackerIterateNetInfoHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the network info history list.
|
|
| const otHistoryTrackerUnicastAddressInfo * | otHistoryTrackerIterateUnicastAddressHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the unicast address history list.
|
|
| const otHistoryTrackerMulticastAddressInfo * | otHistoryTrackerIterateMulticastAddressHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the multicast address history list.
|
|
| const otHistoryTrackerMessageInfo * | otHistoryTrackerIterateRxHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the RX message history list.
|
|
| const otHistoryTrackerMessageInfo * | otHistoryTrackerIterateTxHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the TX message history list.
|
|
| const otHistoryTrackerNeighborInfo * | otHistoryTrackerIterateNeighborHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the neighbor history list.
|
|
| const otHistoryTrackerOnMeshPrefixInfo * | otHistoryTrackerIterateOnMeshPrefixHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the Network Data on mesh prefix entry history list.
|
|
| const otHistoryTrackerExternalRouteInfo * | otHistoryTrackerIterateExternalRouteHistory ( otInstance *aInstance, otHistoryTrackerIterator *aIterator, uint32_t *aEntryAge) |
|
This function iterates over the entries in the Network Data external route entry history list.
|
|
| void | otHistoryTrackerEntryAgeToString (uint32_t aEntryAge, char *aBuffer, uint16_t aSize) |
|
This function converts a given entry age to a human-readable string.
|
|
Detailed Description
Records the history of different events, for example RX and TX messages or network info changes.
All tracked entries are timestamped.
The functions in this module are available when
OPENTHREAD_CONFIG_HISTOR_TRACKER_ENABLE
is enabled.
Macro Definition Documentation
◆ OT_HISTORY_TRACKER_MAX_AGE
| #define OT_HISTORY_TRACKER_MAX_AGE (49 * 24 * 60 * 60 * 1000u) |
This constant specifies the maximum age of entries which is 49 days (in msec).
Entries older than the max age will give this value as their age.
Typedef Documentation
◆ otHistoryTrackerIterator
| typedef struct otHistoryTrackerIterator otHistoryTrackerIterator |
This type represents an iterator to iterate through a history list.
The fields in this type are opaque (intended for use by OpenThread core) and therefore should not be accessed/used by caller.
Before using an iterator, it MUST be initialized using
otHistoryTrackerInitIterator()
,
◆ otHistoryTrackerMessageInfo
| typedef struct otHistoryTrackerMessageInfo otHistoryTrackerMessageInfo |
This structure represents a RX/TX IPv6 message info.
Some of the fields in this struct are applicable to a RX message or a TX message only, e.g.,
mAveRxRss
is the average RSS of all fragment frames that form a received message and is only applicable for a RX message.
Enumeration Type Documentation
◆ anonymous enum
| anonymous enum |
Constants representing message priority used in
otHistoryTrackerMessageInfo
struct.
◆ otHistoryTrackerAddressEvent
◆ otHistoryTrackerNeighborEvent
This enumeration defines the events in a neighbor info (i.e.
whether neighbor is added, removed, or changed).
Event
OT_HISTORY_TRACKER_NEIGHBOR_EVENT_RESTORING
is applicable to child neighbors only. It is triggered after the device (re)starts and when the previous children list is retrieved from non-volatile settings and the device tries to restore connection to them.
◆ otHistoryTrackerNetDataEvent
Function Documentation
◆ otHistoryTrackerEntryAgeToString()
| void otHistoryTrackerEntryAgeToString | ( | uint32_t |
aEntryAge,
|
| char * |
aBuffer,
|
||
| uint16_t |
aSize
|
||
| ) |
This function converts a given entry age to a human-readable string.
The entry age string follows the format "<hh>:<mm>:<ss>.<mmmm>" for hours, minutes, seconds and millisecond (if shorter than one day) or "<dd> days <hh>:<mm>:<ss>.<mmmm>" (if longer than one day).
If the resulting string does not fit in
aBuffer
(within its
aSize
characters), the string will be truncated but the outputted string is always null-terminated.
- Parameters
-
[in] aEntryAgeThe entry age (duration in msec). [out] aBufferA pointer to a char array to output the string (MUST NOT be NULL). [in] aSizeThe size of aBuffer. Recommended to useOT_HISTORY_TRACKER_ENTRY_AGE_STRING_SIZE.
◆ otHistoryTrackerInitIterator()
| void otHistoryTrackerInitIterator | ( | otHistoryTrackerIterator * |
aIterator
|
) |
This function initializes an
otHistoryTrackerIterator
.
An iterator MUST be initialized before it is used.
An iterator can be initialized again to start from the beginning of the list.
When iterating over entries in a list, to ensure the entry ages are consistent, the age is given relative to the time the iterator was initialized, i.e., the entry age is provided as the duration (in milliseconds) from the event (when entry was recorded) to the iterator initialization time.
- Parameters
-
[in] aIteratorA pointer to the iterator to initialize (MUST NOT be NULL).
◆ otHistoryTrackerIterateExternalRouteHistory()
| const otHistoryTrackerExternalRouteInfo * otHistoryTrackerIterateExternalRouteHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the Network Data external route entry history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
The
otHistoryTrackerExternalRouteInfoentry orNULLif no more entries in the list.
◆ otHistoryTrackerIterateMulticastAddressHistory()
| const otHistoryTrackerMulticastAddressInfo * otHistoryTrackerIterateMulticastAddressHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the multicast address history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
A pointer to
otHistoryTrackerMulticastAddressInfoentry orNULLif no more entries in the list.
◆ otHistoryTrackerIterateNeighborHistory()
| const otHistoryTrackerNeighborInfo * otHistoryTrackerIterateNeighborHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the neighbor history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
The
otHistoryTrackerNeighborInfoentry orNULLif no more entries in the list.
◆ otHistoryTrackerIterateNetInfoHistory()
| const otHistoryTrackerNetworkInfo * otHistoryTrackerIterateNetInfoHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the network info history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
A pointer to
otHistoryTrackerNetworkInfoentry orNULLif no more entries in the list.
◆ otHistoryTrackerIterateOnMeshPrefixHistory()
| const otHistoryTrackerOnMeshPrefixInfo * otHistoryTrackerIterateOnMeshPrefixHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the Network Data on mesh prefix entry history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
The
otHistoryTrackerOnMeshPrefixInfoentry orNULLif no more entries in the list.
◆ otHistoryTrackerIterateRxHistory()
| const otHistoryTrackerMessageInfo * otHistoryTrackerIterateRxHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the RX message history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
The
otHistoryTrackerMessageInfoentry orNULLif no more entries in the list.
◆ otHistoryTrackerIterateTxHistory()
| const otHistoryTrackerMessageInfo * otHistoryTrackerIterateTxHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the TX message history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
The
otHistoryTrackerMessageInfoentry orNULLif no more entries in the list.
◆ otHistoryTrackerIterateUnicastAddressHistory()
| const otHistoryTrackerUnicastAddressInfo * otHistoryTrackerIterateUnicastAddressHistory | ( | otInstance * |
aInstance,
|
| otHistoryTrackerIterator * |
aIterator,
|
||
| uint32_t * |
aEntryAge
|
||
| ) |
This function iterates over the entries in the unicast address history list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in,out] aIteratorA pointer to an iterator. MUST be initialized or the behavior is undefined. [out] aEntryAgeA pointer to a variable to output the entry's age. MUST NOT be NULL. Age is provided as the duration (in milliseconds) from when entry was recorded to aIteratorinitialization time. It is set toOT_HISTORY_TRACKER_MAX_AGEfor entries older than max age.
- Returns
-
A pointer to
otHistoryTrackerUnicastAddressInfoentry orNULLif no more entries in the list.