otDnsQueryConfig Struct Reference
This structure represents a DNS query configuration.
#include <
include/openthread/dns_client.h
>
Public Attributes |
|
| otSockAddr | mServerSockAddr |
|
Server address (IPv6 address/port). All zero or zero port for unspecified.
|
|
| uint32_t | mResponseTimeout |
|
Wait time (in msec) to rx response. Zero indicates unspecified value.
|
|
| uint8_t | mMaxTxAttempts |
|
Maximum tx attempts before reporting failure. Zero for unspecified value.
|
|
| otDnsRecursionFlag | mRecursionFlag |
|
Indicates whether the server can resolve the query recursively or not.
|
|
| otDnsNat64Mode | mNat64Mode |
|
Allow/Disallow NAT64 address translation during address resolution.
|
|
This structure represents a DNS query configuration.
Any of the fields in this structure can be set to zero to indicate that it is not specified. How the unspecified fields are treated is determined by the function which uses the instance of
otDnsQueryConfig
.
The documentation for this struct was generated from the following file:
-
include/openthread/
dns_client.h