This module includes functions that control link-layer configuration.
Classes | |
struct | otThreadLinkInfo |
This structure represents link-specific information for messages received from the Thread radio. | |
struct | otMacFilterEntry |
This structure represents a Mac Filter entry. | |
struct | otMacCounters |
This structure represents the MAC layer counters. | |
struct | otActiveScanResult |
This structure represents a received IEEE 802.15.4 Beacon. | |
struct | otEnergyScanResult |
This structure represents an energy scan result. |
Macros | |
#define | OT_US_PER_TEN_SYMBOLS 160 |
The microseconds per 10 symbols. | |
#define | OT_MAC_FILTER_FIXED_RSS_DISABLED 127 |
Used to indicate no fixed received signal strength was set. | |
#define | OT_MAC_FILTER_ITERATOR_INIT 0 |
Initializer for otMacFilterIterator. |
Typedefs | |
typedef struct otThreadLinkInfo | otThreadLinkInfo |
This structure represents link-specific information for messages received from the Thread radio. | |
typedef uint8_t | otMacFilterIterator |
Used to iterate through mac filter entries. | |
typedef enum otMacFilterAddressMode | otMacFilterAddressMode |
Defines address mode of the mac filter. | |
typedef struct otMacFilterEntry | otMacFilterEntry |
This structure represents a Mac Filter entry. | |
typedef struct otMacCounters | otMacCounters |
This structure represents the MAC layer counters. | |
typedef struct otActiveScanResult | otActiveScanResult |
This structure represents a received IEEE 802.15.4 Beacon. | |
typedef struct otEnergyScanResult | otEnergyScanResult |
This structure represents an energy scan result. | |
typedef void(* | otHandleActiveScanResult) (otActiveScanResult *aResult, void *aContext) |
This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes. | |
typedef void(* | otHandleEnergyScanResult) (otEnergyScanResult *aResult, void *aContext) |
This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes. | |
typedef void(* | otLinkPcapCallback) (const otRadioFrame *aFrame, bool aIsTx, void *aContext) |
This function pointer is called when an IEEE 802.15.4 frame is received. |
Enumerations | |
enum | otMacFilterAddressMode { OT_MAC_FILTER_ADDRESS_MODE_DISABLED, OT_MAC_FILTER_ADDRESS_MODE_ALLOWLIST, OT_MAC_FILTER_ADDRESS_MODE_DENYLIST } |
Defines address mode of the mac filter. |
Functions | |
otError | otLinkActiveScan (otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleActiveScanResult aCallback, void *aCallbackContext) |
This function starts an IEEE 802.15.4 Active Scan. | |
bool | otLinkIsActiveScanInProgress (otInstance *aInstance) |
This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress. | |
otError | otLinkEnergyScan (otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleEnergyScanResult aCallback, void *aCallbackContext) |
This function starts an IEEE 802.15.4 Energy Scan. | |
bool | otLinkIsEnergyScanInProgress (otInstance *aInstance) |
This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress. | |
otError | otLinkSendDataRequest (otInstance *aInstance) |
This function enqueues an IEEE 802.15.4 Data Request message for transmission. | |
bool | otLinkIsInTransmitState (otInstance *aInstance) |
This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state. | |
uint8_t | otLinkGetChannel (otInstance *aInstance) |
Get the IEEE 802.15.4 channel. | |
otError | otLinkSetChannel (otInstance *aInstance, uint8_t aChannel) |
Set the IEEE 802.15.4 channel. | |
uint32_t | otLinkGetSupportedChannelMask (otInstance *aInstance) |
Get the supported channel mask of MAC layer. | |
otError | otLinkSetSupportedChannelMask (otInstance *aInstance, uint32_t aChannelMask) |
Set the supported channel mask of MAC layer. | |
const otExtAddress * | otLinkGetExtendedAddress (otInstance *aInstance) |
Get the IEEE 802.15.4 Extended Address. | |
otError | otLinkSetExtendedAddress (otInstance *aInstance, const otExtAddress *aExtAddress) |
This function sets the IEEE 802.15.4 Extended Address. | |
void | otLinkGetFactoryAssignedIeeeEui64 (otInstance *aInstance, otExtAddress *aEui64) |
Get the factory-assigned IEEE EUI-64. | |
otPanId | otLinkGetPanId (otInstance *aInstance) |
Get the IEEE 802.15.4 PAN ID. | |
otError | otLinkSetPanId (otInstance *aInstance, otPanId aPanId) |
Set the IEEE 802.15.4 PAN ID. | |
uint32_t | otLinkGetPollPeriod (otInstance *aInstance) |
Get the data poll period of sleepy end device. | |
otError | otLinkSetPollPeriod (otInstance *aInstance, uint32_t aPollPeriod) |
Set/clear user-specified/external data poll period for sleepy end device. | |
otShortAddress | otLinkGetShortAddress (otInstance *aInstance) |
Get the IEEE 802.15.4 Short Address. | |
uint8_t | otLinkGetMaxFrameRetriesDirect (otInstance *aInstance) |
This method returns the maximum number of frame retries during direct transmission. | |
void | otLinkSetMaxFrameRetriesDirect (otInstance *aInstance, uint8_t aMaxFrameRetriesDirect) |
This method sets the maximum number of frame retries during direct transmission. | |
uint8_t | otLinkGetMaxFrameRetriesIndirect (otInstance *aInstance) |
This method returns the maximum number of frame retries during indirect transmission. | |
void | otLinkSetMaxFrameRetriesIndirect (otInstance *aInstance, uint8_t aMaxFrameRetriesIndirect) |
This method sets the maximum number of frame retries during indirect transmission. | |
otMacFilterAddressMode | otLinkFilterGetAddressMode (otInstance *aInstance) |
This function gets the address mode of MAC filter. | |
void | otLinkFilterSetAddressMode (otInstance *aInstance, otMacFilterAddressMode aMode) |
This function sets the address mode of MAC filter. | |
otError | otLinkFilterAddAddress (otInstance *aInstance, const otExtAddress *aExtAddress) |
This method adds an Extended Address to MAC filter. | |
void | otLinkFilterRemoveAddress (otInstance *aInstance, const otExtAddress *aExtAddress) |
This method removes an Extended Address from MAC filter. | |
void | otLinkFilterClearAddresses (otInstance *aInstance) |
This method clears all the Extended Addresses from MAC filter. | |
otError | otLinkFilterGetNextAddress (otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry) |
This method gets an in-use address filter entry. | |
otError | otLinkFilterAddRssIn (otInstance *aInstance, const otExtAddress *aExtAddress, int8_t aRss) |
This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter. | |
void | otLinkFilterRemoveRssIn (otInstance *aInstance, const otExtAddress *aExtAddress) |
This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address. | |
void | otLinkFilterSetDefaultRssIn (otInstance *aInstance, int8_t aRss) |
This method sets the default received signal strength (in dBm) on MAC Filter. | |
void | otLinkFilterClearDefaultRssIn (otInstance *aInstance) |
This method clears any previously set default received signal strength (in dBm) on MAC Filter. | |
void | otLinkFilterClearAllRssIn (otInstance *aInstance) |
This method clears all the received signal strength entries (including default RSS-in) on MAC Filter. | |
otError | otLinkFilterGetNextRssIn (otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry) |
This method gets an in-use RssIn filter entry. | |
void | otLinkSetRadioFilterEnabled (otInstance *aInstance, bool aFilterEnabled) |
This function enables/disables IEEE 802.15.4 radio filter mode. | |
bool | otLinkIsRadioFilterEnabled (otInstance *aInstance) |
This function indicates whether the IEEE 802.15.4 radio filter is enabled or not. | |
uint8_t | otLinkConvertRssToLinkQuality (otInstance *aInstance, int8_t aRss) |
This method converts received signal strength to link quality. | |
int8_t | otLinkConvertLinkQualityToRss (otInstance *aInstance, uint8_t aLinkQuality) |
This method converts link quality to typical received signal strength. | |
const uint32_t * | otLinkGetTxDirectRetrySuccessHistogram (otInstance *aInstance, uint8_t *aNumberOfEntries) |
This method gets histogram of retries for a single direct packet until success. | |
const uint32_t * | otLinkGetTxIndirectRetrySuccessHistogram (otInstance *aInstance, uint8_t *aNumberOfEntries) |
This method gets histogram of retries for a single indirect packet until success. | |
void | otLinkResetTxRetrySuccessHistogram (otInstance *aInstance) |
This method clears histogram statistics for direct and indirect transmissions. | |
const otMacCounters * | otLinkGetCounters (otInstance *aInstance) |
Get the MAC layer counters. | |
void | otLinkResetCounters (otInstance *aInstance) |
Reset the MAC layer counters. | |
void | otLinkSetPcapCallback (otInstance *aInstance, otLinkPcapCallback aPcapCallback, void *aCallbackContext) |
This function registers a callback to provide received raw IEEE 802.15.4 frames. | |
bool | otLinkIsPromiscuous (otInstance *aInstance) |
This function indicates whether or not promiscuous mode is enabled at the link layer. | |
otError | otLinkSetPromiscuous (otInstance *aInstance, bool aPromiscuous) |
This function enables or disables the link layer promiscuous mode. | |
uint8_t | otLinkCslGetChannel (otInstance *aInstance) |
This function gets the CSL channel. | |
otError | otLinkCslSetChannel (otInstance *aInstance, uint8_t aChannel) |
This function sets the CSL channel. | |
uint16_t | otLinkCslGetPeriod (otInstance *aInstance) |
This function gets the CSL period. | |
otError | otLinkCslSetPeriod (otInstance *aInstance, uint16_t aPeriod) |
This function sets the CSL period. | |
uint32_t | otLinkCslGetTimeout (otInstance *aInstance) |
This function gets the CSL timeout. | |
otError | otLinkCslSetTimeout (otInstance *aInstance, uint32_t aTimeout) |
This function sets the CSL timeout. | |
uint16_t | otLinkGetCcaFailureRate (otInstance *aInstance) |
This function returns the current CCA (Clear Channel Assessment) failure rate. | |
otError | otLinkSetEnabled (otInstance *aInstance, bool aEnable) |
This function enables or disables the link layer. | |
bool | otLinkIsEnabled (otInstance *aInstance) |
This function indicates whether or not the link layer is enabled. | |
otError | otLinkSendEmptyData (otInstance *aInstance) |
This function instructs the device to send an empty IEEE 802.15.4 data frame. |
Detailed Description
This module includes functions that control link-layer configuration.
Macro Definition Documentation
◆ OT_MAC_FILTER_FIXED_RSS_DISABLED
#define OT_MAC_FILTER_FIXED_RSS_DISABLED 127 |
Used to indicate no fixed received signal strength was set.
Typedef Documentation
◆ otHandleActiveScanResult
typedef void(* otHandleActiveScanResult) (otActiveScanResult *aResult, void *aContext) |
This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.
- Parameters
-
[in] aResult
A valid pointer to the beacon information or NULL when the active scan completes. [in] aContext
A pointer to application-specific context.
◆ otHandleEnergyScanResult
typedef void(* otHandleEnergyScanResult) (otEnergyScanResult *aResult, void *aContext) |
This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.
- Parameters
-
[in] aResult
A valid pointer to the energy scan result information or NULL when the energy scan completes. [in] aContext
A pointer to application-specific context.
◆ otLinkPcapCallback
typedef void(* otLinkPcapCallback) (const otRadioFrame *aFrame, bool aIsTx, void *aContext) |
This function pointer is called when an IEEE 802.15.4 frame is received.
- Note
- This callback is called after FCS processing and
aFrame
may not contain the actual FCS that was received. - This callback is called before IEEE 802.15.4 security processing.
- Parameters
-
[in] aFrame
A pointer to the received IEEE 802.15.4 frame. [in] aIsTx
Whether this frame is transmitted, not received. [in] aContext
A pointer to application-specific context.
Enumeration Type Documentation
◆ otMacFilterAddressMode
Function Documentation
◆ otLinkActiveScan()
otError otLinkActiveScan | ( | otInstance * | aInstance, |
uint32_t | aScanChannels, |
||
uint16_t | aScanDuration, |
||
otHandleActiveScanResult | aCallback, |
||
void * | aCallbackContext |
||
) |
This function starts an IEEE 802.15.4 Active Scan.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aScanChannels
A bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK). [in] aScanDuration
The time in milliseconds to spend scanning each channel. [in] aCallback
A pointer to a function called on receiving a beacon or scan completes. [in] aCallbackContext
A pointer to application-specific context.
- Return values
-
OT_ERROR_NONE
Accepted the Active Scan request. OT_ERROR_BUSY
Already performing an Active Scan.
◆ otLinkConvertLinkQualityToRss()
int8_t otLinkConvertLinkQualityToRss | ( | otInstance * | aInstance, |
uint8_t | aLinkQuality |
||
) |
This method converts link quality to typical received signal strength.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aLinkQuality
LinkQuality value, should be in range [0,3].
- Returns
- Typical platform received signal strength mapping to
aLinkQuality
.
◆ otLinkConvertRssToLinkQuality()
uint8_t otLinkConvertRssToLinkQuality | ( | otInstance * | aInstance, |
int8_t | aRss |
||
) |
This method converts received signal strength to link quality.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aRss
The received signal strength value to be converted.
- Returns
- Link quality value mapping to
aRss
.
◆ otLinkCslGetChannel()
uint8_t otLinkCslGetChannel | ( | otInstance * | aInstance | ) |
This function gets the CSL channel.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The CSL channel.
◆ otLinkCslGetPeriod()
uint16_t otLinkCslGetPeriod | ( | otInstance * | aInstance | ) |
This function gets the CSL period.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The CSL period in units of 10 symbols.
◆ otLinkCslGetTimeout()
uint32_t otLinkCslGetTimeout | ( | otInstance * | aInstance | ) |
This function gets the CSL timeout.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The CSL timeout in seconds.
◆ otLinkCslSetChannel()
otError otLinkCslSetChannel | ( | otInstance * | aInstance, |
uint8_t | aChannel |
||
) |
This function sets the CSL channel.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aChannel
The CSL sample channel. Channel value should be 0
(Set CSL Channel unspecified) or within the range [1, 10] (if 915-MHz supported) and 11, 26.
- Return values
-
OT_ERROR_NONE
Successfully set the CSL parameters. OT_ERROR_INVALID_ARGS
Invalid aChannel
.
◆ otLinkCslSetPeriod()
otError otLinkCslSetPeriod | ( | otInstance * | aInstance, |
uint16_t | aPeriod |
||
) |
This function sets the CSL period.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPeriod
The CSL period in units of 10 symbols.
- Return values
-
OT_ERROR_NONE
Successfully set the CSL period. OT_ERROR_INVALID_ARGS
Invalid CSL period.
◆ otLinkCslSetTimeout()
otError otLinkCslSetTimeout | ( | otInstance * | aInstance, |
uint32_t | aTimeout |
||
) |
This function sets the CSL timeout.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aTimeout
The CSL timeout in seconds.
- Return values
-
OT_ERROR_NONE
Successfully set the CSL timeout. OT_ERROR_INVALID_ARGS
Invalid CSL timeout.
◆ otLinkEnergyScan()
otError otLinkEnergyScan | ( | otInstance * | aInstance, |
uint32_t | aScanChannels, |
||
uint16_t | aScanDuration, |
||
otHandleEnergyScanResult | aCallback, |
||
void * | aCallbackContext |
||
) |
This function starts an IEEE 802.15.4 Energy Scan.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aScanChannels
A bit vector indicating on which channels to perform energy scan. [in] aScanDuration
The time in milliseconds to spend scanning each channel. [in] aCallback
A pointer to a function called to pass on scan result on indicate scan completion. [in] aCallbackContext
A pointer to application-specific context.
- Return values
-
OT_ERROR_NONE
Accepted the Energy Scan request. OT_ERROR_BUSY
Could not start the energy scan.
◆ otLinkFilterAddAddress()
otError otLinkFilterAddAddress | ( | otInstance * | aInstance, |
const otExtAddress * | aExtAddress |
||
) |
This method adds an Extended Address to MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aExtAddress
A pointer to the Extended Address (MUST NOT be NULL).
- Return values
-
OT_ERROR_NONE
Successfully added aExtAddress
to MAC filter.OT_ERROR_NO_BUFS
No available entry exists.
◆ otLinkFilterAddRssIn()
otError otLinkFilterAddRssIn | ( | otInstance * | aInstance, |
const otExtAddress * | aExtAddress, |
||
int8_t | aRss |
||
) |
This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aExtAddress
A pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL. [in] aRss
A received signal strength (in dBm).
- Return values
-
OT_ERROR_NONE
Successfully added an entry for aExtAddress
andaRss
.OT_ERROR_NO_BUFS
No available entry exists.
◆ otLinkFilterClearAddresses()
void otLinkFilterClearAddresses | ( | otInstance * | aInstance | ) |
This method clears all the Extended Addresses from MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
◆ otLinkFilterClearAllRssIn()
void otLinkFilterClearAllRssIn | ( | otInstance * | aInstance | ) |
This method clears all the received signal strength entries (including default RSS-in) on MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
◆ otLinkFilterClearDefaultRssIn()
void otLinkFilterClearDefaultRssIn | ( | otInstance * | aInstance | ) |
This method clears any previously set default received signal strength (in dBm) on MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
◆ otLinkFilterGetAddressMode()
otMacFilterAddressMode otLinkFilterGetAddressMode | ( | otInstance * | aInstance | ) |
This function gets the address mode of MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- the address mode.
◆ otLinkFilterGetNextAddress()
otError otLinkFilterGetNextAddress | ( | otInstance * | aInstance, |
otMacFilterIterator * | aIterator, |
||
otMacFilterEntry * | aEntry |
||
) |
This method gets an in-use address filter entry.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in,out] aIterator
A pointer to the MAC filter iterator context. To get the first in-use address filter entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT. MUST NOT be NULL. [out] aEntry
A pointer to where the information is placed. MUST NOT be NULL.
- Return values
-
OT_ERROR_NONE
Successfully retrieved an in-use address filter entry. OT_ERROR_NOT_FOUND
No subsequent entry exists.
◆ otLinkFilterGetNextRssIn()
otError otLinkFilterGetNextRssIn | ( | otInstance * | aInstance, |
otMacFilterIterator * | aIterator, |
||
otMacFilterEntry * | aEntry |
||
) |
This method gets an in-use RssIn filter entry.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in,out] aIterator
A pointer to the MAC filter iterator context. MUST NOT be NULL. To get the first entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT. [out] aEntry
A pointer to where the information is placed. The last entry would have the extended address as all 0xff to indicate the default received signal strength if it was set. aEntry
MUST NOT be NULL.
- Return values
-
OT_ERROR_NONE
Successfully retrieved the next entry. OT_ERROR_NOT_FOUND
No subsequent entry exists.
◆ otLinkFilterRemoveAddress()
void otLinkFilterRemoveAddress | ( | otInstance * | aInstance, |
const otExtAddress * | aExtAddress |
||
) |
This method removes an Extended Address from MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
No action is performed if there is no existing entry in Filter matching the given Extended Address.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aExtAddress
A pointer to the Extended Address (MUST NOT be NULL).
◆ otLinkFilterRemoveRssIn()
void otLinkFilterRemoveRssIn | ( | otInstance * | aInstance, |
const otExtAddress * | aExtAddress |
||
) |
This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
No action is performed if there is no existing entry in Filter matching the given Extended Address.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aExtAddress
A pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL.
◆ otLinkFilterSetAddressMode()
void otLinkFilterSetAddressMode | ( | otInstance * | aInstance, |
otMacFilterAddressMode | aMode |
||
) |
This function sets the address mode of MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMode
The address mode to set.
◆ otLinkFilterSetDefaultRssIn()
void otLinkFilterSetDefaultRssIn | ( | otInstance * | aInstance, |
int8_t | aRss |
||
) |
This method sets the default received signal strength (in dBm) on MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
The default RSS value is used for all received frames from addresses for which there is no explicit RSS-IN entry in the Filter list (added using otLinkFilterAddRssIn()
).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aRss
The default received signal strength (in dBm) to set.
◆ otLinkGetCcaFailureRate()
uint16_t otLinkGetCcaFailureRate | ( | otInstance * | aInstance | ) |
This function returns the current CCA (Clear Channel Assessment) failure rate.
The rate is maintained over a window of (roughly) last OPENTHREAD_CONFIG_CCA_FAILURE_RATE_AVERAGING_WINDOW
frame transmissions.
- Returns
- The CCA failure rate with maximum value
0xffff
corresponding to 100% failure rate.
◆ otLinkGetChannel()
uint8_t otLinkGetChannel | ( | otInstance * | aInstance | ) |
Get the IEEE 802.15.4 channel.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The IEEE 802.15.4 channel.
- See also
- otLinkSetChannel
◆ otLinkGetCounters()
const otMacCounters* otLinkGetCounters | ( | otInstance * | aInstance | ) |
Get the MAC layer counters.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- A pointer to the MAC layer counters.
◆ otLinkGetExtendedAddress()
const otExtAddress* otLinkGetExtendedAddress | ( | otInstance * | aInstance | ) |
Get the IEEE 802.15.4 Extended Address.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- A pointer to the IEEE 802.15.4 Extended Address.
◆ otLinkGetFactoryAssignedIeeeEui64()
void otLinkGetFactoryAssignedIeeeEui64 | ( | otInstance * | aInstance, |
otExtAddress * | aEui64 |
||
) |
Get the factory-assigned IEEE EUI-64.
- Parameters
-
[in] aInstance
A pointer to the OpenThread instance. [out] aEui64
A pointer to where the factory-assigned IEEE EUI-64 is placed.
◆ otLinkGetMaxFrameRetriesDirect()
uint8_t otLinkGetMaxFrameRetriesDirect | ( | otInstance * | aInstance | ) |
This method returns the maximum number of frame retries during direct transmission.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The maximum number of retries during direct transmission.
◆ otLinkGetMaxFrameRetriesIndirect()
uint8_t otLinkGetMaxFrameRetriesIndirect | ( | otInstance * | aInstance | ) |
This method returns the maximum number of frame retries during indirect transmission.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The maximum number of retries during indirect transmission.
◆ otLinkGetPanId()
otPanId otLinkGetPanId | ( | otInstance * | aInstance | ) |
Get the IEEE 802.15.4 PAN ID.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The IEEE 802.15.4 PAN ID.
- See also
- otLinkSetPanId
◆ otLinkGetPollPeriod()
uint32_t otLinkGetPollPeriod | ( | otInstance * | aInstance | ) |
Get the data poll period of sleepy end device.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The data poll period of sleepy end device in milliseconds.
- See also
- otLinkSetPollPeriod
◆ otLinkGetShortAddress()
otShortAddress otLinkGetShortAddress | ( | otInstance * | aInstance | ) |
Get the IEEE 802.15.4 Short Address.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- A pointer to the IEEE 802.15.4 Short Address.
◆ otLinkGetSupportedChannelMask()
uint32_t otLinkGetSupportedChannelMask | ( | otInstance * | aInstance | ) |
Get the supported channel mask of MAC layer.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The supported channel mask as
uint32_t
with bit 0 (lsb) mapping to channel 0, bit 1 to channel 1, so on.
◆ otLinkGetTxDirectRetrySuccessHistogram()
const uint32_t* otLinkGetTxDirectRetrySuccessHistogram | ( | otInstance * | aInstance, |
uint8_t * | aNumberOfEntries |
||
) |
This method gets histogram of retries for a single direct packet until success.
This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [out] aNumberOfEntries
A pointer to where the size of returned histogram array is placed.
- Returns
- A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.
◆ otLinkGetTxIndirectRetrySuccessHistogram()
const uint32_t* otLinkGetTxIndirectRetrySuccessHistogram | ( | otInstance * | aInstance, |
uint8_t * | aNumberOfEntries |
||
) |
This method gets histogram of retries for a single indirect packet until success.
This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [out] aNumberOfEntries
A pointer to where the size of returned histogram array is placed.
- Returns
- A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.
◆ otLinkIsActiveScanInProgress()
bool otLinkIsActiveScanInProgress | ( | otInstance * | aInstance | ) |
This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- true if an IEEE 802.15.4 Active Scan is in progress, false otherwise.
◆ otLinkIsEnabled()
bool otLinkIsEnabled | ( | otInstance * | aInstance | ) |
This function indicates whether or not the link layer is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
true
Link layer is enabled. false
Link layer is not enabled.
◆ otLinkIsEnergyScanInProgress()
bool otLinkIsEnergyScanInProgress | ( | otInstance * | aInstance | ) |
This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- true if an IEEE 802.15.4 Energy Scan is in progress, false otherwise.
◆ otLinkIsInTransmitState()
bool otLinkIsInTransmitState | ( | otInstance * | aInstance | ) |
This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.
MAC module is in the transmit state during CSMA/CA procedure, CCA, Data, Beacon or Data Request frame transmission and receiving an ACK of a transmitted frame. MAC module is not in the transmit state during transmission of an ACK frame or a Beacon Request frame.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- true if an IEEE 802.15.4 MAC is in the transmit state, false otherwise.
◆ otLinkIsPromiscuous()
bool otLinkIsPromiscuous | ( | otInstance * | aInstance | ) |
This function indicates whether or not promiscuous mode is enabled at the link layer.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
true
Promiscuous mode is enabled. false
Promiscuous mode is not enabled.
◆ otLinkIsRadioFilterEnabled()
bool otLinkIsRadioFilterEnabled | ( | otInstance * | aInstance | ) |
This function indicates whether the IEEE 802.15.4 radio filter is enabled or not.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Return values
-
TRUE
If the radio filter is enabled. FALSE
If the radio filter is disabled.
◆ otLinkResetCounters()
void otLinkResetCounters | ( | otInstance * | aInstance | ) |
Reset the MAC layer counters.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
◆ otLinkResetTxRetrySuccessHistogram()
void otLinkResetTxRetrySuccessHistogram | ( | otInstance * | aInstance | ) |
This method clears histogram statistics for direct and indirect transmissions.
This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
◆ otLinkSendDataRequest()
otError otLinkSendDataRequest | ( | otInstance * | aInstance | ) |
This function enqueues an IEEE 802.15.4 Data Request message for transmission.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONE
Successfully enqueued an IEEE 802.15.4 Data Request message. OT_ERROR_INVALID_STATE
Device is not in rx-off-when-idle mode. OT_ERROR_NO_BUFS
Insufficient message buffers available.
◆ otLinkSendEmptyData()
otError otLinkSendEmptyData | ( | otInstance * | aInstance | ) |
This function instructs the device to send an empty IEEE 802.15.4 data frame.
This function is only supported on an Rx-Off-When-Idle device to send an empty data frame to its parent. Note: available only when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONE
Successfully enqueued an empty message. OT_ERROR_INVALID_STATE
Device is not in Rx-Off-When-Idle mode. OT_ERROR_NO_BUFS
Insufficient message buffers available.
◆ otLinkSetChannel()
otError otLinkSetChannel | ( | otInstance * | aInstance, |
uint8_t | aChannel |
||
) |
Set the IEEE 802.15.4 channel.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aChannel
The IEEE 802.15.4 channel.
- Return values
-
OT_ERROR_NONE
Successfully set the channel. OT_ERROR_INVALID_ARGS
If aChannel
is not in the range [11, 26] or is not in the supported channel mask.OT_ERROR_INVALID_STATE
Thread protocols are enabled.
- See also
- otLinkGetChannel
◆ otLinkSetEnabled()
otError otLinkSetEnabled | ( | otInstance * | aInstance, |
bool | aEnable |
||
) |
This function enables or disables the link layer.
- Note
- The link layer may only be enabled / disabled when the Thread Interface is disabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aEnable
true to enable the link layer, or false otherwise.
- Return values
-
OT_ERROR_NONE
Successfully enabled / disabled the link layer. OT_ERROR_INVALID_STATE
Could not disable the link layer because the Thread interface is enabled.
◆ otLinkSetExtendedAddress()
otError otLinkSetExtendedAddress | ( | otInstance * | aInstance, |
const otExtAddress * | aExtAddress |
||
) |
This function sets the IEEE 802.15.4 Extended Address.
This function succeeds only when Thread protocols are disabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aExtAddress
A pointer to the IEEE 802.15.4 Extended Address.
- Return values
-
OT_ERROR_NONE
Successfully set the IEEE 802.15.4 Extended Address. OT_ERROR_INVALID_ARGS
aExtAddress
was NULL.OT_ERROR_INVALID_STATE
Thread protocols are enabled.
◆ otLinkSetMaxFrameRetriesDirect()
void otLinkSetMaxFrameRetriesDirect | ( | otInstance * | aInstance, |
uint8_t | aMaxFrameRetriesDirect |
||
) |
This method sets the maximum number of frame retries during direct transmission.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMaxFrameRetriesDirect
The maximum number of retries during direct transmission.
◆ otLinkSetMaxFrameRetriesIndirect()
void otLinkSetMaxFrameRetriesIndirect | ( | otInstance * | aInstance, |
uint8_t | aMaxFrameRetriesIndirect |
||
) |
This method sets the maximum number of frame retries during indirect transmission.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMaxFrameRetriesIndirect
The maximum number of retries during indirect transmission.
◆ otLinkSetPanId()
otError otLinkSetPanId | ( | otInstance * | aInstance, |
otPanId | aPanId |
||
) |
Set the IEEE 802.15.4 PAN ID.
This function succeeds only when Thread protocols are disabled. A successful call to this function also invalidates the Active and Pending Operational Datasets in non-volatile memory.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPanId
The IEEE 802.15.4 PAN ID.
- Return values
-
OT_ERROR_NONE
Successfully set the PAN ID. OT_ERROR_INVALID_ARGS
If aPanId is not in the range [0, 65534]. OT_ERROR_INVALID_STATE
Thread protocols are enabled.
- See also
- otLinkGetPanId
◆ otLinkSetPcapCallback()
void otLinkSetPcapCallback | ( | otInstance * | aInstance, |
otLinkPcapCallback | aPcapCallback, |
||
void * | aCallbackContext |
||
) |
This function registers a callback to provide received raw IEEE 802.15.4 frames.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPcapCallback
A pointer to a function that is called when receiving an IEEE 802.15.4 link frame or NULL to disable the callback. [in] aCallbackContext
A pointer to application-specific context.
◆ otLinkSetPollPeriod()
otError otLinkSetPollPeriod | ( | otInstance * | aInstance, |
uint32_t | aPollPeriod |
||
) |
Set/clear user-specified/external data poll period for sleepy end device.
- Note
- This function updates only poll period of sleepy end device. To update child timeout the function
otThreadSetChildTimeout()
shall be called. -
Minimal non-zero value should be
OPENTHREAD_CONFIG_MAC_MINIMUM_POLL_PERIOD
(10ms). Or zero to clear user-specified poll period. - User-specified value should be no more than the maximal value 0x3FFFFFF ((1 << 26) - 1) allowed, otherwise it would be clipped by the maximal value.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPollPeriod
data poll period in milliseconds.
- Return values
-
OT_ERROR_NONE
Successfully set/cleared user-specified poll period. OT_ERROR_INVALID_ARGS
If aPollPeriod is invalid.
- See also
- otLinkGetPollPeriod
◆ otLinkSetPromiscuous()
otError otLinkSetPromiscuous | ( | otInstance * | aInstance, |
bool | aPromiscuous |
||
) |
This function enables or disables the link layer promiscuous mode.
- Note
- Promiscuous mode may only be enabled when the Thread interface is disabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPromiscuous
true to enable promiscuous mode, or false otherwise.
- Return values
-
OT_ERROR_NONE
Successfully enabled promiscuous mode. OT_ERROR_INVALID_STATE
Could not enable promiscuous mode because the Thread interface is enabled.
◆ otLinkSetRadioFilterEnabled()
void otLinkSetRadioFilterEnabled | ( | otInstance * | aInstance, |
bool | aFilterEnabled |
||
) |
This function enables/disables IEEE 802.15.4 radio filter mode.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
The radio filter is mainly intended for testing. It can be used to temporarily block all tx/rx on the 802.15.4 radio. When radio filter is enabled, radio is put to sleep instead of receive (to ensure device does not receive any frame and/or potentially send ack). Also the frame transmission requests return immediately without sending the frame over the air (return "no ack" error if ack is requested, otherwise return success).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aFilterEnabled
TRUE to enable radio filter, FALSE to disable
◆ otLinkSetSupportedChannelMask()
otError otLinkSetSupportedChannelMask | ( | otInstance * | aInstance, |
uint32_t | aChannelMask |
||
) |
Set the supported channel mask of MAC layer.
This function succeeds only when Thread protocols are disabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aChannelMask
The supported channel mask (bit 0 or lsb mapping to channel 0, and so on).
- Return values
-
OT_ERROR_NONE
Successfully set the supported channel mask. OT_ERROR_INVALID_STATE
Thread protocols are enabled.