This module includes functions that control the Thread stack's execution.
Classes |
|
| struct | otCliCommand |
|
This structure represents a CLI command.
|
|
Typedefs |
|
| typedef int(* | otCliOutputCallback ) (void *aContext, const char *aFormat, va_list aArguments) |
|
This function pointer is called to notify about Console output.
|
|
| typedef struct otCliCommand | otCliCommand |
Functions |
|
| void | otCliInit ( otInstance *aInstance, otCliOutputCallback aCallback, void *aContext) |
|
Initialize the CLI module.
|
|
| void | otCliInputLine (char *aBuf) |
|
This method is called to feed in a console input line.
|
|
| void | otCliSetUserCommands (const otCliCommand *aUserCommands, uint8_t aLength, void *aContext) |
|
Set a user command table.
|
|
| void | otCliSetUserCommandError ( otError aError) |
|
This method sets the user command error.
|
|
| void | otCliOutputBytes (const uint8_t *aBytes, uint8_t aLength) |
|
Write a number of bytes to the CLI console as a hex string.
|
|
| void | otCliOutputFormat (const char *aFmt,...) |
|
Write formatted string to the CLI console.
|
|
| void | otCliAppendResult ( otError aError) |
|
Write error code to the CLI console.
|
|
| void | otCliPlatLogv ( otLogLevel aLogLevel, otLogRegion aLogRegion, const char *aFormat, va_list aArgs) |
|
Callback to write the OpenThread Log to the CLI console.
|
|
Detailed Description
This module includes functions that control the Thread stack's execution.
Typedef Documentation
◆ otCliOutputCallback
| typedef int(* otCliOutputCallback) (void *aContext, const char *aFormat, va_list aArguments) |
This function pointer is called to notify about Console output.
- Parameters
-
[out] aContextA user context pointer. [in] aFormatThe format string. [in] aArgumentsThe format string arguments.
- Returns
- Number of bytes written by the callback.
Function Documentation
◆ otCliAppendResult()
| void otCliAppendResult | ( | otError |
aError
|
) |
Write error code to the CLI console.
If the
aError
is
OT_ERROR_PENDING
nothing will be outputted.
- Parameters
-
[in] aErrorError code value.
◆ otCliInit()
| void otCliInit | ( | otInstance * |
aInstance,
|
| otCliOutputCallback |
aCallback,
|
||
| void * |
aContext
|
||
| ) |
Initialize the CLI module.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aCallbackA callback method called to process CLI output. [in] aContextA user context pointer.
◆ otCliInputLine()
| void otCliInputLine | ( | char * |
aBuf
|
) |
This method is called to feed in a console input line.
- Parameters
-
[in] aBufA pointer to a null-terminated string.
◆ otCliOutputBytes()
| void otCliOutputBytes | ( | const uint8_t * |
aBytes,
|
| uint8_t |
aLength
|
||
| ) |
Write a number of bytes to the CLI console as a hex string.
- Parameters
-
[in] aBytesA pointer to data which should be printed. [in] aLengthaByteslength.
◆ otCliOutputFormat()
| void otCliOutputFormat | ( | const char * |
aFmt,
|
...
|
|||
| ) |
Write formatted string to the CLI console.
- Parameters
-
[in] aFmtA pointer to the format string. [in] ...A matching list of arguments.
◆ otCliPlatLogv()
| void otCliPlatLogv | ( | otLogLevel |
aLogLevel,
|
| otLogRegion |
aLogRegion,
|
||
| const char * |
aFormat,
|
||
| va_list |
aArgs
|
||
| ) |
Callback to write the OpenThread Log to the CLI console.
- Parameters
-
[in] aLogLevelThe log level. [in] aLogRegionThe log region. [in] aFormatA pointer to the format string. [in] aArgsva_list matching aFormat.
◆ otCliSetUserCommandError()
| void otCliSetUserCommandError | ( | otError |
aError
|
) |
This method sets the user command error.
- Parameters
-
[in] aErrorAn error
◆ otCliSetUserCommands()
| void otCliSetUserCommands | ( | const otCliCommand * |
aUserCommands,
|
| uint8_t |
aLength,
|
||
| void * |
aContext
|
||
| ) |
Set a user command table.
- Parameters
-
[in] aUserCommandsA pointer to an array with user commands. [in] aLengthaUserCommandslength.[in] aContextThecontext passed to the handler.