This module includes functions that control the OpenThread Instance.
Macros |
|
| #define | OT_UPTIME_STRING_SIZE 24 |
|
Recommended size for string representation of uptime.
|
|
Typedefs |
|
| typedef struct otInstance | otInstance |
|
This structure represents the OpenThread instance structure.
|
|
| typedef uint32_t | otChangedFlags |
|
This type represents a bit-field indicating specific state/configuration that has changed.
|
|
| typedef void(* | otStateChangedCallback ) ( otChangedFlags aFlags, void *aContext) |
|
This function pointer is called to notify certain configuration or state changes within OpenThread.
|
|
Functions |
|
| otInstance * | otInstanceInit (void *aInstanceBuffer, size_t *aInstanceBufferSize) |
|
This function initializes the OpenThread library.
|
|
| otInstance * | otInstanceInitSingle (void) |
|
This function initializes the static single instance of the OpenThread library.
|
|
| bool | otInstanceIsInitialized ( otInstance *aInstance) |
|
This function indicates whether or not the instance is valid/initialized.
|
|
| void | otInstanceFinalize ( otInstance *aInstance) |
|
This function disables the OpenThread library.
|
|
| uint64_t | otInstanceGetUptime ( otInstance *aInstance) |
|
This function returns the current instance uptime (in msec).
|
|
| void | otInstanceGetUptimeAsString ( otInstance *aInstance, char *aBuffer, uint16_t aSize) |
|
This function returns the current instance uptime as a human-readable string.
|
|
| otError | otSetStateChangedCallback ( otInstance *aInstance, otStateChangedCallback aCallback, void *aContext) |
|
This function registers a callback to indicate when certain configuration or state changes within OpenThread.
|
|
| void | otRemoveStateChangeCallback ( otInstance *aInstance, otStateChangedCallback aCallback, void *aContext) |
|
This function removes a callback to indicate when certain configuration or state changes within OpenThread.
|
|
| void | otInstanceReset ( otInstance *aInstance) |
|
This method triggers a platform reset.
|
|
| void | otInstanceFactoryReset ( otInstance *aInstance) |
|
This method deletes all the settings stored on non-volatile memory, and then triggers platform reset.
|
|
| void | otInstanceResetRadioStack ( otInstance *aInstance) |
|
This method resets the internal states of the OpenThread radio stack.
|
|
| otError | otInstanceErasePersistentInfo ( otInstance *aInstance) |
|
This function erases all the OpenThread persistent info (network settings) stored on non-volatile memory.
|
|
| const char * | otGetVersionString (void) |
|
This function gets the OpenThread version string.
|
|
| const char * | otGetRadioVersionString ( otInstance *aInstance) |
|
This function gets the OpenThread radio version string.
|
|
Detailed Description
This module includes functions that control the OpenThread Instance.
Typedef Documentation
◆ otChangedFlags
| typedef uint32_t otChangedFlags |
This type represents a bit-field indicating specific state/configuration that has changed.
See
OT_CHANGED_*
definitions.
◆ otStateChangedCallback
| typedef void(* otStateChangedCallback) ( otChangedFlags aFlags, void *aContext) |
This function pointer is called to notify certain configuration or state changes within OpenThread.
- Parameters
-
[in] aFlagsA bit-field indicating specific state that has changed. See OT_CHANGED_*definitions.[in] aContextA pointer to application-specific context.
Enumeration Type Documentation
◆ anonymous enum
| anonymous enum |
This enumeration defines flags that are passed as part of
otStateChangedCallback
.
Function Documentation
◆ otGetRadioVersionString()
| const char* otGetRadioVersionString | ( | otInstance * |
aInstance
|
) |
This function gets the OpenThread radio version string.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- A pointer to the OpenThread radio version.
◆ otGetVersionString()
| const char* otGetVersionString | ( | void |
|
) |
This function gets the OpenThread version string.
- Returns
- A pointer to the OpenThread version.
◆ otInstanceErasePersistentInfo()
| otError otInstanceErasePersistentInfo | ( | otInstance * |
aInstance
|
) |
This function erases all the OpenThread persistent info (network settings) stored on non-volatile memory.
Erase is successful only if the device is in
disabled
state/role.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONEAll persistent info/state was erased successfully. OT_ERROR_INVALID_STATEDevice is not in disabledstate/role.
◆ otInstanceFactoryReset()
| void otInstanceFactoryReset | ( | otInstance * |
aInstance
|
) |
This method deletes all the settings stored on non-volatile memory, and then triggers platform reset.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otInstanceFinalize()
| void otInstanceFinalize | ( | otInstance * |
aInstance
|
) |
This function disables the OpenThread library.
Call this function when OpenThread is no longer in use.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otInstanceGetUptime()
| uint64_t otInstanceGetUptime | ( | otInstance * |
aInstance
|
) |
This function returns the current instance uptime (in msec).
This function requires
OPENTHREAD_CONFIG_UPTIME_ENABLE
to be enabled.
The uptime is given as number of milliseconds since OpenThread instance was initialized.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The uptime (number of milliseconds).
◆ otInstanceGetUptimeAsString()
| void otInstanceGetUptimeAsString | ( | otInstance * |
aInstance,
|
| char * |
aBuffer,
|
||
| uint16_t |
aSize
|
||
| ) |
This function returns the current instance uptime as a human-readable string.
This function requires
OPENTHREAD_CONFIG_UPTIME_ENABLE
to be enabled.
The string follows the format "<hh>:<mm>:<ss>.<mmmm>" for hours, minutes, seconds and millisecond (if uptime is shorter than one day) or "<dd>d.<hh>:<mm>:<ss>.<mmmm>" (if longer than a day).
If the resulting string does not fit in
aBuffer
(within its
aSize
characters), the string will be truncated but the outputted string is always null-terminated.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [out] aBufferA pointer to a char array to output the string. [in] aSizeThe size of aBuffer(in bytes). Recommended to useOT_UPTIME_STRING_SIZE.
◆ otInstanceInit()
| otInstance * otInstanceInit | ( | void * |
aInstanceBuffer,
|
| size_t * |
aInstanceBufferSize
|
||
| ) |
This function initializes the OpenThread library.
This function initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.
This function is available and can only be used when support for multiple OpenThread instances is enabled.
- Parameters
-
[in] aInstanceBufferThe buffer for OpenThread to use for allocating the otInstance structure. [in,out] aInstanceBufferSizeOn input, the size of aInstanceBuffer. On output, if not enough space for otInstance, the number of bytes required for otInstance.
- Returns
- A pointer to the new OpenThread instance.
- See also
- otInstanceFinalize
◆ otInstanceInitSingle()
| otInstance * otInstanceInitSingle | ( | void |
|
) |
This function initializes the static single instance of the OpenThread library.
This function initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.
This function is available and can only be used when support for multiple OpenThread instances is disabled.
- Returns
- A pointer to the single OpenThread instance.
◆ otInstanceIsInitialized()
| bool otInstanceIsInitialized | ( | otInstance * |
aInstance
|
) |
This function indicates whether or not the instance is valid/initialized.
The instance is considered valid if it is acquired and initialized using either
otInstanceInitSingle()
(in single instance case) or
otInstanceInit()
(in multi instance case). A subsequent call to
otInstanceFinalize()
causes the instance to be considered as uninitialized.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- TRUE if the given instance is valid/initialized, FALSE otherwise.
◆ otInstanceReset()
| void otInstanceReset | ( | otInstance * |
aInstance
|
) |
This method triggers a platform reset.
The reset process ensures that all the OpenThread state/info (stored in volatile memory) is erased. Note that the
otPlatformReset
does not erase any persistent state/info saved in non-volatile memory.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otInstanceResetRadioStack()
| void otInstanceResetRadioStack | ( | otInstance * |
aInstance
|
) |
This method resets the internal states of the OpenThread radio stack.
Callbacks and configurations are preserved.
This API is only available under radio builds (
OPENTHREAD_RADIO = 1
).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otRemoveStateChangeCallback()
| void otRemoveStateChangeCallback | ( | otInstance * |
aInstance,
|
| otStateChangedCallback |
aCallback,
|
||
| void * |
aContext
|
||
| ) |
This function removes a callback to indicate when certain configuration or state changes within OpenThread.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aCallbackA pointer to a function that is called with certain configuration or state changes. [in] aContextA pointer to application-specific context.
◆ otSetStateChangedCallback()
| otError otSetStateChangedCallback | ( | otInstance * |
aInstance,
|
| otStateChangedCallback |
aCallback,
|
||
| void * |
aContext
|
||
| ) |
This function registers a callback to indicate when certain configuration or state changes within OpenThread.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aCallbackA pointer to a function that is called with certain configuration or state changes. [in] aContextA pointer to application-specific context.
- Return values
-
OT_ERROR_NONEAdded the callback to the list of callbacks. OT_ERROR_ALREADYThe callback was already registered. OT_ERROR_NO_BUFSCould not add the callback due to resource constraints.