otRadioCoexMetrics Struct Reference
The following are valid radio state transitions:
#include <
include/openthread/platform/radio.h
>
Public Attributes |
|
| uint32_t | mNumGrantGlitch |
|
Number of grant glitches.
|
|
| uint32_t | mNumTxRequest |
|
Number of tx requests.
|
|
| uint32_t | mNumTxGrantImmediate |
|
Number of tx requests while grant was active.
|
|
| uint32_t | mNumTxGrantWait |
|
Number of tx requests while grant was inactive.
|
|
| uint32_t | mNumTxGrantWaitActivated |
|
Number of tx requests while grant was inactive that were ultimately granted.
|
|
| uint32_t | mNumTxGrantWaitTimeout |
|
Number of tx requests while grant was inactive that timed out.
|
|
| uint32_t | mNumTxGrantDeactivatedDuringRequest |
|
Number of tx that were in progress when grant was deactivated.
|
|
| uint32_t | mNumTxDelayedGrant |
|
Number of tx requests that were not granted within 50us.
|
|
| uint32_t | mAvgTxRequestToGrantTime |
|
Average time in usec from tx request to grant.
|
|
| uint32_t | mNumRxRequest |
|
Number of rx requests.
|
|
| uint32_t | mNumRxGrantImmediate |
|
Number of rx requests while grant was active.
|
|
| uint32_t | mNumRxGrantWait |
|
Number of rx requests while grant was inactive.
|
|
| uint32_t | mNumRxGrantWaitActivated |
|
Number of rx requests while grant was inactive that were ultimately granted.
|
|
| uint32_t | mNumRxGrantWaitTimeout |
|
Number of rx requests while grant was inactive that timed out.
|
|
| uint32_t | mNumRxGrantDeactivatedDuringRequest |
|
Number of rx that were in progress when grant was deactivated.
|
|
| uint32_t | mNumRxDelayedGrant |
|
Number of rx requests that were not granted within 50us.
|
|
| uint32_t | mAvgRxRequestToGrantTime |
|
Average time in usec from rx request to grant.
|
|
| uint32_t | mNumRxGrantNone |
|
Number of rx requests that completed without receiving grant.
|
|
| bool | mStopped |
|
Stats collection stopped due to saturation.
|
|
The following are valid radio state transitions:
(Radio ON) +----——+ Enable() +-——+ Receive() +---——+ Transmit() +----——+ | |-----——>| |-----——>| |--------——>| | | Disabled | | Sleep | | Receive | | Transmit | | |<-----——| |<-----——| |<--------——| | +----——+ Disable() +-——+ Sleep() +---——+ Receive() +----——+ (Radio OFF) or signal TransmitDone
During the IEEE 802.15.4 data request command the transition Sleep->Receive->Transmit can be shortened to direct transition from Sleep to Transmit if the platform supports the OT_RADIO_CAPS_SLEEP_TO_TX capability. This structure represents radio coexistence metrics.
The documentation for this struct was generated from the following file:
-
include/openthread/platform/
radio.h