otHistoryTrackerMessageInfo Struct Reference
This structure represents a RX/TX IPv6 message info.
#include <
include/openthread/history_tracker.h
>
Public Attributes |
|
| uint16_t | mPayloadLength |
|
IPv6 payload length (exclude IP6 header itself).
|
|
| uint16_t | mNeighborRloc16 |
RLOC16 of neighbor which sent/received the msg (
0xfffe
if no RLOC16).
|
|
| otSockAddr | mSource |
|
Source IPv6 address and port (if UDP/TCP)
|
|
| otSockAddr | mDestination |
|
Destination IPv6 address and port (if UDP/TCP).
|
|
| uint16_t | mChecksum |
|
Message checksum (valid only for UDP/TCP/ICMP6).
|
|
| uint8_t | mIpProto |
IP Protocol number (
OT_IP6_PROTO_*
enumeration).
|
|
| uint8_t | mIcmp6Type |
ICMP6 type if msg is ICMP6, zero otherwise (
OT_ICMP6_TYPE_*
enumeration).
|
|
| int8_t | mAveRxRss |
|
RSS of received message or OT_RADIO_INVALI_RSSI if not known.
|
|
| bool | mLinkSecurity : 1 |
|
Indicates whether msg used link security.
|
|
| bool | mTxSuccess : 1 |
|
Indicates TX success (e.g., ack received). Applicable for TX msg only.
|
|
| uint8_t | mPriority : 2 |
Message priority (
OT_HISTORY_TRACKER_MSG_PRIORITY_*
enumeration).
|
|
| bool | mRadioIeee802154 : 1 |
|
Indicates whether msg was sent/received over a 15.4 radio link.
|
|
| bool | mRadioTrelUdp6 : 1 |
|
Indicates whether msg was sent/received over a TREL radio link.
|
|
This structure represents a RX/TX IPv6 message info.
Some of the fields in this struct are applicable to a RX message or a TX message only, e.g.,
mAveRxRss
is the average RSS of all fragment frames that form a received message and is only applicable for a RX message.
The documentation for this struct was generated from the following file:
-
include/openthread/
history_tracker.h