This structure represents a Network Diagnostic Connectivity value.
#include <
include/openthread/netdiag.h
>
Public Attributes |
|
| int8_t | mParentPriority |
|
The priority of the sender as a parent.
|
|
| uint8_t | mLinkQuality3 |
|
The number of neighboring devices with which the sender shares a link of quality 3.
|
|
| uint8_t | mLinkQuality2 |
|
The number of neighboring devices with which the sender shares a link of quality 2.
|
|
| uint8_t | mLinkQuality1 |
|
The number of neighboring devices with which the sender shares a link of quality 1.
|
|
| uint8_t | mLeaderCost |
|
The sender's routing cost to the Leader.
|
|
| uint8_t | mIdSequence |
|
The most recent ID sequence number received by the sender.
|
|
| uint8_t | mActiveRouters |
|
The number of active Routers in the sender's Thread Network Partition.
|
|
| uint16_t | mSedBufferSize |
|
The guaranteed buffer capacity in octets for all IPv6 datagrams destined to a given SED.
|
|
| uint8_t | mSedDatagramCount |
|
The guaranteed queue capacity in number of IPv6 datagrams destined to a given SED.
|
|
This structure represents a Network Diagnostic Connectivity value.
Member Data Documentation
◆ mSedBufferSize
| uint16_t otNetworkDiagConnectivity::mSedBufferSize |
The guaranteed buffer capacity in octets for all IPv6 datagrams destined to a given SED.
Optional.
◆ mSedDatagramCount
| uint8_t otNetworkDiagConnectivity::mSedDatagramCount |
The guaranteed queue capacity in number of IPv6 datagrams destined to a given SED.
Optional.
The documentation for this struct was generated from the following file:
-
include/openthread/
netdiag.h