Definition of the standalone bootloader interface.

Macros

#define NO_BOOTLOADER_MODE 0xFF
Define a numerical value for NO BOOTLOADER mode. In other words, the bootloader should not be run.
#define STANDALONE_BOOTLOADER_NORMAL_MODE 1
Define a numerical value for the normal bootloader mode.
#define STANDALONE_BOOTLOADER_RECOVERY_MODE 0
Define a numerical value for the recovery bootloader mode.

Functions

uint16_t halGetStandaloneBootloaderVersion (void)
Detects if the standalone bootloader is installed, and if so returns the installed version.
EmberStatus halLaunchStandaloneBootloader (uint8_t mode)
Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.

Detailed Description

Definition of the standalone bootloader interface.

Some functions in this file return an EmberStatus value. See error-def.h for definitions of all EmberStatus return values.

See bootloader-interface-standalone.h for source code.

Macro Definition Documentation

◆ NO_BOOTLOADER_MODE

#define NO_BOOTLOADER_MODE   0xFF

Define a numerical value for NO BOOTLOADER mode. In other words, the bootloader should not be run.

◆ STANDALONE_BOOTLOADER_NORMAL_MODE

#define STANDALONE_BOOTLOADER_NORMAL_MODE   1

Define a numerical value for the normal bootloader mode.

◆ STANDALONE_BOOTLOADER_RECOVERY_MODE

#define STANDALONE_BOOTLOADER_RECOVERY_MODE   0

Define a numerical value for the recovery bootloader mode.

Function Documentation

◆ halGetStandaloneBootloaderVersion()

uint16_t halGetStandaloneBootloaderVersion ( void )

Detects if the standalone bootloader is installed, and if so returns the installed version.

A returned version of 0x1234 would indicate version 1.2 build 34

Returns
BOOTLOADER_INVALID_VERSION if the standalone bootloader is not present, or the version of the installed standalone bootloader.

◆ halLaunchStandaloneBootloader()

EmberStatus halLaunchStandaloneBootloader ( uint8_t mode )

Quits the current application and launches the standalone bootloader (if installed). The function returns an error if the standalone bootloader is not present.

Parameters
mode Controls the mode in which the standalone bootloader will run. See the bootloader Application Note for full details. Options are: Both modes also allow an image transfer to begin via serial xmodem.
Returns
An EmberStatus error if the standalone bootloader is not present, or EMBER_SUCCESS .