Macros

#define TOKEN_NEXT_ADDRESS (region, address)
By default, tokens are automatically located after the previous token.
#define CURRENT_STACK_TOKEN_VERSION 0x03FC
The current version number of the stack tokens. MSB is the version, LSB is a complement.

Convenience Macros

The following convenience macros are used to simplify the definition process for commonly specified parameters to the basic TOKEN_DEF macro. See hal/micro/token.h for a more complete explanation.

#define DEFINE_BASIC_TOKEN (name, type, ...) TOKEN_DEF (name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#define DEFINE_COUNTER_TOKEN (name, type, ...) TOKEN_DEF (name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)
#define DEFINE_INDEXED_TOKEN (name, type, arraysize, ...) TOKEN_DEF (name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)
#define DEFINE_FIXED_BASIC_TOKEN (name, type, address, ...)
#define DEFINE_FIXED_COUNTER_TOKEN (name, type, address, ...)
#define DEFINE_FIXED_INDEXED_TOKEN (name, type, arraysize, address, ...)
#define DEFINE_MFG_TOKEN (name, type, address, ...)

Creator Codes

The CREATOR is used as a distinct identifier tag for the token.

The CREATOR is necessary because the token name is defined differently depending on the hardware platform. Therefore, the CREATOR ensures that token definitions and data stay tagged and known. The only requirement is that each creator definition must be unique. See hal/micro/token.h for a more complete explanation.

#define CREATOR_STACK_NVDATA_VERSION 0xFF01
#define CREATOR_STACK_BOOT_COUNTER 0xE263
#define CREATOR_STACK_NONCE_COUNTER 0xE563
#define CREATOR_STACK_ANALYSIS_REBOOT 0xE162
#define CREATOR_STACK_KEYS 0xEB79
#define CREATOR_STACK_NODE_DATA 0xEE64
#define CREATOR_STACK_CLASSIC_DATA 0xE364
#define CREATOR_STACK_ALTERNATE_KEY 0xE475
#define CREATOR_STACK_APS_FRAME_COUNTER 0xE123
#define CREATOR_STACK_TRUST_CENTER 0xE124
#define CREATOR_STACK_NETWORK_MANAGEMENT 0xE125
#define CREATOR_STACK_PARENT_INFO 0xE126
#define CREATOR_STACK_PARENT_ADDITIONAL_INFO 0xE127
#define CREATOR_STACK_MULTI_PHY_NWK_INFO 0xE128
#define CREATOR_STACK_MIN_RECEIVED_RSSI 0xE129
#define CREATOR_MULTI_NETWORK_STACK_KEYS 0xE210
#define CREATOR_MULTI_NETWORK_STACK_NODE_DATA 0xE211
#define CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY 0xE212
#define CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER 0xE213
#define CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT 0xE214
#define CREATOR_MULTI_NETWORK_STACK_PARENT_INFO 0xE215
#define CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER 0xE220
#define CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO 0xE221
#define CREATOR_STACK_GP_DATA 0xE258
#define CREATOR_STACK_GP_PROXY_TABLE 0xE259
#define CREATOR_STACK_GP_SINK_TABLE 0xE25A
#define CREATOR_STACK_GP_INCOMING_FC 0xE25B
#define CREATOR_STACK_GP_INCOMING_FC_IN_SINK 0xE25C
#define CREATOR_STACK_BINDING_TABLE 0xE274
#define CREATOR_STACK_CHILD_TABLE 0xFF0D
#define CREATOR_STACK_KEY_TABLE 0xE456
#define CREATOR_STACK_CERTIFICATE_TABLE 0xE500
#define CREATOR_STACK_ZLL_DATA 0xE501
#define CREATOR_STACK_ZLL_SECURITY 0xE502
#define CREATOR_STACK_ADDITIONAL_CHILD_DATA 0xE503

NVM3 Object Keys

The NVM3 object key is used as a distinct identifier tag for a token stored in NVM3.

Every token must have a defined NVM3 object key and the object key must be unique. The object key defined must be in the following format: NVM3KEY_tokenname

where tokenname is the name of the token without NVM3KEY_ or TOKEN_ prefix.

#define NVM3KEY_DOMAIN_USER 0x00000U
#define NVM3KEY_DOMAIN_ZIGBEE 0x10000U
#define NVM3KEY_DOMAIN_COMMON 0x80000U
#define NVM3KEY_STACK_NVDATA_VERSION ( NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)
#define NVM3KEY_STACK_BOOT_COUNTER ( NVM3KEY_DOMAIN_ZIGBEE | 0xE263)
#define NVM3KEY_STACK_NONCE_COUNTER ( NVM3KEY_DOMAIN_ZIGBEE | 0xE563)
#define NVM3KEY_STACK_ANALYSIS_REBOOT ( NVM3KEY_DOMAIN_ZIGBEE | 0xE162)
#define NVM3KEY_STACK_KEYS ( NVM3KEY_DOMAIN_ZIGBEE | 0xEB79)
#define NVM3KEY_STACK_NODE_DATA ( NVM3KEY_DOMAIN_ZIGBEE | 0xEE64)
#define NVM3KEY_STACK_CLASSIC_DATA ( NVM3KEY_DOMAIN_ZIGBEE | 0xE364)
#define NVM3KEY_STACK_ALTERNATE_KEY ( NVM3KEY_DOMAIN_ZIGBEE | 0xE475)
#define NVM3KEY_STACK_APS_FRAME_COUNTER ( NVM3KEY_DOMAIN_ZIGBEE | 0xE123)
#define NVM3KEY_STACK_TRUST_CENTER ( NVM3KEY_DOMAIN_ZIGBEE | 0xE124)
#define NVM3KEY_STACK_NETWORK_MANAGEMENT ( NVM3KEY_DOMAIN_ZIGBEE | 0xE125)
#define NVM3KEY_STACK_PARENT_INFO ( NVM3KEY_DOMAIN_ZIGBEE | 0xE126)
#define NVM3KEY_STACK_PARENT_ADDITIONAL_INFO ( NVM3KEY_DOMAIN_ZIGBEE | 0xE127)
#define NVM3KEY_STACK_MULTI_PHY_NWK_INFO ( NVM3KEY_DOMAIN_ZIGBEE | 0xE128)
#define NVM3KEY_STACK_MIN_RECEIVED_RSSI ( NVM3KEY_DOMAIN_ZIGBEE | 0xE129)
#define NVM3KEY_MULTI_NETWORK_STACK_KEYS ( NVM3KEY_DOMAIN_ZIGBEE | 0x0000)
#define NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA ( NVM3KEY_DOMAIN_ZIGBEE | 0x0080)
#define NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY ( NVM3KEY_DOMAIN_ZIGBEE | 0x0100)
#define NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER ( NVM3KEY_DOMAIN_ZIGBEE | 0x0180)
#define NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT ( NVM3KEY_DOMAIN_ZIGBEE | 0x0200)
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO ( NVM3KEY_DOMAIN_ZIGBEE | 0x0280)
#define NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER ( NVM3KEY_DOMAIN_ZIGBEE | 0xE220)
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO ( NVM3KEY_DOMAIN_ZIGBEE | 0x0300)
#define NVM3KEY_STACK_GP_DATA ( NVM3KEY_DOMAIN_ZIGBEE | 0xE258)
#define NVM3KEY_STACK_GP_PROXY_TABLE ( NVM3KEY_DOMAIN_ZIGBEE | 0x0380)
#define NVM3KEY_STACK_GP_SINK_TABLE ( NVM3KEY_DOMAIN_ZIGBEE | 0x0400)
#define NVM3KEY_STACK_GP_INCOMING_FC ( NVM3KEY_DOMAIN_ZIGBEE | 0x0480)
#define NVM3KEY_STACK_BINDING_TABLE ( NVM3KEY_DOMAIN_ZIGBEE | 0x0500)
#define NVM3KEY_STACK_CHILD_TABLE ( NVM3KEY_DOMAIN_ZIGBEE | 0x0580)
#define NVM3KEY_STACK_KEY_TABLE ( NVM3KEY_DOMAIN_ZIGBEE | 0x0600)
#define NVM3KEY_STACK_CERTIFICATE_TABLE ( NVM3KEY_DOMAIN_ZIGBEE | 0x0680)
#define NVM3KEY_STACK_ZLL_DATA ( NVM3KEY_DOMAIN_ZIGBEE | 0xE501)
#define NVM3KEY_STACK_ZLL_SECURITY ( NVM3KEY_DOMAIN_ZIGBEE | 0xE502)
#define NVM3KEY_STACK_ADDITIONAL_CHILD_DATA ( NVM3KEY_DOMAIN_ZIGBEE | 0x0700)
#define NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK ( NVM3KEY_DOMAIN_ZIGBEE | 0x0780)

Detailed Description

These tokens are divided into three sections (the three main types of tokens mentioned in token.h):

  • manufacturing
  • stack
  • application

For a full explanation of the tokens, see hal/micro/token.h . See token-stack.h for source code.

A set of tokens is predefined in the APPLICATION DATA section at the end of token-stack.h because these tokens are required by the stack, but they are classified as application tokens since they are sized by the application via its CONFIGURATION_HEADER.

The user application can include its own tokens in a header file similar to this one. The macro ::APPLICATION_TOKEN_HEADER should be defined to equal the name of the header file in which application tokens are defined. See the APPLICATION DATA section at the end of token-stack.h for examples of token definitions.

Since token-stack.h contains both the typedefs and the token defs, two #defines are used to select which one is needed when this file is included. #define DEFINETYPES is used to select the type definitions and #define DEFINETOKENS is used to select the token definitions. See token.h and token.c to see how these are used.

Macro Definition Documentation

CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY

#define CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY   0xE212

CREATOR_MULTI_NETWORK_STACK_KEYS

#define CREATOR_MULTI_NETWORK_STACK_KEYS   0xE210

CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT

#define CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT   0xE214

CREATOR_MULTI_NETWORK_STACK_NODE_DATA

#define CREATOR_MULTI_NETWORK_STACK_NODE_DATA   0xE211

CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER

#define CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER   0xE220

CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO

#define CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO   0xE221

CREATOR_MULTI_NETWORK_STACK_PARENT_INFO

#define CREATOR_MULTI_NETWORK_STACK_PARENT_INFO   0xE215

CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER

#define CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER   0xE213

CREATOR_STACK_ADDITIONAL_CHILD_DATA

#define CREATOR_STACK_ADDITIONAL_CHILD_DATA   0xE503

CREATOR_STACK_ALTERNATE_KEY

#define CREATOR_STACK_ALTERNATE_KEY   0xE475

CREATOR_STACK_ANALYSIS_REBOOT

#define CREATOR_STACK_ANALYSIS_REBOOT   0xE162

CREATOR_STACK_APS_FRAME_COUNTER

#define CREATOR_STACK_APS_FRAME_COUNTER   0xE123

CREATOR_STACK_BINDING_TABLE

#define CREATOR_STACK_BINDING_TABLE   0xE274

CREATOR_STACK_BOOT_COUNTER

#define CREATOR_STACK_BOOT_COUNTER   0xE263

CREATOR_STACK_CERTIFICATE_TABLE

#define CREATOR_STACK_CERTIFICATE_TABLE   0xE500

CREATOR_STACK_CHILD_TABLE

#define CREATOR_STACK_CHILD_TABLE   0xFF0D

CREATOR_STACK_CLASSIC_DATA

#define CREATOR_STACK_CLASSIC_DATA   0xE364

CREATOR_STACK_GP_DATA

#define CREATOR_STACK_GP_DATA   0xE258

CREATOR_STACK_GP_INCOMING_FC

#define CREATOR_STACK_GP_INCOMING_FC   0xE25B

CREATOR_STACK_GP_INCOMING_FC_IN_SINK

#define CREATOR_STACK_GP_INCOMING_FC_IN_SINK   0xE25C

CREATOR_STACK_GP_PROXY_TABLE

#define CREATOR_STACK_GP_PROXY_TABLE   0xE259

CREATOR_STACK_GP_SINK_TABLE

#define CREATOR_STACK_GP_SINK_TABLE   0xE25A

CREATOR_STACK_KEY_TABLE

#define CREATOR_STACK_KEY_TABLE   0xE456

CREATOR_STACK_KEYS

#define CREATOR_STACK_KEYS   0xEB79

CREATOR_STACK_MIN_RECEIVED_RSSI

#define CREATOR_STACK_MIN_RECEIVED_RSSI   0xE129

CREATOR_STACK_MULTI_PHY_NWK_INFO

#define CREATOR_STACK_MULTI_PHY_NWK_INFO   0xE128

CREATOR_STACK_NETWORK_MANAGEMENT

#define CREATOR_STACK_NETWORK_MANAGEMENT   0xE125

CREATOR_STACK_NODE_DATA

#define CREATOR_STACK_NODE_DATA   0xEE64

CREATOR_STACK_NONCE_COUNTER

#define CREATOR_STACK_NONCE_COUNTER   0xE563

CREATOR_STACK_NVDATA_VERSION

#define CREATOR_STACK_NVDATA_VERSION   0xFF01

CREATOR_STACK_PARENT_ADDITIONAL_INFO

#define CREATOR_STACK_PARENT_ADDITIONAL_INFO   0xE127

CREATOR_STACK_PARENT_INFO

#define CREATOR_STACK_PARENT_INFO   0xE126

CREATOR_STACK_TRUST_CENTER

#define CREATOR_STACK_TRUST_CENTER   0xE124

CREATOR_STACK_ZLL_DATA

#define CREATOR_STACK_ZLL_DATA   0xE501

CREATOR_STACK_ZLL_SECURITY

#define CREATOR_STACK_ZLL_SECURITY   0xE502

CURRENT_STACK_TOKEN_VERSION

#define CURRENT_STACK_TOKEN_VERSION   0x03FC

The current version number of the stack tokens. MSB is the version, LSB is a complement.

See hal/micro/token.h for a more complete explanation.

DEFINE_BASIC_TOKEN

#define DEFINE_BASIC_TOKEN ( name,
type,
...
) TOKEN_DEF (name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)

DEFINE_COUNTER_TOKEN

#define DEFINE_COUNTER_TOKEN ( name,
type,
...
) TOKEN_DEF (name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)

DEFINE_FIXED_BASIC_TOKEN

#define DEFINE_FIXED_BASIC_TOKEN ( name,
type,
address,
...
)
Value:
TOKEN_NEXT_ADDRESS (name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition: token-stack.h:67

DEFINE_FIXED_COUNTER_TOKEN

#define DEFINE_FIXED_COUNTER_TOKEN ( name,
type,
address,
...
)
Value:
TOKEN_NEXT_ADDRESS (name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 1, 0, type, 1, __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition: token-stack.h:67

DEFINE_FIXED_INDEXED_TOKEN

#define DEFINE_FIXED_INDEXED_TOKEN ( name,
type,
arraysize,
address,
...
)
Value:
TOKEN_NEXT_ADDRESS (name, (address)) \
TOKEN_DEF(name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition: token-stack.h:67

DEFINE_INDEXED_TOKEN

#define DEFINE_INDEXED_TOKEN ( name,
type,
arraysize,
...
) TOKEN_DEF (name, CREATOR_##name, 0, 1, type, (arraysize), __VA_ARGS__)

DEFINE_MFG_TOKEN

#define DEFINE_MFG_TOKEN ( name,
type,
address,
...
)
Value:
TOKEN_NEXT_ADDRESS (name, (address)) \
TOKEN_MFG(name, CREATOR_##name, 0, 0, type, 1, __VA_ARGS__)
#define TOKEN_NEXT_ADDRESS(region, address)
By default, tokens are automatically located after the previous token.
Definition: token-stack.h:67

NVM3KEY_DOMAIN_COMMON

#define NVM3KEY_DOMAIN_COMMON   0x80000U

NVM3KEY_DOMAIN_USER

#define NVM3KEY_DOMAIN_USER   0x00000U

NVM3KEY_DOMAIN_ZIGBEE

#define NVM3KEY_DOMAIN_ZIGBEE   0x10000U

NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY

#define NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0100)

NVM3KEY_MULTI_NETWORK_STACK_KEYS

#define NVM3KEY_MULTI_NETWORK_STACK_KEYS   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0000)

NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT

#define NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0200)

NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA

#define NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0080)

NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER

#define NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE220)

NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO

#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0300)

NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO

#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0280)

NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER

#define NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0180)

NVM3KEY_STACK_ADDITIONAL_CHILD_DATA

#define NVM3KEY_STACK_ADDITIONAL_CHILD_DATA   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0700)

NVM3KEY_STACK_ALTERNATE_KEY

#define NVM3KEY_STACK_ALTERNATE_KEY   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE475)

NVM3KEY_STACK_ANALYSIS_REBOOT

#define NVM3KEY_STACK_ANALYSIS_REBOOT   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE162)

NVM3KEY_STACK_APS_FRAME_COUNTER

#define NVM3KEY_STACK_APS_FRAME_COUNTER   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE123)

NVM3KEY_STACK_BINDING_TABLE

#define NVM3KEY_STACK_BINDING_TABLE   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0500)

NVM3KEY_STACK_BOOT_COUNTER

#define NVM3KEY_STACK_BOOT_COUNTER   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE263)

NVM3KEY_STACK_CERTIFICATE_TABLE

#define NVM3KEY_STACK_CERTIFICATE_TABLE   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0680)

NVM3KEY_STACK_CHILD_TABLE

#define NVM3KEY_STACK_CHILD_TABLE   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0580)

NVM3KEY_STACK_CLASSIC_DATA

#define NVM3KEY_STACK_CLASSIC_DATA   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE364)

NVM3KEY_STACK_GP_DATA

#define NVM3KEY_STACK_GP_DATA   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE258)

NVM3KEY_STACK_GP_INCOMING_FC

#define NVM3KEY_STACK_GP_INCOMING_FC   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0480)

NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK

#define NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0780)

NVM3KEY_STACK_GP_PROXY_TABLE

#define NVM3KEY_STACK_GP_PROXY_TABLE   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0380)

NVM3KEY_STACK_GP_SINK_TABLE

#define NVM3KEY_STACK_GP_SINK_TABLE   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0400)

NVM3KEY_STACK_KEY_TABLE

#define NVM3KEY_STACK_KEY_TABLE   ( NVM3KEY_DOMAIN_ZIGBEE | 0x0600)

NVM3KEY_STACK_KEYS

#define NVM3KEY_STACK_KEYS   ( NVM3KEY_DOMAIN_ZIGBEE | 0xEB79)

NVM3KEY_STACK_MIN_RECEIVED_RSSI

#define NVM3KEY_STACK_MIN_RECEIVED_RSSI   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE129)

NVM3KEY_STACK_MULTI_PHY_NWK_INFO

#define NVM3KEY_STACK_MULTI_PHY_NWK_INFO   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE128)

NVM3KEY_STACK_NETWORK_MANAGEMENT

#define NVM3KEY_STACK_NETWORK_MANAGEMENT   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE125)

NVM3KEY_STACK_NODE_DATA

#define NVM3KEY_STACK_NODE_DATA   ( NVM3KEY_DOMAIN_ZIGBEE | 0xEE64)

NVM3KEY_STACK_NONCE_COUNTER

#define NVM3KEY_STACK_NONCE_COUNTER   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE563)

NVM3KEY_STACK_NVDATA_VERSION

#define NVM3KEY_STACK_NVDATA_VERSION   ( NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)

NVM3KEY_STACK_PARENT_ADDITIONAL_INFO

#define NVM3KEY_STACK_PARENT_ADDITIONAL_INFO   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE127)

NVM3KEY_STACK_PARENT_INFO

#define NVM3KEY_STACK_PARENT_INFO   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE126)

NVM3KEY_STACK_TRUST_CENTER

#define NVM3KEY_STACK_TRUST_CENTER   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE124)

NVM3KEY_STACK_ZLL_DATA

#define NVM3KEY_STACK_ZLL_DATA   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE501)

NVM3KEY_STACK_ZLL_SECURITY

#define NVM3KEY_STACK_ZLL_SECURITY   ( NVM3KEY_DOMAIN_ZIGBEE | 0xE502)

TOKEN_NEXT_ADDRESS

#define TOKEN_NEXT_ADDRESS ( region,
address
)

By default, tokens are automatically located after the previous token.

If a token needs to be placed at a specific location, one of the DEFINE_FIXED_* definitions should be used. This macro is inherently used in the DEFINE_FIXED_* definition to locate a token and under special circumstances (such as manufacturing tokens) it may be explicitly used.

Parameters
region A name for the next region being located.
address The address of the beginning of the next region.