Defines a beacon entry that is processed when scanning, joining, or rejoining.

#include < ember-types.h >

Data Fields

uint8_t channel
uint8_t lqi
int8_t rssi
uint8_t depth
uint8_t nwkUpdateId
int8_t power
int8_t parentPriority
bool enhanced : 1
bool permitJoin : 1
bool hasCapacity : 1
EmberPanId panId
EmberNodeId sender
uint8_t extendedPanId [ EXTENDED_PAN_ID_SIZE ]

Defines a beacon entry that is processed when scanning, joining, or rejoining.

Field Documentation

channel

uint8_t EmberBeaconData::channel

depth

uint8_t EmberBeaconData::depth

enhanced

bool EmberBeaconData::enhanced

extendedPanId

uint8_t EmberBeaconData::extendedPanId[ EXTENDED_PAN_ID_SIZE ]

hasCapacity

bool EmberBeaconData::hasCapacity

lqi

uint8_t EmberBeaconData::lqi

nwkUpdateId

uint8_t EmberBeaconData::nwkUpdateId

panId

EmberPanId EmberBeaconData::panId

parentPriority

int8_t EmberBeaconData::parentPriority

permitJoin

bool EmberBeaconData::permitJoin

power

int8_t EmberBeaconData::power

rssi

int8_t EmberBeaconData::rssi

sender

EmberNodeId EmberBeaconData::sender

The documentation for this struct was generated from the following file:
  • ember-types.h