EmberMulticastTableEntry Struct Reference
Defines an entry in the multicast table.
#include <
ember-types.h
>
Data Fields | |
EmberMulticastId | multicastId |
uint8_t | endpoint |
uint8_t | networkIndex |
Defines an entry in the multicast table.
A multicast table entry indicates that a particular endpoint is a member of a particular multicast group. Only devices with an endpoint in a multicast group will receive messages sent to that multicast group.
Field Documentation
◆ endpoint
uint8_t EmberMulticastTableEntry::endpoint |
The endpoint that is a member, or 0 if this entry is not in use (the ZDO is not a member of any multicast groups).
◆ multicastId
EmberMulticastId EmberMulticastTableEntry::multicastId |
The multicast group ID.
◆ networkIndex
uint8_t EmberMulticastTableEntry::networkIndex |
The network index of the network the entry is related to.
The documentation for this struct was generated from the following file:
ember-types.h