EmberEndpoint Struct Reference
Gives the endpoint information for a particular endpoint.
#include <
stack-info.h
>
Data Fields | |
uint8_t | endpoint |
EmberEndpointDescription const * | description |
uint16_t const * | inputClusterList |
uint16_t const * | outputClusterList |
Gives the endpoint information for a particular endpoint.
Field Documentation
◆ description
EmberEndpointDescription const* EmberEndpoint::description |
The endpoint's description.
◆ endpoint
uint8_t EmberEndpoint::endpoint |
An endpoint of the application on this node.
◆ inputClusterList
uint16_t const* EmberEndpoint::inputClusterList |
Input clusters the endpoint will accept.
◆ outputClusterList
uint16_t const* EmberEndpoint::outputClusterList |
Output clusters the endpoint may send.
The documentation for this struct was generated from the following file:
stack-info.h