EmberTransientKeyData Struct Reference

This data structure contains the transient key data that is used during Zigbee 3.0 joining.

#include < ember-types.h >

Data Fields

EmberEUI64 eui64
EmberKeyData keyData
uint32_t incomingFrameCounter
EmberKeyStructBitmask bitmask
uint16_t remainingTimeSeconds

This data structure contains the transient key data that is used during Zigbee 3.0 joining.

Field Documentation

◆ bitmask

EmberKeyStructBitmask EmberTransientKeyData::bitmask

◆ eui64

EmberEUI64 EmberTransientKeyData::eui64

◆ incomingFrameCounter

uint32_t EmberTransientKeyData::incomingFrameCounter

◆ keyData

EmberKeyData EmberTransientKeyData::keyData

◆ remainingTimeSeconds

uint16_t EmberTransientKeyData::remainingTimeSeconds

The documentation for this struct was generated from the following file:
  • ember-types.h