EmberEventData Struct Reference
Complete events with a control and a handler procedure.
#include <
ember-types.h
>
Data Fields | |
EmberEventControl * | control |
void(* | handler )(void) |
Complete events with a control and a handler procedure.
An application typically creates an array of events along with their handlers. The main loop passes the array to emberRunEvents() to call the handlers of any events whose time has arrived.
Field Documentation
◆ control
EmberEventControl* EmberEventData::control |
The control structure for the event.
◆ handler
void(* EmberEventData::handler) (void) |
The procedure to call when the event fires.
The documentation for this struct was generated from the following file:
ember-types.h