Information about the ZLL network and specific device that responded to a ZLL scan request.

#include < zll-types.h >

Data Fields

EmberZigbeeNetwork zigbeeNetwork
EmberZllSecurityAlgorithmData securityAlgorithm
EmberEUI64 eui64
EmberNodeId nodeId
EmberZllState state
EmberNodeType nodeType
uint8_t numberSubDevices
uint8_t totalGroupIdentifiers
uint8_t rssiCorrection

Information about the ZLL network and specific device that responded to a ZLL scan request.

Field Documentation

◆ eui64

EmberEUI64 EmberZllNetwork::eui64

◆ nodeId

EmberNodeId EmberZllNetwork::nodeId

◆ nodeType

EmberNodeType EmberZllNetwork::nodeType

◆ numberSubDevices

uint8_t EmberZllNetwork::numberSubDevices

◆ rssiCorrection

uint8_t EmberZllNetwork::rssiCorrection

◆ securityAlgorithm

EmberZllSecurityAlgorithmData EmberZllNetwork::securityAlgorithm

◆ state

EmberZllState EmberZllNetwork::state

◆ totalGroupIdentifiers

uint8_t EmberZllNetwork::totalGroupIdentifiers

◆ zigbeeNetwork

EmberZigbeeNetwork EmberZllNetwork::zigbeeNetwork

The documentation for this struct was generated from the following file:
  • zll-types.h