Common bootloader interface defines and functions.
Macros | |
#define | BOOTLOADER_BASE_TYPE(extendedType) ((uint8_t)(((extendedType) >> 8U) & 0xFFU)) |
Macro returning the base type of a bootloader when given an extended type. | |
#define | BOOTLOADER_MAKE_EXTENDED_TYPE(baseType, extendedSpecifier) ((uint16_t)(((uint16_t)baseType) << 8U) | (((uint16_t)extendedSpecifier) & 0xFFU)) |
Macro returning the extended type of a bootloader when given a base type and extendedSpecifier. | |
#define | BL_EXT_TYPE_NULL ((BL_TYPE_NULL << 8U) | 0x00U) |
Macro defining the extended NULL bootloader type. | |
#define | BL_EXT_TYPE_STANDALONE_UNKNOWN ((BL_TYPE_STANDALONE << 8U) | 0x00U) |
Macro defining the extended standalone unknown bootloader type. | |
#define | BL_EXT_TYPE_SERIAL_UART ((BL_TYPE_STANDALONE << 8U) | 0x01U) |
Macro defining the extended standalone UART bootloader type. | |
#define | BL_EXT_TYPE_SERIAL_UART_OTA ((BL_TYPE_STANDALONE << 8U) | 0x03U) |
Macro defining the extended standalone OTA and UART bootloader type. | |
#define | BL_EXT_TYPE_EZSP_SPI ((BL_TYPE_STANDALONE << 8U) | 0x04U) |
#define | BL_EXT_TYPE_EZSP_SPI_OTA ((BL_TYPE_STANDALONE << 8U) | 0x06U) |
#define | BL_EXT_TYPE_SERIAL_USB ((BL_TYPE_STANDALONE << 8U) | 0x07U) |
Macro defining the extended standalone USB bootloader type. | |
#define | BL_EXT_TYPE_SERIAL_USB_OTA ((BL_TYPE_STANDALONE << 8U) | 0x08U) |
Macro defining the extended standalone OTA and USB bootloader type. | |
#define | BL_EXT_TYPE_APP_UNKNOWN ((BL_TYPE_APPLICATION << 8U) | 0x00U) |
Macro defining the extended application unknown bootloader type. | |
#define | BL_EXT_TYPE_APP_SPI ((BL_TYPE_APPLICATION << 8U) | 0x01U) |
Macro defining the extended application SPI bootloader type. | |
#define | BL_EXT_TYPE_APP_I2C ((BL_TYPE_APPLICATION << 8U) | 0x02U) |
Macro defining the extended application I2C bootloader type. | |
#define | BL_EXT_TYPE_APP_LOCAL_STORAGE ((BL_TYPE_APPLICATION << 8U) | 0x03U) |
Macro defining a type for the local storage app bootloader. | |
#define | BOOTLOADER_INVALID_VERSION 0xFFFF |
Define an invalid bootloader version. | |
#define | CUSTOMER_APPLICATION_VERSION 0 |
Macro defining the customer application version stored in the ApplicationProperties_t struct. | |
#define | CUSTOMER_APPLICATION_CAPABILITIES 0 |
Macro defining the customer application capabilities stored in the ApplicationProperties_t struct. | |
#define | CUSTOMER_APPLICATION_PRODUCT_ID { 0 } |
Macro defining the customer application product ID stored in the ApplicationProperties_t struct. | |
#define | MPSI_PLUGIN_SUPPORT 0 |
Macro defining the support for the MPSI protocol stored in the capabilities field of the ApplicationProperties_t struct. | |
#define | APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT 31 |
Macro defining the bit position that corresponds to MPSI support in the capabilities field of the ApplicationProperties_t struct. | |
#define | APPLICATION_PROPERTIES_CAPABILITIES |
Macro defining the capabilities that this application has. This value is set in the capabilities field of the ApplicationProperties_t struct. |
Functions | |
BlBaseType | halBootloaderGetType (void) |
Returns the bootloader base type the application was built for. | |
BlExtendedType | halBootloaderGetInstalledType (void) |
Returns the extended bootloader type of the bootloader that is present on the chip. | |
uint16_t | halGetBootloaderVersion (void) |
Returns the version of the installed bootloader, regardless of its type. | |
void | halGetExtendedBootloaderVersion (uint32_t *getEmberVersion, uint32_t *customerVersion) |
Return extended bootloader version information, if supported. This API is not supported for EM2XX chips and only returns extra information on bootloaders built on or after the 4.7 release. |
Bootloader Numerical Definitions | |
These are numerical definitions for the possible bootloader types and a typedef of the bootloader base type. | |
#define | BL_TYPE_NULL (0) |
Numerical definition for a bootloader type. | |
#define | BL_TYPE_STANDALONE (1) |
Numerical definition for a bootloader type. | |
#define | BL_TYPE_APPLICATION (2) |
Numerical definition for a bootloader type. | |
#define | BL_TYPE_BOOTLOADER (3) |
Numerical definition for a bootloader type. | |
#define | BL_TYPE_SMALL_BOOTLOADER (4) |
Numerical definition for a bootloader type. |
Bootloader type definitions | |
typedef uint8_t | BlBaseType |
Define the bootloader base type. | |
typedef uint16_t | BlExtendedType |
Define the bootloader extended type. |
Detailed Description
Common bootloader interface defines and functions.
See bootloader-interface.h
for source code.
Macro Definition Documentation
◆ APPLICATION_PROPERTIES_CAPABILITIES
#define APPLICATION_PROPERTIES_CAPABILITIES |
Macro defining the capabilities that this application has. This value is set in the capabilities field of the ApplicationProperties_t struct.
◆ APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT
#define APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT 31 |
Macro defining the bit position that corresponds to MPSI support in the capabilities field of the ApplicationProperties_t struct.
◆ BL_EXT_TYPE_APP_I2C
#define BL_EXT_TYPE_APP_I2C ((BL_TYPE_APPLICATION << 8U) | 0x02U) |
Macro defining the extended application I2C bootloader type.
◆ BL_EXT_TYPE_APP_LOCAL_STORAGE
#define BL_EXT_TYPE_APP_LOCAL_STORAGE ((BL_TYPE_APPLICATION << 8U) | 0x03U) |
Macro defining a type for the local storage app bootloader.
◆ BL_EXT_TYPE_APP_SPI
#define BL_EXT_TYPE_APP_SPI ((BL_TYPE_APPLICATION << 8U) | 0x01U) |
Macro defining the extended application SPI bootloader type.
◆ BL_EXT_TYPE_APP_UNKNOWN
#define BL_EXT_TYPE_APP_UNKNOWN ((BL_TYPE_APPLICATION << 8U) | 0x00U) |
Macro defining the extended application unknown bootloader type.
◆ BL_EXT_TYPE_EZSP_SPI
#define BL_EXT_TYPE_EZSP_SPI ((BL_TYPE_STANDALONE << 8U) | 0x04U) |
◆ BL_EXT_TYPE_EZSP_SPI_OTA
#define BL_EXT_TYPE_EZSP_SPI_OTA ((BL_TYPE_STANDALONE << 8U) | 0x06U) |
◆ BL_EXT_TYPE_NULL
#define BL_EXT_TYPE_NULL ((BL_TYPE_NULL << 8U) | 0x00U) |
Macro defining the extended NULL bootloader type.
◆ BL_EXT_TYPE_SERIAL_UART
#define BL_EXT_TYPE_SERIAL_UART ((BL_TYPE_STANDALONE << 8U) | 0x01U) |
Macro defining the extended standalone UART bootloader type.
◆ BL_EXT_TYPE_SERIAL_UART_OTA
#define BL_EXT_TYPE_SERIAL_UART_OTA ((BL_TYPE_STANDALONE << 8U) | 0x03U) |
Macro defining the extended standalone OTA and UART bootloader type.
◆ BL_EXT_TYPE_SERIAL_USB
#define BL_EXT_TYPE_SERIAL_USB ((BL_TYPE_STANDALONE << 8U) | 0x07U) |
Macro defining the extended standalone USB bootloader type.
◆ BL_EXT_TYPE_SERIAL_USB_OTA
#define BL_EXT_TYPE_SERIAL_USB_OTA ((BL_TYPE_STANDALONE << 8U) | 0x08U) |
Macro defining the extended standalone OTA and USB bootloader type.
◆ BL_EXT_TYPE_STANDALONE_UNKNOWN
#define BL_EXT_TYPE_STANDALONE_UNKNOWN ((BL_TYPE_STANDALONE << 8U) | 0x00U) |
Macro defining the extended standalone unknown bootloader type.
◆ BL_TYPE_APPLICATION
#define BL_TYPE_APPLICATION (2) |
Numerical definition for a bootloader type.
◆ BL_TYPE_BOOTLOADER
#define BL_TYPE_BOOTLOADER (3) |
Numerical definition for a bootloader type.
◆ BL_TYPE_NULL
#define BL_TYPE_NULL (0) |
Numerical definition for a bootloader type.
◆ BL_TYPE_SMALL_BOOTLOADER
#define BL_TYPE_SMALL_BOOTLOADER (4) |
Numerical definition for a bootloader type.
◆ BL_TYPE_STANDALONE
#define BL_TYPE_STANDALONE (1) |
Numerical definition for a bootloader type.
◆ BOOTLOADER_BASE_TYPE
#define BOOTLOADER_BASE_TYPE | ( | extendedType | ) | ((uint8_t)(((extendedType) >> 8U) & 0xFFU)) |
Macro returning the base type of a bootloader when given an extended type.
◆ BOOTLOADER_INVALID_VERSION
#define BOOTLOADER_INVALID_VERSION 0xFFFF |
Define an invalid bootloader version.
◆ BOOTLOADER_MAKE_EXTENDED_TYPE
#define BOOTLOADER_MAKE_EXTENDED_TYPE | ( | baseType, |
|
extendedSpecifier |
|||
) | ((uint16_t)(((uint16_t)baseType) << 8U) | (((uint16_t)extendedSpecifier) & 0xFFU)) |
Macro returning the extended type of a bootloader when given a base type and extendedSpecifier.
◆ CUSTOMER_APPLICATION_CAPABILITIES
#define CUSTOMER_APPLICATION_CAPABILITIES 0 |
Macro defining the customer application capabilities stored in the ApplicationProperties_t struct.
- Note
- The capabilities field in the ApplicationProperties_t struct is shared with other values.
◆ CUSTOMER_APPLICATION_PRODUCT_ID
#define CUSTOMER_APPLICATION_PRODUCT_ID { 0 } |
Macro defining the customer application product ID stored in the ApplicationProperties_t struct.
◆ CUSTOMER_APPLICATION_VERSION
#define CUSTOMER_APPLICATION_VERSION 0 |
Macro defining the customer application version stored in the ApplicationProperties_t struct.
◆ MPSI_PLUGIN_SUPPORT
#define MPSI_PLUGIN_SUPPORT 0 |
Macro defining the support for the MPSI protocol stored in the capabilities field of the ApplicationProperties_t struct.
Typedef Documentation
◆ BlBaseType
typedef uint8_t BlBaseType |
Define the bootloader base type.
◆ BlExtendedType
typedef uint16_t BlExtendedType |
Define the bootloader extended type.
Function Documentation
◆ halBootloaderGetInstalledType()
BlExtendedType halBootloaderGetInstalledType | ( | void |
| ) |
Returns the extended bootloader type of the bootloader that is present on the chip.
◆ halBootloaderGetType()
BlBaseType halBootloaderGetType | ( | void |
| ) |
Returns the bootloader base type the application was built for.
- Returns
- BL_TYPE_NULL, BL_TYPE_STANDALONE, or BL_TYPE_APPLICATION
◆ halGetBootloaderVersion()
uint16_t halGetBootloaderVersion | ( | void |
| ) |
Returns the version of the installed bootloader, regardless of its type.
- Returns
- Version if bootloader installed, or BOOTLOADER_INVALID_VERSION. A returned version of 0x1234U would indicate version 1.2 build 34
◆ halGetExtendedBootloaderVersion()
void halGetExtendedBootloaderVersion | ( | uint32_t * | getEmberVersion, |
uint32_t * | customerVersion |
||
) |
Return extended bootloader version information, if supported. This API is not supported for EM2XX chips and only returns extra information on bootloaders built on or after the 4.7 release.
- Parameters
-
getEmberVersion
If specified, we will return the full 32bit ember version for this bootloader. Format is major, minor, patch, doc (4bit nibbles) followed by a 16bit build number. customerVersion
This will return the 32bit value specified in CUSTOMER_BOOTLOADER_VERSION at build time.