Forming and Joining Networks

Macros

#define NETWORK_STORAGE_SIZE 16
Number of bytes required to store relevant info for a saved network.
#define NETWORK_STORAGE_SIZE_SHIFT 4
Log_base2 of NETWORK_STORAGE_SIZE .
#define FORM_AND_JOIN_MAX_NETWORKS 15
Number of joinable networks that can be remembered during the scan process.

Functions

EmberStatus emberScanForUnusedPanId (uint32_t channelMask, uint8_t duration)
Find an unused PAN id.
EmberStatus emberScanForJoinableNetwork (uint32_t channelMask, uint8_t *extendedPanId)
Finds a joinable network.
EmberStatus emberScanForNextJoinableNetwork (void)
See emberScanForJoinableNetwork() .
bool emberFormAndJoinIsScanning (void)
Returns true if and only if the form and join library is in the process of scanning and is therefore expecting scan results to be passed to it from the application.
bool emberFormAndJoinCanContinueJoinableNetworkScan (void)
Returns true if and only if the application can continue a joinable network scan by calling emberScanForNextJoinableNetwork() . See emberScanForJoinableNetwork() .
void emberJoinableNetworkFoundHandler ( EmberZigbeeNetwork *networkFound, uint8_t lqi, int8_t rssi)
A callback the application needs to implement.
void emberScanErrorHandler ( EmberStatus status)
A callback the application needs to implement.
bool emberFormAndJoinScanCompleteHandler (uint8_t channel, EmberStatus status)
The application must call this function from within its emberScanCompleteHandler() (on the node) or ezspScanCompleteHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.
bool emberFormAndJoinNetworkFoundHandler ( EmberZigbeeNetwork *networkFound, uint8_t lqi, int8_t rssi)
The application must call this function from within its emberNetworkFoundHandler() (on the node) or ezspNetworkFoundHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.
bool emberFormAndJoinEnergyScanResultHandler (uint8_t channel, int8_t maxRssiValue)
The application must call this function from within its emberEnergyScanResultHandler() (on the node) or ezspEnergyScanResultHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.
bool emberFormAndJoinUnusedPanIdFoundHandler ( EmberPanId panId, uint8_t channel)
The application must call this function from within its emberUnusedPandIdFoundHandler() (on the node) or ezspEnergyScanResultHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.
void emberFormAndJoinTick (void)
void emberFormAndJoinTaskInit (void)
When processor idling is desired on the SOC, this must be called to properly initialize the form and join library.
void emberFormAndJoinRunTask (void)
When processor idling is desired on the SOC, this should be called regularly instead of emberFormAndJoinTick()
void emberFormAndJoinCleanup ( EmberStatus status)
When form-and-join state is no longer needed, the application can call this routine to cleanup and free resources. On the SOC platforms this will free the allocated message buffer.

Variables

bool emberEnableDualChannelScan

Detailed Description

Functions for finding an existing network to join and for finding an unused PAN id with which to form a network.

Summary of application requirements:

For the SOC:

For an EZSP Host:

  • Define ::EZSP_APPLICATION_HAS_ENERGY_SCAN_RESULT_HANDLER in the configuration header.
  • Include form-and-join.c and form-and-join-host-adapter.c in the build.
  • Optionally include form-and-join-host-callbacks.c in the build.

For either platform, the application can omit the form-and-join-*-callback.c file from the build and implement the callbacks itself if necessary. In this case the appropriate form-and-join callback function must be called from within each callback, as is done within the form-and-join-*-callback.c files.

On either platform, FORM_AND_JOIN_MAX_NETWORKS can be explicitly defined to limit (or expand) the number of joinable networks that the library will save for consideration during the scan process.

The library is able to resume scanning for joinable networks from where it left off, via a call to emberScanForNextJoinableNetwork() . Thus if the first joinable network found is not the correct one, the application can continue scanning without starting from the beginning and without finding the same network that it has already rejected. The library can also be used on the host processor.

Macro Definition Documentation

◆ FORM_AND_JOIN_MAX_NETWORKS

#define FORM_AND_JOIN_MAX_NETWORKS   15

Number of joinable networks that can be remembered during the scan process.

Note for SoC Platforms: This is currently limited to a maximum of 15 due to the size of each network entry (16 bytes) and the EmberMessageBuffer API's requirement that total buffer storage length be kept to an 8-bit quantity (less than 256).

Note for EZSP Host Platforms: In the host implementation of this library, the storage size for the detected networks buffer is controlled by ::EZSP_HOST_FORM_AND_JOIN_BUFFER_SIZE, so that limits the highest value that the host can set for FORM_AND_JOIN_MAX_NETWORKS.

◆ NETWORK_STORAGE_SIZE

#define NETWORK_STORAGE_SIZE   16

Number of bytes required to store relevant info for a saved network.

This constant represents the minimum number of bytes required to store all members of the NetworkInfo struct used in the adapter code. Its value should not be changed unless the underlying adapter code is updated accordingly. Note that this constant's value may be different than sizeof(NetworkInfo) because some compilers pad the structs to align on word boundaries. Thus, the adapter code stores/retrieves these pieces of data individually (to be platform-agnostic) rather than as a struct.

For efficiency's sake, this number should be kept to a power of 2 and not and not exceed 32 (PACKET_BUFFER_SIZE).

◆ NETWORK_STORAGE_SIZE_SHIFT

#define NETWORK_STORAGE_SIZE_SHIFT   4

Log_base2 of NETWORK_STORAGE_SIZE .

Function Documentation

◆ emberFormAndJoinCanContinueJoinableNetworkScan()

bool emberFormAndJoinCanContinueJoinableNetworkScan ( void )

Returns true if and only if the application can continue a joinable network scan by calling emberScanForNextJoinableNetwork() . See emberScanForJoinableNetwork() .

◆ emberFormAndJoinCleanup()

void emberFormAndJoinCleanup ( EmberStatus status )

When form-and-join state is no longer needed, the application can call this routine to cleanup and free resources. On the SOC platforms this will free the allocated message buffer.

◆ emberFormAndJoinEnergyScanResultHandler()

bool emberFormAndJoinEnergyScanResultHandler ( uint8_t channel,
int8_t maxRssiValue
)

The application must call this function from within its emberEnergyScanResultHandler() (on the node) or ezspEnergyScanResultHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.

Returns
true iff the library made use of the call.

◆ emberFormAndJoinIsScanning()

bool emberFormAndJoinIsScanning ( void )

Returns true if and only if the form and join library is in the process of scanning and is therefore expecting scan results to be passed to it from the application.

◆ emberFormAndJoinNetworkFoundHandler()

bool emberFormAndJoinNetworkFoundHandler ( EmberZigbeeNetwork * networkFound,
uint8_t lqi,
int8_t rssi
)

The application must call this function from within its emberNetworkFoundHandler() (on the node) or ezspNetworkFoundHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.

Returns
true iff the library made use of the call.

◆ emberFormAndJoinRunTask()

void emberFormAndJoinRunTask ( void )

When processor idling is desired on the SOC, this should be called regularly instead of emberFormAndJoinTick()

◆ emberFormAndJoinScanCompleteHandler()

bool emberFormAndJoinScanCompleteHandler ( uint8_t channel,
EmberStatus status
)

The application must call this function from within its emberScanCompleteHandler() (on the node) or ezspScanCompleteHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.

Returns
true iff the library made use of the call.

◆ emberFormAndJoinTaskInit()

void emberFormAndJoinTaskInit ( void )

When processor idling is desired on the SOC, this must be called to properly initialize the form and join library.

◆ emberFormAndJoinTick()

void emberFormAndJoinTick ( void )

Used by the form and join code on the node to time out a joinable scan after 30 seconds of inactivity. The application must call emberFormAndJoinTick() regularly. This function does not exist for the EZSP host library.

◆ emberFormAndJoinUnusedPanIdFoundHandler()

bool emberFormAndJoinUnusedPanIdFoundHandler ( EmberPanId panId,
uint8_t channel
)

The application must call this function from within its emberUnusedPandIdFoundHandler() (on the node) or ezspEnergyScanResultHandler() (on an EZSP host). Default callback implementations are provided in the form-and-join-*-callbacks.c files.

◆ emberJoinableNetworkFoundHandler()

void emberJoinableNetworkFoundHandler ( EmberZigbeeNetwork * networkFound,
uint8_t lqi,
int8_t rssi
)

A callback the application needs to implement.

Notifies the application of the network found after a call to emberScanForJoinableNetwork() or emberScanForNextJoinableNetwork() .

Parameters
networkFound
lqi The lqi value of the received beacon.
rssi The rssi value of the received beacon.

◆ emberScanErrorHandler()

void emberScanErrorHandler ( EmberStatus status )

A callback the application needs to implement.

If an error occurs while scanning, this function is called and the scan effort is aborted.

Possible return status values are:

Parameters
status

◆ emberScanForJoinableNetwork()

EmberStatus emberScanForJoinableNetwork ( uint32_t channelMask,
uint8_t * extendedPanId
)

Finds a joinable network.

Performs an active scan on the specified channels looking for networks that:

  1. currently permit joining,
  2. match the stack profile of the application,
  3. match the extended PAN id argument if it is not NULL.

Upon finding a matching network, the application is notified via the emberJoinableNetworkFoundHandler() callback, and scanning stops. If an error occurs during the scanning process, the application is informed via the emberScanErrorHandler() , and scanning stops.

If the application determines that the discovered network is not the correct one, it may call emberScanForNextJoinableNetwork() to continue the scanning process where it was left off and find a different joinable network. If the next network is not the correct one, the application can continue to call emberScanForNextJoinableNetwork() . Each call must occur within 30 seconds of the previous one, otherwise the state of the scan process is deleted to free up memory. Calling emberScanForJoinableNetwork() causes any old state to be forgotten and starts scanning from the beginning.

Parameters
channelMask
extendedPanId
Returns
EMBER_LIBRARY_NOT_PRESENT if the form and join library is not available.

◆ emberScanForNextJoinableNetwork()

EmberStatus emberScanForNextJoinableNetwork ( void )

◆ emberScanForUnusedPanId()

EmberStatus emberScanForUnusedPanId ( uint32_t channelMask,
uint8_t duration
)

Find an unused PAN id.

Does an energy scan on the indicated channels and randomly chooses one from amongst those with the least average energy. Then picks a short PAN id that does not appear during an active scan on the chosen channel. The chosen PAN id and channel are returned via the emberUnusedPanIdFoundHandler() callback. If an error occurs, the application is informed via the emberScanErrorHandler() .

Parameters
channelMask
duration The duration of the energy scan. See the documentation for emberStartScan() in stack/include/network-formation.h for information on duration values.
Returns
EMBER_LIBRARY_NOT_PRESENT if the form and join library is not available.

Variable Documentation

◆ emberEnableDualChannelScan

bool emberEnableDualChannelScan

With some board layouts, the EM250 and EM260 are susceptible to a dual channel issue in which packets from 12 channels above or below can sometimes be heard faintly. This affects channels 11 - 14 and 23 - 26. Hardware reference designs EM250_REF_DES_LAT, version C0 and EM250_REF_DES_CER, version B0 solve the problem.

Setting the emberEnableDualChannelScan variable to true enables a software workaround to the dual channel issue which can be used with vulnerable boards. After emberScanForJoinableNetwork() discovers a network on one of the susceptible channels, the channel number that differs by 12 is also scanned. If the same network can be heard there, the true channel is determined by comparing the link quality of the received beacons. The default value of emberEnableDualChannelScan is true for the EM250 and EM260. It is not used on other platforms.