#include < micro-common.h >

Data Fields

uint32_t outgoingNwkFrameCounter
uint32_t incomingParentNwkFrameCounter
uint32_t outgoingLinkKeyFrameCounter
uint32_t incomingLinkKeyFrameCounter

Field Documentation

incomingLinkKeyFrameCounter

uint32_t RTCCRamData::incomingLinkKeyFrameCounter

incomingParentNwkFrameCounter

uint32_t RTCCRamData::incomingParentNwkFrameCounter

outgoingLinkKeyFrameCounter

uint32_t RTCCRamData::outgoingLinkKeyFrameCounter

outgoingNwkFrameCounter

uint32_t RTCCRamData::outgoingNwkFrameCounter

The documentation for this struct was generated from the following file:
  • micro-common.h