#include <zll-types.h
>
◆ bitmask
uint32_t EmberTokTypeStackZllData::bitmask |
◆ freeGroupIdMax
uint16_t EmberTokTypeStackZllData::freeGroupIdMax |
◆ freeGroupIdMin
uint16_t EmberTokTypeStackZllData::freeGroupIdMin |
◆ freeNodeIdMax
uint16_t EmberTokTypeStackZllData::freeNodeIdMax |
◆ freeNodeIdMin
uint16_t EmberTokTypeStackZllData::freeNodeIdMin |
◆ myGroupIdMin
uint16_t EmberTokTypeStackZllData::myGroupIdMin |
◆ rssiCorrection
uint8_t EmberTokTypeStackZllData::rssiCorrection |
The documentation for this struct was generated from the following file: