Crash and Watchdog Diagnostics
Crash and watchdog diagnostic functions.
Macros | |
#define | halResetWasCrash() (((1 << halGetResetInfo()) & RESET_CRASH_REASON_MASK) != 0U) |
Macro evaluating to true if the last reset was a crash, false otherwise. |
Functions | |
uint32_t | halGetMainStackBytesUsed (void) |
Returns the number of bytes used in the main stack. | |
void | halPrintCrashSummary (uint8_t port) |
Print a summary of crash details. | |
void | halPrintCrashDetails (uint8_t port) |
Print the complete, decoded crash details. | |
void | halPrintCrashData (uint8_t port) |
Print the complete crash data. | |
const HalAssertInfoType * | halGetAssertInfo (void) |
If last reset was from an assert, return saved assert information. |
Detailed Description
Crash and watchdog diagnostic functions.
See diagnostic.h
for source code.
Macro Definition Documentation
◆ halResetWasCrash
#define halResetWasCrash | ( |
| ) | (((1 << halGetResetInfo()) & RESET_CRASH_REASON_MASK) != 0U) |
Macro evaluating to true if the last reset was a crash, false otherwise.
Function Documentation
◆ halGetAssertInfo()
const HalAssertInfoType* halGetAssertInfo | ( | void |
| ) |
If last reset was from an assert, return saved assert information.
- Returns
- Pointer to struct containing assert filename and line.
◆ halGetMainStackBytesUsed()
uint32_t halGetMainStackBytesUsed | ( | void |
| ) |
Returns the number of bytes used in the main stack.
- Returns
- The number of bytes used in the main stack.
◆ halPrintCrashData()
void halPrintCrashData | ( | uint8_t | port | ) |
Print the complete crash data.
- Parameters
-
port
Serial port number (0 or 1).
◆ halPrintCrashDetails()
void halPrintCrashDetails | ( | uint8_t | port | ) |
Print the complete, decoded crash details.
- Parameters
-
port
Serial port number (0 or 1).
◆ halPrintCrashSummary()
void halPrintCrashSummary | ( | uint8_t | port | ) |
Print a summary of crash details.
- Parameters
-
port
Serial port number (0 or 1).