EmberEndpointDescription Struct Reference

Endpoint information (a ZigBee Simple Descriptor).

#include < stack-info.h >

Data Fields

uint16_t profileId
uint16_t deviceId
uint8_t deviceVersion
uint8_t inputClusterCount
uint8_t outputClusterCount

Endpoint information (a ZigBee Simple Descriptor).

This is a ZigBee Simple Descriptor and contains information about an endpoint. This information is shared with other nodes in the network by the ZDO.

Field Documentation

◆ deviceId

uint16_t EmberEndpointDescription::deviceId

The endpoint's device ID within the application profile.

◆ deviceVersion

uint8_t EmberEndpointDescription::deviceVersion

The endpoint's device version.

◆ inputClusterCount

uint8_t EmberEndpointDescription::inputClusterCount

The number of input clusters.

◆ outputClusterCount

uint8_t EmberEndpointDescription::outputClusterCount

The number of output clusters.

◆ profileId

uint16_t EmberEndpointDescription::profileId

Identifies the endpoint's application profile.


The documentation for this struct was generated from the following file:
  • stack-info.h