EmberSignatureData Struct Reference
This data structure contains a DSA signature. It is the bit concatenation of the 'r' and 's' components of the signature.
#include <
ember-types.h
>
Data Fields | |
uint8_t | contents [EMBER_SIGNATURE_SIZE] |
This data structure contains a DSA signature. It is the bit concatenation of the 'r' and 's' components of the signature.
Field Documentation
◆ contents
uint8_t EmberSignatureData::contents[EMBER_SIGNATURE_SIZE] |
The documentation for this struct was generated from the following file:
ember-types.h