CHIPEMLIB

Detailed Description

Chip errata workarounds initialization API.

API to initialize chip for errata workarounds.

Functions

__STATIC_INLINE void CHIP_Init (void)
 Chip initialization routine for revision errata workarounds. This function must be called immediately in main().
 

Function Documentation

__STATIC_INLINE void CHIP_Init ( void  )

Chip initialization routine for revision errata workarounds. This function must be called immediately in main().

Note
This function must be called immediately in main().

This init function will configure the device to a state where it is as similar as later revisions as possible, to improve software compatibility with newer parts. See the device specific errata for details.

Definition at line 70 of file em_chip.h.

References _GPIO_P_CTRL_RESETVALUE, BUS_RegBitWrite(), CMU, CMU_BASE, CMU_LFACLKEN0_LCD, EMU, EMU_BASE, GPIO, LCD_BASE, SYSTEM_ChipRevision_TypeDef::major, SYSTEM_ChipRevision_TypeDef::minor, MSC, SYSTEM_ChipRevisionGet(), and SYSTEM_GetProdRev().

Referenced by BSP_initDevice().