LESENSE_ConfAltEx_TypeDef Struct ReferenceEMLIB > LESENSE

Configuration structure for alternate excitation.

Definition at line 945 of file em_lesense.h .

#include < em_lesense.h >

Data Fields

LESENSE_AltExDesc_TypeDef AltEx [16]
LESENSE_AltExMap_TypeDef altExMap

Field Documentation

LESENSE_AltExDesc_TypeDef LESENSE_ConfAltEx_TypeDef::AltEx[16]

Alternate excitation channel descriptors. When altExMap==lesenseAltExMapALTEX only the 8 first descriptors are used. In this mode they describe the configuration of the LES_ALTEX0-7 pins. When altExMap==lesenseAltExMapACMP all 16 descriptors are used. In this mode they describe the configuration of the 16 possible ACMP0-1 excitation channels. Please refer to the user manual for a complete mapping of the routing. NOTE: Some parameters in the descriptors are not valid when altExMap==lesenseAltExMapACMP. Please refer to the definition of the LESENSE_AltExDesc_TypeDef structure for details regarding which parameters are valid.

Definition at line 961 of file em_lesense.h .

Referenced by LESENSE_AltExConfig() .

LESENSE_AltExMap_TypeDef LESENSE_ConfAltEx_TypeDef::altExMap

Select alternate excitation mapping.

Definition at line 947 of file em_lesense.h .

Referenced by LESENSE_AltExConfig() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_lesense.h