BURTC_TypeDef Struct ReferenceDevices > EFM32WG_BURTC

Definition at line 48 of file efm32wg_burtc.h .

Data Fields

__IOM uint32_t CMD
__IM uint32_t CNT
__IOM uint32_t COMP0
__IOM uint32_t CTRL
__IOM uint32_t FREEZE
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t LFXOFDET
__IOM uint32_t LOCK
__IOM uint32_t LPMODE
__IOM uint32_t POWERDOWN
uint32_t RESERVED0 [48]
BURTC_RET_TypeDef RET [128]
__IM uint32_t STATUS
__IM uint32_t SYNCBUSY
__IM uint32_t TIMESTAMP

Field Documentation

__IOM uint32_t BURTC_TypeDef::CMD

Command Register

Definition at line 56 of file efm32wg_burtc.h .

__IM uint32_t BURTC_TypeDef::CNT

Counter Value Register

Definition at line 51 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::COMP0

Counter Compare Value

Definition at line 52 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::FREEZE

Freeze Register

Definition at line 64 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::IEN

Interrupt Enable Register

Definition at line 62 of file efm32wg_burtc.h .

__IM uint32_t BURTC_TypeDef::IF

Interrupt Flag Register

Definition at line 59 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 61 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 60 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::LFXOFDET

LFXO

Definition at line 54 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::LOCK

Configuration Lock Register

Definition at line 58 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::LPMODE

Low power mode configuration

Definition at line 50 of file efm32wg_burtc.h .

__IOM uint32_t BURTC_TypeDef::POWERDOWN

Retention RAM power-down Register

Definition at line 57 of file efm32wg_burtc.h .

uint32_t BURTC_TypeDef::RESERVED0[48]

Reserved registers

Definition at line 67 of file efm32wg_burtc.h .

BURTC_RET_TypeDef BURTC_TypeDef::RET[128]

RetentionReg

Definition at line 68 of file efm32wg_burtc.h .

__IM uint32_t BURTC_TypeDef::STATUS

Status Register

Definition at line 55 of file efm32wg_burtc.h .

__IM uint32_t BURTC_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 65 of file efm32wg_burtc.h .

__IM uint32_t BURTC_TypeDef::TIMESTAMP

Backup mode timestamp

Definition at line 53 of file efm32wg_burtc.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/ efm32wg_burtc.h