LESENSE_DecStCond_TypeDef Struct ReferenceEMLIB > LESENSE
Decoder state condition descriptor structure.
Definition at line 1022
of file em_lesense.h
.
#include <
em_lesense.h
>
Data Fields | |
uint8_t | compMask |
uint8_t | compVal |
uint8_t | nextState |
LESENSE_StTransAct_TypeDef | prsAct |
bool | setInt |
Field Documentation
uint8_t LESENSE_DecStCond_TypeDef::compMask |
Configure compare mask. Set bit X to exclude sensor X from evaluation. Note: decoder can handle sensor inputs from up to 4 sensors, therefore this mask is 4 bit long.
Definition at line 1030
of file em_lesense.h
.
Referenced by LESENSE_DecoderStateConfig().
uint8_t LESENSE_DecStCond_TypeDef::compVal |
Configure compare value. State transition is triggered when sensor state equals to this value. Valid range: 0-15 (4 bits).
Definition at line 1025
of file em_lesense.h
.
Referenced by LESENSE_DecoderStateConfig().
uint8_t LESENSE_DecStCond_TypeDef::nextState |
Configure index of state to be entered if the sensor state equals to compVal. Valid range: 0-15 (4 bits).
Definition at line 1034
of file em_lesense.h
.
Referenced by LESENSE_DecoderStateConfig().
LESENSE_StTransAct_TypeDef LESENSE_DecStCond_TypeDef::prsAct |
Configure which PRS action to perform when sensor state equals to compVal.
Definition at line 1038
of file em_lesense.h
.
Referenced by LESENSE_DecoderStateConfig().
bool LESENSE_DecStCond_TypeDef::setInt |
If enabled, interrupt flag is set when sensor state equals to compVal.
Definition at line 1041
of file em_lesense.h
.
Referenced by LESENSE_DecoderStateConfig().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h