FPUEH_TypeDef Struct ReferenceDevices > EFM32WG_FPUEH
Definition at line 48
of file efm32wg_fpueh.h
.
Data Fields | |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
Field Documentation
__IOM uint32_t FPUEH_TypeDef::IEN |
Interrupt Enable Register
Definition at line 52
of file efm32wg_fpueh.h
.
__IM uint32_t FPUEH_TypeDef::IF |
Interrupt Flag Register
Definition at line 49
of file efm32wg_fpueh.h
.
__IOM uint32_t FPUEH_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 51
of file efm32wg_fpueh.h
.
__IOM uint32_t FPUEH_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 50
of file efm32wg_fpueh.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32WG/Include/
efm32wg_fpueh.h